Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Power Raspberry PI using Solar Panel
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 693 subscribers
  • Views 21067 views
  • Users 0 members are here
  • solar panel raspberry pi
  • raspberry pi
  • power raspberry pi solar
Related

Power Raspberry PI using Solar Panel

feiticeir0
feiticeir0 over 3 years ago

Hi all.

Following a project - AllSky - taking photos all night at the sky - I want to place the PI - Raspberry PI 4 B+ 4GB memory using a SSD NVMe 512GB  - where I don't have a power outlet.

I've the following setup:

- Solar Panel -

  • max power: 20W
  • Vmpp: 18.2V
  • Voc: 22.6V
  • Impp: 1.12A
  • short-circuit: 1.18A

image

That connects to a Waveshare Solar Power Manager (C), that is powered by 3x 18650 batteries - each battery has 3350mAh - NCR18650B.

imageimage

I've set the setup voltage switch for 12V - the same as the solar panel.

image

I don't have a problem with the charging. It charges very well, to full charge.

My problem is, it just wont last all night.

Starting to take pictures at 21:30 (9pm), it only lasts to (the last picture taken) 3:44 (3:44am) . Just over 6h.. This can't be right.

My question is - what can I do to make it last longer. Should I buy more powerful batteries - like 5000mAh or more ? Chose other solar charger ?

I have the Raspberry PI Lite version - and I've disabled some unwanted services like - bluetooth, avahi-daemon, triggerhappy, etc.. I even disabled the status LEDS... Slight smile

Any idea would be great.

Thank you

  • Sign in to reply
  • Cancel
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    What's the time interval like between image captures ? Can you shut the power-hungry R-Pi 4 down between images and then use an ultra low power microcontroller to wake it up before the next one is due ?

    Looks like AllSky can run on a lower-powered R-Pi:

    "A Raspberry Pi (Zero 2, 2, 3, 4) running Pi OS."

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 3 years ago

    What's the time interval like between image captures ? Can you shut the power-hungry R-Pi 4 down between images and then use an ultra low power microcontroller to wake it up before the next one is due ?

    Looks like AllSky can run on a lower-powered R-Pi:

    "A Raspberry Pi (Zero 2, 2, 3, 4) running Pi OS."

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ntewinkel
    ntewinkel over 3 years ago in reply to beacon_dave
    beacon_dave said:
    Can you shut the power-hungry R-Pi 4 down between images

    It looks like there’s no sleep-wake mode on the RPi  (unless that’s a recent addition?), so like you said, it would have to be a shutdown-halt, and then the micro controller triggers a reset (restart).

    You’d have to reduce the start up as much as possible, and I wonder if the starting power draw would offset the savings?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave

    It looks like the default for that AllSky software may be 10-second exposures, every 10 seconds, so it's possible the Pi cannot be shut down unless there are boring intervals (e.g. if one is only interested between certain times of the night maybe). A lower power Pi is definitely a good idea! I think Pi 3B used a lot less power than Pi 4 (from memory), so that would squeeze out another hour or two.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • feiticeir0
    feiticeir0 over 3 years ago in reply to beacon_dave

    I could use a lower RPI, but this is the one the recommend. They even go for the 8GB memory RPi 4. Probably a less power hungry one, like a RPi 3 b+. I have those . I will try .

    The pictures are 1 minute apart during nighttime.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to feiticeir0

    Voltaic do some larger solar power banks which might be worth a look ?

    https://voltaicsystems.com/battery-packs  

    Their larger laptop ones are designed for use with 18v panels and are rated at 88.8Wh and 246.6Wh capacity.

    They have an 'always on' output power feature as well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to feiticeir0

    I think there's a good chance Pi 3B is very likely to perform well if all the software does is take photos (and not processing the images). Although I have several Pi 4's, I almost always use a Pi 3B if I can because the performance is excellent.