Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Power Raspberry PI using Solar Panel
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 695 subscribers
  • Views 20854 views
  • Users 0 members are here
  • solar panel raspberry pi
  • raspberry pi
  • power raspberry pi solar
Related

Power Raspberry PI using Solar Panel

feiticeir0
feiticeir0 over 3 years ago

Hi all.

Following a project - AllSky - taking photos all night at the sky - I want to place the PI - Raspberry PI 4 B+ 4GB memory using a SSD NVMe 512GB  - where I don't have a power outlet.

I've the following setup:

- Solar Panel -

  • max power: 20W
  • Vmpp: 18.2V
  • Voc: 22.6V
  • Impp: 1.12A
  • short-circuit: 1.18A

image

That connects to a Waveshare Solar Power Manager (C), that is powered by 3x 18650 batteries - each battery has 3350mAh - NCR18650B.

imageimage

I've set the setup voltage switch for 12V - the same as the solar panel.

image

I don't have a problem with the charging. It charges very well, to full charge.

My problem is, it just wont last all night.

Starting to take pictures at 21:30 (9pm), it only lasts to (the last picture taken) 3:44 (3:44am) . Just over 6h.. This can't be right.

My question is - what can I do to make it last longer. Should I buy more powerful batteries - like 5000mAh or more ? Chose other solar charger ?

I have the Raspberry PI Lite version - and I've disabled some unwanted services like - bluetooth, avahi-daemon, triggerhappy, etc.. I even disabled the status LEDS... Slight smile

Any idea would be great.

Thank you

  • Sign in to reply
  • Cancel
Parents
  • bidrohini
    bidrohini over 3 years ago

    The idea is good. I hope you can now proceed with the suggestion that you have received here. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bidrohini
    bidrohini over 3 years ago

    The idea is good. I hope you can now proceed with the suggestion that you have received here.