Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Welcome to the New Raspberry Pi 5 - Is it what you hoped?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 701 subscribers
  • Views 8914 views
  • Users 0 members are here
  • raspberry pi 5
  • rpi 5
  • pi 5
Related

Welcome to the New Raspberry Pi 5 - Is it what you hoped?

cstanton
cstanton over 3 years ago

image

We were told that there would be no Raspberry Pi 5 in 2023.

In fact it was said in a lot of places that was the case.

It turns out, that was a lie :D

 Raspberry Pi 5 8GB 

And what a delicious one it is.

• 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, with 512KB L2 caches and a 2MB shared L3 cache
• VideoCore VII GPU
• LPDDR4X-4267 SDRAM (4GB and 8GB SKUs available at launch)
• 2.4 GHz and 5.0 GHz 802.11ac Wi-Fi
• Bluetooth 5.0 / Bluetooth Low Energy (BLE)
• Micro SD card slot, with support for high-speed SDR104 mode
• 2 × USB 3.0 ports, supporting simultaneous 5Gbps operation
• 2 × USB 2.0 ports
• Gigabit Ethernet, with PoE+ support (requires PoE+ HAT)
• 2 × 4 lane MIPI camera/display transceivers
• PCIe 2.0 x1 interface for fast peripherals
• 5V/5A DC power (PD enabled)
• Raspberry Pi standard 40-pin header
• Real-Time Clock (RTC), powered from external battery
• On-board power button!!

I cannot wait to get a hold of one, and I'm amazed that finally, we have need for a heatsink and fan, which comes with thermal pads!

Have you been waiting for a new Raspberry Pi? Perhaps you were content with the existing one? I'll be interested in putting it through its paces.

We previously asked you:  What would you look forward to being on the Raspberry Pi 5 ? - how does this meet up with your expectations? 

  • Sign in to reply
  • Cancel
Parents
  • balajivan1995
    balajivan1995 over 3 years ago

    If only we could have an option to add SSD directly...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balajivan1995
    balajivan1995 over 3 years ago

    If only we could have an option to add SSD directly...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cstanton
    cstanton over 3 years ago in reply to balajivan1995

    A HAT is fine too?


    image

    (This is a prototype m.2 HAT)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to cstanton

    Make the header a bit taller and you might be able to make a longer PCB to squeeze a 2280 onto it too ...

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to Gough Lui

    And then you add a heatsink and fan for the 2280...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balajivan1995
    balajivan1995 over 3 years ago in reply to cstanton

    I have once added a SSD to RPI using USB. If we could squeeze in m2 or nvme connector we don't have to buy extra hat or sata to usb converter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 3 years ago in reply to balajivan1995

    I'd say because of the densely packed PCB that the Pi is already packing that's exactly why it's broken out onto a HAT. At least it's no longer constrained via USB.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balajivan1995
    balajivan1995 over 3 years ago in reply to cstanton

    Could be. Also I don't think the hardware used in RPI directly supports nvme or sata.