Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Welcome to the New Raspberry Pi 5 - Is it what you hoped?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 702 subscribers
  • Views 8794 views
  • Users 0 members are here
  • raspberry pi 5
  • rpi 5
  • pi 5
Related

Welcome to the New Raspberry Pi 5 - Is it what you hoped?

cstanton
cstanton over 2 years ago

image

We were told that there would be no Raspberry Pi 5 in 2023.

In fact it was said in a lot of places that was the case.

It turns out, that was a lie :D

 Raspberry Pi 5 8GB 

And what a delicious one it is.

• 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, with 512KB L2 caches and a 2MB shared L3 cache
• VideoCore VII GPU
• LPDDR4X-4267 SDRAM (4GB and 8GB SKUs available at launch)
• 2.4 GHz and 5.0 GHz 802.11ac Wi-Fi
• Bluetooth 5.0 / Bluetooth Low Energy (BLE)
• Micro SD card slot, with support for high-speed SDR104 mode
• 2 × USB 3.0 ports, supporting simultaneous 5Gbps operation
• 2 × USB 2.0 ports
• Gigabit Ethernet, with PoE+ support (requires PoE+ HAT)
• 2 × 4 lane MIPI camera/display transceivers
• PCIe 2.0 x1 interface for fast peripherals
• 5V/5A DC power (PD enabled)
• Raspberry Pi standard 40-pin header
• Real-Time Clock (RTC), powered from external battery
• On-board power button!!

I cannot wait to get a hold of one, and I'm amazed that finally, we have need for a heatsink and fan, which comes with thermal pads!

Have you been waiting for a new Raspberry Pi? Perhaps you were content with the existing one? I'll be interested in putting it through its paces.

We previously asked you:  What would you look forward to being on the Raspberry Pi 5 ? - how does this meet up with your expectations? 

  • Sign in to reply
  • Cancel
  • misaz
    misaz over 2 years ago in reply to scottiebabe

    Maybe it is just resistor which would be there even not the cool RAM indicator. Something like boot mode selector for the nerby chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago

    Very nice upgrade - it gets a nice performance boost and addresses most of the quibbles with Pi 4. I'm looking forward to see a Pi 500 - I hope it has room for a fast SSD.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balajivan1995
    balajivan1995 over 2 years ago in reply to cstanton

    Could be. Also I don't think the hardware used in RPI directly supports nvme or sata. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to misaz

    Maybe its an ntc thermistor to measure board temp *tin foil hat* lol 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    Nice!

    Great to see the high-speed interfaces have improved and way more easily accessible for users.

    It's a great leap. It opens up the ability to add all sorts of accelerators and high-speed peripherals (AI, video capture, maybe a proper Pi oscilloscope!), real Pi clusters, and I wonder if low-cost PCIe-capable FPGA boards one day become available.

    Exciting for programmers too, a good opportunity to experiment more with drivers. Also will be great to see the capabilities of the new GPU.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to shabaz
    shabaz said:
    maybe a proper Pi oscilloscope

    Have you seen this?

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago

    I cant wait to see how old projects with facial recognition and cameras perform on the new hardware. Thank you for the power button and 2 HDMI ports. The spec sheet makes it sound like a dragster.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to cstanton

    Impressive!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago

    I was so excited to get my RPi4's... until this morning. Stuck out tongue winking eye  The RTC and the power button are fantastic.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 2 years ago

    This announcement was really interesting to see this morning!

    The performance boost is always a welcome upgrade. I especially like the PCIe for SSD support.

    I can see 3rd party cases like the Argon One getting some upgrades to take advantage of the new SSD and fan connectors.

    I agree with feiticeir0 that the power adapter is a bit of a letdown. The original reason for going with a USB power supply was to avoid needing to buy yet another special adapter. But given the problems with so many substandard cables and adapters out there, that might be a good thing. Maybe we’ll eventually see a list of high quality compatible 3rd party options.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>