Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Welcome to the New Raspberry Pi 5 - Is it what you hoped?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 702 subscribers
  • Views 8807 views
  • Users 0 members are here
  • raspberry pi 5
  • rpi 5
  • pi 5
Related

Welcome to the New Raspberry Pi 5 - Is it what you hoped?

cstanton
cstanton over 2 years ago

image

We were told that there would be no Raspberry Pi 5 in 2023.

In fact it was said in a lot of places that was the case.

It turns out, that was a lie :D

 Raspberry Pi 5 8GB 

And what a delicious one it is.

• 2.4GHz quad-core, 64-bit Arm Cortex-A76 CPU, with 512KB L2 caches and a 2MB shared L3 cache
• VideoCore VII GPU
• LPDDR4X-4267 SDRAM (4GB and 8GB SKUs available at launch)
• 2.4 GHz and 5.0 GHz 802.11ac Wi-Fi
• Bluetooth 5.0 / Bluetooth Low Energy (BLE)
• Micro SD card slot, with support for high-speed SDR104 mode
• 2 × USB 3.0 ports, supporting simultaneous 5Gbps operation
• 2 × USB 2.0 ports
• Gigabit Ethernet, with PoE+ support (requires PoE+ HAT)
• 2 × 4 lane MIPI camera/display transceivers
• PCIe 2.0 x1 interface for fast peripherals
• 5V/5A DC power (PD enabled)
• Raspberry Pi standard 40-pin header
• Real-Time Clock (RTC), powered from external battery
• On-board power button!!

I cannot wait to get a hold of one, and I'm amazed that finally, we have need for a heatsink and fan, which comes with thermal pads!

Have you been waiting for a new Raspberry Pi? Perhaps you were content with the existing one? I'll be interested in putting it through its paces.

We previously asked you:  What would you look forward to being on the Raspberry Pi 5 ? - how does this meet up with your expectations? 

  • Sign in to reply
  • Cancel
  • DAB
    DAB over 2 years ago

    Looks interesting, I will have to add this to my toy buy list.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 2 years ago

    I hope the pi4 shortages don't repeat themselves with 5.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 2 years ago in reply to Fred27

    Oooh. It seems that there is an accessible PIO - and an unused M3. Awesome!

    twitter.com/.../1707714277438529644

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to Fred27

    I'll copy that here since it appears to be restricted on some accounts

    image

    And because frankly, using images of text is awful for finding information, here's what it says:

    "There is one PIO instance (4 state machines). It's identical to the PIO blocks on RP2040, except the FIFO depth is doubled. It has single-cycle bus access from the dual Cortex-M3 management processors on RP1, and the PIO FIFOs can also be accessed from the host processor (2712) over PCIe, but the PIO configuration registers are only accessible to the RP1 processors.

    One of the RP1's Cortex-M3's is currently going spare, so it should be possible to write your own Cortex-M firmware and load it into the 16kB per-Cortex-M3 private SRAM. There won't be any software support for this at launch though."

    Luke Wren is an engineer at Raspberry Pi. https://twitter.com/wren6991 

    That's brilliant.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to cstanton

    I think the UART port is there because the gpio header runs to the new chip vs the Broadcom soc (I guess it could have been mixed through too). Wonder what the new features are on the gpio pins :D

    edit: for a linux console over serial

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to scottiebabe

    Maybe an rp2040 class ADC? Grin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to scottiebabe

    Did RPI design their own image signal processor in the RP1? So many questions!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to cstanton

    Not in this case, because all 4 in parallel (unless they manage to apply scottiebabe's  complot theory).  My complot theory is that they:

    • Use a different value per memory configuration
    • And also use it as a visual marker (both for humans and for camera operated production/packaging lines ...
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Gough Lui

    It works on a 3A adapter, but then limits the USB outputs to 600 mA combined.
    With a 5A supply, it allows 1.6 A combined USB out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to scottiebabe

    image

    hmmm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>