Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum The Raspberry Pi 5 has a new Chip - The RP1 has a Secret
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 697 subscribers
  • Views 9526 views
  • Users 0 members are here
  • RP1
  • microprocessor
  • cortex-m3
  • raspberry pi 5
  • programmable input output
  • rp2040
  • microcontroller
  • PIO
Related

The Raspberry Pi 5 has a new Chip - The RP1 has a Secret

cstanton
cstanton over 3 years ago

Those of you who are familiar with desktop or laptop computers will already be familiar with "northbridge" and "southbridge" types of chips. These are common on motherboards these days and compliment the central processing unit and graphics processing unit in your computer.

Usually, a northbridge chipset handles integration between CPU, PCI-E and RAM devices, where as the southbridge communicates with the northbridge and any further, external or legacy or basic components. Such as USB, ISA, BIOS, PCI, IDE, etc.

The Raspberry Pi 5 integrates a southbridge chip, the RP1.

Not a great deal is known about this chip yet, the datasheets haven't been fully revealed or distributed, however there have been some discussions about it in various places by the engineers from Raspberry Pi, and Luke Wren has something to say about its capabilities:

image

If you're unable to read the image it says:

"There is one PIO instance (4 state machines). It's identical to the PIO blocks on RP2040, except the FIFO depth is doubled. It has single-cycle bus access from the dual Cortex-M3 management processors on RP1, and the PIO FIFOs can also be accessed from the host processor (2712) over PCIe, but the PIO configuration registers are only accessible to the RP1 processors.

One of RP1's Cortex-M3s is currently going spare, so it should be possible to write your own Cortex-M firmware and load it into the 16 kB per-Cortex-M3 private SRAM. There won't be any software support for this at launch though."

Luke further elaborates on this on X / Twitter:

I want to walk back that point about PCIe access to FIFOs. The PIO block's AHB port is connected to RP1's processor fabric, and we added a second bus interface which exposes (just) the FIFOs to RP1's system bus fabric, so that RP1's internal DMA can access the FIFOs. This ...

— Luke Wren @wren6991@types.pl (@wren6991) September 29, 2023

... does also expose them over PCIe, since there is a route from 2712's PCIe windows through to the top of RP1's system fabric, but this is not actually usable for host transfers since you can't access the status registers.

Using RP1's PIO requires firmware running on RP1.

— Luke Wren @wren6991@types.pl (@wren6991) September 29, 2023

But yeah, there's a PIO block in there, we're putting that bad boy in everything from now on

— Luke Wren @wren6991@types.pl (@wren6991) September 29, 2023

It would appear that we have another microprocessor to play with! Though for most it will not be a trivial component to handle, and there's no software support for it (just yet). Perhaps those of you that were hoping for an embedded RP2040 can play with this instead?

  • Sign in to reply
  • Cancel
Parents
  • baldengineer
    baldengineer over 3 years ago

    I certainly hope these details point towards an addition to the microcontroller family.

    Larger FIFO on the PIO and Cortex-M3 would make for an interesting RP2040 follow on.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 3 years ago

    I certainly hope these details point towards an addition to the microcontroller family.

    Larger FIFO on the PIO and Cortex-M3 would make for an interesting RP2040 follow on.