Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Wiring pi is defunct.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 698 subscribers
  • Views 6278 views
  • Users 0 members are here
  • c
  • gpio
  • wiringpi
  • raspberry_pi
  • raspberry-pi
  • raspberrypi
Related

Wiring pi is defunct.

SensoredHacker0
SensoredHacker0 over 2 years ago

I used to love using the Wiring Pi library in C for programing the IO of the Raspberry pi.
I haven't used a PI for a project in a while, and I guess in that time developer of WiringPi has
stopped supporting the library.
I tried using version 2.52 on a raspberry pi 4, but it says something like the hardware isn't listed in /proc/cpuinfo.

So I guess I cant use wiringPi. what C libraries would you use for programing GPIO in C on a rasperry Pi 4?
Ive looked around the internet, and I see some various options, but Im not sure what code works with which boards, etc.

  • Sign in to reply
  • Cancel
  • dougw
    0 dougw over 2 years ago

    You could try the Pi 4B update for wiringPi:

    http://wiringpi.com/wiringpi-updated-to-2-52-for-the-raspberry-pi-4b

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bossinfo
    0 bossinfo over 2 years ago

    If you programmed in python the Pi constant is defined in the math and Numpy libraries. Oddly enough it SHOULD exist in the math.h in C/C++. 

    • Cancel
    • Vote Up -4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to bossinfo

    I think that it is different Pi - not 3.1415 constant but library for controlling GPIO on Raspberry Pi SBC...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • JWx
    0 JWx over 2 years ago in reply to dougw

    This is strange - OP is using 2.52 which should be compatible with Pi 4 according to the above link...

    Official documentation seems outdated - repository url from http://wiringpi.com/download-and-install/ is dead.

    I have found unofficial fork on github with an issue describing effort to maintain it:

    https://github.com/WiringPi/WiringPi/issues/80

    and links to some packages with greater version numbers (eg. 2.61) - maybe working better, maybe not - users should decide by themselves if they want to try an unofficial fork.

    The libgpio is mentioned there - but in negative context (as a reason to have wiringpi maintained)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago

    WiringPi certainly does work with Pi 4, I have used it myself on Pi 4. 

    However, it is not maintained (the author doesn't wish to maintain it anymore), so it won't work with Pi 5 at all (unless someone adapts it, which the original author I think doesn't have an interest in pursuing). There is a list of alternatives (some are for Python, but there are some listed for C) here: https://raspberrypi.stackexchange.com/questions/117591/controlling-raspberry-pi-gpio-with-c-and-python

    However, I've not tried any alternative personally on Pi 4. With C, I've only used WiringPi on Pi 4.

    I suspect some people (those that need it for, say, a job and thus have the time - several days of effort to do it properly) are directly programming registers (i.e. do a mmap, followed by writing/reading the registers that are mapped) for the particular Pi they are using, and effectively creating their own API. I've had to do that myself on some platforms (e.g. BeagleBone Black), but it's a lot of effort to initially do, and to maintain. 

    In summary, if it's only Pi 4 that interests you, and you wish to use C programming, then WiringPi should work. Otherwise, if you may eventually want Pi 5 support too, you'd need to choose a different library (e.g. pigpio, but there are various options at that link), which today may not work for Pi 5 but at least has a chance of being supported eventually, if it is actively being maintained currently, or create your own.

    If you don't need fast GPIO, then there are other options (e.g. using /sys/class/gpio) but those are slower. Not every application will need speed, so that may be a possibility. 

    Yet another possibility is to use SPI or I2C (e.g. SPI or I2C GPIO expander) and avoid the WiringPi and its alternatives altogether since you'd be using the normal Linux i2cdev or spidev API, which will always be supported (unless something better comes along one day).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SensoredHacker0
    0 SensoredHacker0 over 2 years ago in reply to shabaz

    is that a 32bit or 64 bit version of the OS?
    Im looking a pigpio, they do some weird things, with how it runs as a daemon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG over 2 years ago in reply to SensoredHacker0

    I would also have suggested pigpio library as the one to use for most general needs. I did come across this link, which offers some other alternatives, e.g. sysfs, or if really up for it, using direct register access.

    elinux.org/RPi_GPIO_Code_Samples

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to shabaz
    shabaz said:
    there are other options (e.g. using /sys/class/gpio)

    I use those, if I don't need fast IO. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to Jan Cumps

    I suspect often people don't need the speed, but simply want DigitalIn/DigitalOut style API functions like a microcontroller's libraries may offer, or Arduino even, and probably they would not mind if the underlying implementation used /sys/class/gpio. 

    Even if slower IO is fine, sometimes an OCD gets the better of me and makes me want to implement it using registers, but it's a lot of work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to shabaz

    As an exercise, I created a little C++ GPIO lib:  C++ gpio library for Raspberry Pi - Pt 1: Design and How To Use 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>