Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Wiring pi is defunct.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 698 subscribers
  • Views 6276 views
  • Users 0 members are here
  • c
  • gpio
  • wiringpi
  • raspberry_pi
  • raspberry-pi
  • raspberrypi
Related

Wiring pi is defunct.

SensoredHacker0
SensoredHacker0 over 2 years ago

I used to love using the Wiring Pi library in C for programing the IO of the Raspberry pi.
I haven't used a PI for a project in a while, and I guess in that time developer of WiringPi has
stopped supporting the library.
I tried using version 2.52 on a raspberry pi 4, but it says something like the hardware isn't listed in /proc/cpuinfo.

So I guess I cant use wiringPi. what C libraries would you use for programing GPIO in C on a rasperry Pi 4?
Ive looked around the internet, and I see some various options, but Im not sure what code works with which boards, etc.

  • Sign in to reply
  • Cancel
  • BigG
    0 BigG over 2 years ago in reply to shabaz

    Here's yet another, more generic, C programming option for Linux, which looks to be quite active in development but is not found in that list. Have yet to test performance...

    github.com/.../c-periphery

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to BigG

    Nice find. Regarding your performance comment, I think for general I/O they have a wrapper around /sys/class/gpio, so it won't be super-fast, but most users just want a wrapper anyway, with a simple API, so it should still be fine for a lot of purposes.

    I'm currently writing a direct register access API for a different board that I need to use, it's going to be basic because I don't wish to maintain something complex. but I wish SBC manufacturers had standardized on a way to make it simple for C/C++ developers to use fast access without having to delve into tech ref manuals, e.g. some C/C++ API framework and a config file that was tailored for the processor/SBC.  I wish raspberrypi.com had taken the initiative and come up with something like a framework that any SBC supplier could use to implement GPIO with the same underlying API calls. That way, people could modify apps to suit Pi 5, 6, etc or other manufacturer boards too.

    A few things that would be useful for that would be the ability to write an API on top (such as DigitalIn/DigitalOut for those who want an Arduino-style API), plus the ability to map different identifiers. For instance, if a different SBC used completely different GPIO pins, it would be good if they could be mapped to Pi GPIO numbers (if people were porting code), or even map to physical pin numbers if desired. Lots of SBCs have a 40-way connector, but of course, the registers will be different.

    Also, as well as C++, such a library would also be linkable to C code (since some legacy stuff might not compile as C++ without a load of errors).

    All that, plus maintaining it, is quite some work for an individual, but a nice constrained, not-insurmountable uni project for a sponsored student for raspberrypi org etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to shabaz

    I'm checking out the memmap register access on the RPi. To test if I can plug in another implementation in the little oo lib I made. Got sidetracked by LoRaWAN things Grin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 2 years ago

    I am not surprised if there are some issues with software post hardware changes.

    Anyone working with an operating system that has some years in will have discovered it. Unfortunately the discovering is typically made when something that doesn't work now, worked previously. I have frozen upgrades on a few of my Pi installs because I know the upgrade would break the system.

    I will tuck this note away if I ever have reason to use a Pi 5. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<