Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Jazz up your Project with an Extruded Aluminum Enclosure
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 697 subscribers
  • Views 5088 views
  • Users 0 members are here
Related

Jazz up your Project with an Extruded Aluminum Enclosure

scottiebabe
scottiebabe over 2 years ago

Unbeknownst to the reader, this project is actually a $4 piece of junk. At a casual glance, you may be tempted to believe it is boutique product.

image

Ooh ahh, fancy. I purchased one of these extruded aluminum enclosure from a local seller.

imageimage

Photos curtesy of this product listing: https://www.aliexpress.com/item/33053448840.html

I cut 2 pieces of bare copper clad board to fit within the PCB mounting channels of the enclosure.

I used my Dremel to drill 4 mounting holes aligned to 4 ground pins on the edge connectors of the Pico.

image

I don’t use the drill press stand attachment to my Dremel enough to have a strong opinion about it. There are fancier model making precision drill presses, but I already have this so I use it.

The Pico soldered to a carrier card

image

To machine out the microUSB connector slot, I first a put a piece of blue tape on the enclosure endplate and made an impression of the connector.

image

I then drilled and filled the slot large enough such that the USB connector could slide right through.

image

Not perfect, but close enough for my standards.

Similar process for the SMA connectors.

The 2 pushbuttons were a very long and tedious process. I drilled the holes first and then tried to solder the buttons to match the holes. I used what I had at hand, but this process could be avoided entirely using proper pushbutton and a custom PCB. But, in the end I got it to fit together fairly well.

image

The second prototype card

image

It is just an amplifier/buffer using a screaming fast hex logic inverter.

In the end I have a little CW signal generator capable of tuning from DC to 200 MHz and provides an output power of ~13.5 dBm into 50 Ohms.

Conclusion

The end result looks fabulous on the exterior.

Locating and machining the cutouts for the USB connector and SMA connector were relatively easy.

There is ample room for prototype style construction and a RPI Pico.

Using this style of enclosure is a lot more work as apposed to loosely tossing everything in a box and using panel mount connectors and interface elements. Wherever you drilled the hole, is where the connector ends up.

If your going to go to the trouble of making a custom PCB, you could make a printable drill template for the endplates. Or spend even more and order custom endplates using a PCB or aluminum.

Happy tinkering!

  • Sign in to reply
  • Cancel
Parents
  • fmilburn
    fmilburn over 2 years ago

    I really like that type of construction. Below is a similar idea from a project I did a few years back that stacked two PCBs and used PCBs for faceplates. Designed for solo sailors, it has a miniature AIS ship radio on the bottom and an “alarm” that sounds and stores incoming messages from nearby ships on top. The user could snooze if it didn’t look like there was an imminent collision and it would alarm again only if the ship hadn’t cleared. 
    image

    image
    /members-area/personalblogs/b/frank-milburn-s-blog/posts/ais-alarm---everything-working#:~:text=The%20ALARM%20starts%20immediately%20upon,stored%2C%20with%20older%20messages%20dropped.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fmilburn
    fmilburn over 2 years ago

    I really like that type of construction. Below is a similar idea from a project I did a few years back that stacked two PCBs and used PCBs for faceplates. Designed for solo sailors, it has a miniature AIS ship radio on the bottom and an “alarm” that sounds and stores incoming messages from nearby ships on top. The user could snooze if it didn’t look like there was an imminent collision and it would alarm again only if the ship hadn’t cleared. 
    image

    image
    /members-area/personalblogs/b/frank-milburn-s-blog/posts/ais-alarm---everything-working#:~:text=The%20ALARM%20starts%20immediately%20upon,stored%2C%20with%20older%20messages%20dropped.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • scottiebabe
    scottiebabe over 2 years ago in reply to fmilburn

    Absolutely wonderful project and construction, it looks like commercial product. Its almost like the case was designed for 100 thou board to board connectors.

    Thanks for sharing, I will have to read through your project for some inspiration.