Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Why do we not see Windows for the Raspberry Pi? Well it may have been due to licensing.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 695 subscribers
  • Views 2343 views
  • Users 0 members are here
  • windows on raspberry pi
  • microsoft windows
  • raspberry pi
  • windows
Related

Why do we not see Windows for the Raspberry Pi? Well it may have been due to licensing.

cstanton
cstanton over 2 years ago

Beyond the IoT Core version, perhaps it has to do with an exclusivity deal with Microsoft and Qualcomm since the Raspberry Pi runs an Arm-based processor.

This isn't explicitly a new article, it was published in 2021, but since there's no explicit date on when that deal will or has, or if it'll expire, perhaps we should now start seeing the fruits of that deal expiring.

An excerpt from the article:

"Last week, we reported that MediaTek is planning to build a chipset for Windows on ARM. As it turns out, the Windows on ARM chipset space could be even hotter than that, because there's a reason that we've only seen Qualcomm SoCs in ARM PCs so far. Qualcomm actually has an exclusivity deal with Microsoft for Windows on ARM, and speaking with people familiar with it, we've learned that the deal is set to expire soon.

Other than the fact that Microsoft has publicly said that anyone who wants to can build a Windows on ARM chip, this really shouldn't come as a surprise. Qualcomm didn't just start building PC chips hoping that Microsoft would compile Windows to support it. No, these two companies worked together to make it happen. Because of that, Qualcomm gets to enjoy a bit of exclusivity.

One thing I wasn't able to learn is when the deal will expire, only that it's the thing holding back other chip vendors from competing in the space. It's possible that Samsung might want to throw its hat into the ring with its Exynos processors too, especially given its recent partnership with AMD for graphics power. This is also presumably why Apple Silicon Macs aren't officially supported for running Windows 11, so hopefully that will change as well."

Anecdotes from Reddit claim that the deal will be ending sometime in 2024, and Arm CEO has allegedly confirmed it will be by the start of 2025, which explains for the further development by AMD and NVIDIA working on their own Arm chips for Windows.

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    Gough Lui over 2 years ago

    Interesting, but I kinda like the fact I don't run Windows on my ARM stuff. The Surface RT wasn't a hit because it had all the clunkiness of Windows with none of the backward compatibility benefits. I think the more modern Windows on ARM OS has some limited support for x86 emulation which makes this less of a downside (although I haven't tried it myself), but unless products bring Apple M1/M2/M3 levels of performance and power efficiency, I struggle to see how it will take off. I can't see Microsoft giving away Windows entirely ... nor can I see myself wanting to run it on a Pi when Linux exists. I may run Windows on the desk, but that's alongside Linux too. If they make it run on a Mac M1/M2/M3, it may be interesting to those users ... but those laptops are way too expensive for what they offer me and I'm not sure Apple would necessarily like that as they're seemingly trying to keep everything "walled garden".

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 2 years ago

    Interesting, but I kinda like the fact I don't run Windows on my ARM stuff. The Surface RT wasn't a hit because it had all the clunkiness of Windows with none of the backward compatibility benefits. I think the more modern Windows on ARM OS has some limited support for x86 emulation which makes this less of a downside (although I haven't tried it myself), but unless products bring Apple M1/M2/M3 levels of performance and power efficiency, I struggle to see how it will take off. I can't see Microsoft giving away Windows entirely ... nor can I see myself wanting to run it on a Pi when Linux exists. I may run Windows on the desk, but that's alongside Linux too. If they make it run on a Mac M1/M2/M3, it may be interesting to those users ... but those laptops are way too expensive for what they offer me and I'm not sure Apple would necessarily like that as they're seemingly trying to keep everything "walled garden".

    - Gough