Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Why do we not see Windows for the Raspberry Pi? Well it may have been due to licensing.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 695 subscribers
  • Views 2343 views
  • Users 0 members are here
  • windows on raspberry pi
  • microsoft windows
  • raspberry pi
  • windows
Related

Why do we not see Windows for the Raspberry Pi? Well it may have been due to licensing.

cstanton
cstanton over 2 years ago

Beyond the IoT Core version, perhaps it has to do with an exclusivity deal with Microsoft and Qualcomm since the Raspberry Pi runs an Arm-based processor.

This isn't explicitly a new article, it was published in 2021, but since there's no explicit date on when that deal will or has, or if it'll expire, perhaps we should now start seeing the fruits of that deal expiring.

An excerpt from the article:

"Last week, we reported that MediaTek is planning to build a chipset for Windows on ARM. As it turns out, the Windows on ARM chipset space could be even hotter than that, because there's a reason that we've only seen Qualcomm SoCs in ARM PCs so far. Qualcomm actually has an exclusivity deal with Microsoft for Windows on ARM, and speaking with people familiar with it, we've learned that the deal is set to expire soon.

Other than the fact that Microsoft has publicly said that anyone who wants to can build a Windows on ARM chip, this really shouldn't come as a surprise. Qualcomm didn't just start building PC chips hoping that Microsoft would compile Windows to support it. No, these two companies worked together to make it happen. Because of that, Qualcomm gets to enjoy a bit of exclusivity.

One thing I wasn't able to learn is when the deal will expire, only that it's the thing holding back other chip vendors from competing in the space. It's possible that Samsung might want to throw its hat into the ring with its Exynos processors too, especially given its recent partnership with AMD for graphics power. This is also presumably why Apple Silicon Macs aren't officially supported for running Windows 11, so hopefully that will change as well."

Anecdotes from Reddit claim that the deal will be ending sometime in 2024, and Arm CEO has allegedly confirmed it will be by the start of 2025, which explains for the further development by AMD and NVIDIA working on their own Arm chips for Windows.

  • Sign in to reply
  • Cancel
Parents
  • Fred27
    Fred27 over 2 years ago

    I'm a developer concentrating mostly on a Microsoft stack and using Windows for development. Even so, I can't see a benefit of running Windows on the Raspberry Pi. Windows 10 IoT was a clunky disaster and I have no desire to see anything like that again.

    .NET Core runs really well on both the Pi and BeagleBone and I've created a few products along those lines. From a purely dev perspective running .NET Core on Debian feels like the right way to go. Even if Windows ran reasonably well with a full UI on a Pi5 (for instance) I don't think I'd want to go that way anyway.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Fred27
    Fred27 over 2 years ago

    I'm a developer concentrating mostly on a Microsoft stack and using Windows for development. Even so, I can't see a benefit of running Windows on the Raspberry Pi. Windows 10 IoT was a clunky disaster and I have no desire to see anything like that again.

    .NET Core runs really well on both the Pi and BeagleBone and I've created a few products along those lines. From a purely dev perspective running .NET Core on Debian feels like the right way to go. Even if Windows ran reasonably well with a full UI on a Pi5 (for instance) I don't think I'd want to go that way anyway.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cstanton
    cstanton over 2 years ago in reply to Fred27
    Fred27 said:
    I can't see a benefit of running Windows on the Raspberry Pi

    Never underestimate the intimidation of being unable to navigate a Linux file system in comparison to Windows.

    "What's /etc/ ?"

    "Where are my files? What's /home/ and why can't I write to /usr/lib?"

    "I just want to install Java so that Minecraft will run on my Pi, which version do I run?"

    "I set a sudo password and now I can't remember it, do I have to reinstall?"