Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Why do we not see Windows for the Raspberry Pi? Well it may have been due to licensing.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 695 subscribers
  • Views 2342 views
  • Users 0 members are here
  • windows on raspberry pi
  • microsoft windows
  • raspberry pi
  • windows
Related

Why do we not see Windows for the Raspberry Pi? Well it may have been due to licensing.

cstanton
cstanton over 2 years ago

Beyond the IoT Core version, perhaps it has to do with an exclusivity deal with Microsoft and Qualcomm since the Raspberry Pi runs an Arm-based processor.

This isn't explicitly a new article, it was published in 2021, but since there's no explicit date on when that deal will or has, or if it'll expire, perhaps we should now start seeing the fruits of that deal expiring.

An excerpt from the article:

"Last week, we reported that MediaTek is planning to build a chipset for Windows on ARM. As it turns out, the Windows on ARM chipset space could be even hotter than that, because there's a reason that we've only seen Qualcomm SoCs in ARM PCs so far. Qualcomm actually has an exclusivity deal with Microsoft for Windows on ARM, and speaking with people familiar with it, we've learned that the deal is set to expire soon.

Other than the fact that Microsoft has publicly said that anyone who wants to can build a Windows on ARM chip, this really shouldn't come as a surprise. Qualcomm didn't just start building PC chips hoping that Microsoft would compile Windows to support it. No, these two companies worked together to make it happen. Because of that, Qualcomm gets to enjoy a bit of exclusivity.

One thing I wasn't able to learn is when the deal will expire, only that it's the thing holding back other chip vendors from competing in the space. It's possible that Samsung might want to throw its hat into the ring with its Exynos processors too, especially given its recent partnership with AMD for graphics power. This is also presumably why Apple Silicon Macs aren't officially supported for running Windows 11, so hopefully that will change as well."

Anecdotes from Reddit claim that the deal will be ending sometime in 2024, and Arm CEO has allegedly confirmed it will be by the start of 2025, which explains for the further development by AMD and NVIDIA working on their own Arm chips for Windows.

  • Sign in to reply
  • Cancel
Parents
  • feiticeir0
    feiticeir0 over 2 years ago

    Despite the licensing issue, they would have to strip down windows a lot for it to run well on a Raspberry PI - unless only the PI5 would be supported.

    The Windows Surface RT was a disaster.  And M$ would have a lot of work - alongside the companies that offer software for windows - for it to have the same software availability that Linux has for the ARM versions.

    I'm sure that, if it existed (with graphical environment), a lot of people would use it (not me). IMHO, having Linux running in it - and very well - there's no need for M$ to bring windows to it.  It's a niche environment and I'm not sure if M$ would have a profit at all (Work that would be x licenses sold x Software availability) .

    Not when there are mini computers the size of the Raspberry PI with x86_64 processors that can run windows.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • feiticeir0
    feiticeir0 over 2 years ago

    Despite the licensing issue, they would have to strip down windows a lot for it to run well on a Raspberry PI - unless only the PI5 would be supported.

    The Windows Surface RT was a disaster.  And M$ would have a lot of work - alongside the companies that offer software for windows - for it to have the same software availability that Linux has for the ARM versions.

    I'm sure that, if it existed (with graphical environment), a lot of people would use it (not me). IMHO, having Linux running in it - and very well - there's no need for M$ to bring windows to it.  It's a niche environment and I'm not sure if M$ would have a profit at all (Work that would be x licenses sold x Software availability) .

    Not when there are mini computers the size of the Raspberry PI with x86_64 processors that can run windows.