Raspberry Pi Forum Raspberry Pi Pico 2 and a new micro-controller with RISC-V and Arm?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 678 subscribers
  • Views 6964 views
  • Users 0 members are here
  • RP2350
  • rp2350a
  • rp2354b
  • raspberyr pi pico 2
  • rp2354a
  • rp2350b
Related

Raspberry Pi Pico 2 and a new micro-controller with RISC-V and Arm?

cstanton
cstanton over 1 year ago

image

I haven't made the jump to playing with RISC-V yet, I'm wondering what the advantages are there.

And this makes it quad-core, right?

Crazy.

I have a lot of reading to do!

 Hardware Design with the RP2350 /  RP2350 Datasheet /  RP2350 Product Brief 

 Of course there's the Pico 2:  Raspberry Pi Pico 2 Datasheet  - I admit I haven't touched a Pico 1 yet.

What am I missing out on?

  • Sign in to reply
  • Cancel
  • aswinvenu
    aswinvenu over 1 year ago in reply to shabaz

    May be its a trial run for a future RISCV only SoC. May be Pico3 be an exclusive RISCV CPU!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    I'm going to say it:

    Risk architecture (like many these days) only matters to 

    • controller manufacturers that have to pay a per-chip license to ARM, and
    • assembler language developers that do a better job than the GCC / Lang toolchain developers
    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    And also feels like quite a hostile move against ARM. They can't surely be happy about it. I'm guessing there's zero revenue payable to ARM unless the cores are actually used (well, made available to customers to access), and now it's in raspberrypi.com control to turn off that license fee tap if they want, by just programming the register to disable the cores.

    Also, wondering just out of curiosity does anyone know if that's the only third-party IP in the chips, or if rasperrypi.com also pay fees for anything else in the chip? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • aswinvenu
    aswinvenu over 1 year ago in reply to Fred27

    image

    3.9.2. Mixed Architecture Combinations :
    The ARCHSEL register has one bit for each processor socket, so it is possible to request mixed combinations of Arm and RISC-V processors: either Arm core 0 and RISC-V core 1, or RISC-V core 0 and Arm core 1

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 1 year ago in reply to shabaz

    They even pay fees for standard peripherals like I2C driver. In this particular case, I2C controller is licenced from synopsys. Majority of this chip is just bought elsewhere. It is quite common nowadays.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 1 year ago in reply to Jan Cumps

    CPU architecture affect much more and one more reason is: perfromance. While for some embedded application it does not matter much, nowdays we see increased usage of AI/ML models on MCU and in that case perofrmance is very important and it really matter if your AI model run 5 times faster on the same clock rate just because instruction set is more optimized for these applications.

    I thought that vendors will go Maxim way that integrates HW accelerator and optimized DMA for accelerating loading data, coeficients, and do ccomputations in HW accelerated and highly paralelised way, but it seems that most other vendors go by increasing clock rate and optimizing instruction set (ARM Cortex-M35, 55, 85) for these applications instead.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to misaz

    I was going to ask how you knew that, if there was a list, but just noticed that the RP2040 documentation (RP2040 PDF datasheet) contains it. 

    Easiest way is to search for the text "used with permission" and the IP is discovered, summarized here:

    • UART: ARM PrimeCell
    • I2C: Synopsys
    • SPI: ARM PrimeCell
    • SSI: Synopsys

    The only difference with RP2350 PDF datasheet, is that the latter does not mention Synopsis for the IP for SSI (used for the QSPI interface in the RP2040, for the Flash memory).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to misaz

    I thought that the i2c fees expired in the earlier 2000s ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 1 year ago in reply to Jan Cumps

    It is not fee for a I2C licence. It is fee for a licence for a VHDL/Verilog implementation of controller.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 1 year ago in reply to Jan Cumps

    I don't know how well the Risk 5 competes with ARM M33, clock for clock or watt for watt. And there may well be big performance differences between different manufacturers implementations of the same cores.

    I've been working a project using the ST32MU575 (Cortex M33 like the Pico 2350) and the interesting thing about this chip is how much of it is devoted to peripherals. It costs more than the 2350 but totally blows it away in terms of on chip peripheral support. Partly as an experiment, but for some other reasons too,  I have chosen to implement quite a complex project without using interrupts at all. This is possible on the 'U575 because of the sophisticated timers and the complex linking possible between timers, the two ADCs (1  is 14 bit)  and the USARTS etc. The DMA is pretty flashy too, offering a linked list architecture which can do amazing stuff once your brain gets over the shock !

    I'd really like to see some some comparisons between the different cores on the 2350 because I think Jan may be right, but with the additional caveat that its (often) what surrounds the core that matters.

    (Oh, and don't forget tool and debugging support !)

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>