Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum solved - Pico C/C++ SDK: have you tried setting the UART baud?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 697 subscribers
  • Views 5115 views
  • Users 0 members are here
  • raspberry
  • pico
  • sdk
Related

solved - Pico C/C++ SDK: have you tried setting the UART baud?

Jan Cumps
Jan Cumps over 2 years ago

I tried the last Pico SDK, and tried to make it run the blinky (hello world" example.

In that example, the speed is set to 9600 baud. But it seems to spanw 115.200 nonetheless, over the UART pins. I created the project with the new VSCode plugin.

Build file (generated by the plugin):

# Generated Cmake Pico project file

cmake_minimum_required(VERSION 3.13)

set(CMAKE_C_STANDARD 11)
set(CMAKE_CXX_STANDARD 17)
set(CMAKE_EXPORT_COMPILE_COMMANDS ON)

# Initialise pico_sdk from installed location
# (note this can come from environment, CMake cache etc)

# == DO NEVER EDIT THE NEXT LINES for Raspberry Pi Pico VS Code Extension to work ==
if(WIN32)
    set(USERHOME $ENV{USERPROFILE})
else()
    set(USERHOME $ENV{HOME})
endif()
set(sdkVersion 2.0.0)
set(toolchainVersion 13_2_Rel1)
set(picotoolVersion 2.0.0)
include(${USERHOME}/.pico-sdk/cmake/pico-vscode.cmake)
# ====================================================================================
set(PICO_BOARD pico CACHE STRING "Board type")

# Pull in Raspberry Pi Pico SDK (must be before project)
include(pico_sdk_import.cmake)

project(blinky C CXX ASM)

# Initialise the Raspberry Pi Pico SDK
pico_sdk_init()

# Add executable. Default name is the project name, version 0.1

add_executable(blinky blinky.c )

pico_set_program_name(blinky "blinky")
pico_set_program_version(blinky "0.1")

# Modify the below lines to enable/disable output over UART/USB
pico_enable_stdio_uart(blinky 1)
pico_enable_stdio_usb(blinky 0)

# Add the standard library to the build
target_link_libraries(blinky
        pico_stdlib)

# Add the standard include files to the build
target_include_directories(blinky PRIVATE
  ${CMAKE_CURRENT_LIST_DIR}
  ${CMAKE_CURRENT_LIST_DIR}/.. # for our common lwipopts or any other standard includes, if required
)

pico_add_extra_outputs(blinky)

Source file (also generated by the plugin):

#include <stdio.h>
#include "pico/stdlib.h"
#include "hardware/uart.h"
#include "hardware/gpio.h"
#include "hardware/divider.h"

// UART defines
// By default the stdout UART is `uart0`, so we will use the second one
#define UART_ID uart1
#define BAUD_RATE 9600

// Use pins 4 and 5 for UART1
// Pins can be changed, see the GPIO function select table in the datasheet for information on GPIO assignments
#define UART_TX_PIN 4
#define UART_RX_PIN 5

// GPIO defines
// Example uses GPIO 2
#define GPIO 2




int main()
{
    stdio_init_all();

    // Set up our UART
    uart_init(UART_ID, BAUD_RATE);
    // Set the TX and RX pins by using the function select on the GPIO
    // Set datasheet for more information on function select
    gpio_set_function(UART_TX_PIN, GPIO_FUNC_UART);
    gpio_set_function(UART_RX_PIN, GPIO_FUNC_UART);
    // For more examples of UART use see https://github.com/raspberrypi/pico-examples/tree/master/uart

    // GPIO initialisation.
    // We will make this GPIO an input, and pull it up by default
    gpio_init(GPIO);
    gpio_set_dir(GPIO, GPIO_IN);
    gpio_pull_up(GPIO);
    // See https://github.com/raspberrypi/pico-examples/tree/master/gpio for other gpio examples, including using interrupts

    // Example of using the HW divider. The pico_divider library provides a more user friendly set of APIs 
    // over the divider (and support for 64 bit divides), and of course by default regular C language integer
    // divisions are redirected thru that library, meaning you can just use C level `/` and `%` operators and
    // gain the benefits of the fast hardware divider.
    int32_t dividend = 123456;
    int32_t divisor = -321;
    // This is the recommended signed fast divider for general use.
    divmod_result_t result = hw_divider_divmod_s32(dividend, divisor);
    printf("%d/%d = %d remainder %d\n", dividend, divisor, to_quotient_s32(result), to_remainder_s32(result));
    // This is the recommended unsigned fast divider for general use.
    int32_t udividend = 123456;
    int32_t udivisor = 321;
    divmod_result_t uresult = hw_divider_divmod_u32(udividend, udivisor);
    printf("%d/%d = %d remainder %d\n", udividend, udivisor, to_quotient_u32(uresult), to_remainder_u32(uresult));
    // See https://github.com/raspberrypi/pico-examples/tree/master/divider for more complex use

    while (true) {
        printf("Hello, world!\n");
        sleep_ms(1000);
    }
}

If I use a TTL-to-USB bridge, it generates garble at 9600, readable data at 115200...

115200 baud:

image

9600 baud:

image

I'm using a Pico RP2040, SDK 2.0.0, GCC 13.2.1

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 2 years ago

    solved.

    the example code is using UART1,  gpio 4 and 5, while my TTL-UART bridge was connected to gpio 0 and 1.

    If I change the code to UART0, pin 0 and 1, it works.

    (not sure though, why I did get data - at 115200 - on pin 0 ....)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 2 years ago in reply to Jan Cumps

     Jan Cumps Did I read your post correctly, broke at 9600 but works at 115200??  Duh, what can say I can't say it here. LOL  ~~ Cris H. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • phoenixcomm
    0 phoenixcomm over 2 years ago in reply to Jan Cumps

     Jan Cumps Did I read your post correctly, broke at 9600 but works at 115200??  Duh, what can say I can't say it here. LOL  ~~ Cris H. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to phoenixcomm

    no,

    If I set UART1 to 9600, and talk to that UART1, it works as expected. Data appears at 9600 on the TX pin of UART1.

    What I noticed, is that it also sends the same message to UART0 TX, at the default speed (115200)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 2 years ago in reply to Jan Cumps

    It was something else in the end, and I did not analyse it well:

    printf() always uses UART0

    The example code initialises UART1, and sets it speed to 9600 baud, and then it does printf() -- and that doesn't use that UART1

    But because I didn't change UART0's speed, it will output it at 115200

    If I change UART0 speed, the code behaves as expected.

    I got confused by the example tht the VS Code plugin generated:

    #include <stdio.h>
    #include "pico/stdlib.h"
    #include "hardware/uart.h"
    #include "hardware/gpio.h"
    
    // UART defines
    // By default the stdout UART is `uart0`, so we will use the second one
    #define UART_ID uart1
    #define BAUD_RATE 9600
    
    // Use pins 4 and 5 for UART1
    // Pins can be changed, see the GPIO function select table in the datasheet for information on GPIO assignments
    #define UART_TX_PIN 4
    #define UART_RX_PIN 5
    
    int main()
    {
        stdio_init_all();
    
        // Set up our UART
        uart_init(UART_ID, BAUD_RATE);
        // Set the TX and RX pins by using the function select on the GPIO
        // Set datasheet for more information on function select
        gpio_set_function(UART_TX_PIN, GPIO_FUNC_UART);
        gpio_set_function(UART_RX_PIN, GPIO_FUNC_UART);
        while (true) {
            printf("Hello, world!\n");
            sleep_ms(1000);
        }
    }