Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace Digital 2 and reaction timer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 704 subscribers
  • Views 706 views
  • Users 0 members are here
  • raspberry
  • pi
  • raspberry_pi
  • piface digital 2
Related

PiFace Digital 2 and reaction timer

e14 Contributor
e14 Contributor over 10 years ago

Help!

 

I'm a complete noob, although do have a bit of a background in programming.

 

I have a Pi B+ and a PiFaceDigital 2 - all working fine etc..

 

I want to create a programe that does the following:

 

1)     Wait for an input on one of the inputs (a push switch or similar - there will be four connected)

2)     When a push switch is activiate, tell me which push switch has been activated, and the time elapsed since starting the programme. I also want to activate one of the relays at this stage

 

I can control the outputs in code, but am struggling with the interpupts to listen to the push switches. Also, not sure on the timing element - I guess I need to run a timer of some sort, and the interupt will stop the timer.

 

As I'm a noob, I could do with seeing some examples of code - I'm quick to learn, and can adapt stuff, but I'm really struggling with the interupts element of the PiFaceDigital board.

 

Any ideas? Help very much appreciated.

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    OK - I did this - but I have some problems with the PiFaceDigital not initialising - as it's seperate, I'll start a new question...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hiteccol80
    hiteccol80 over 6 years ago in reply to e14 Contributor

    Hi I read your question with great interest as I want to do something very similar with the same set up as you have.  Could you let me have your script please.

     

    My requirement is as follows but I am sure I could use your script.

     

    Help!

     

    I'm a complete noob at Python, although do have a background in computer hardware and electronics.

     

    I have a Pi B+ and a PiFace Digital 2 - all working fine and I can control each of the outputs from the emulator and the command line in code using one of the examples provided etc.

     

    I want to create a programe that does the following:

     

    1)     Wait for an input on one of the inputs (a push switch or similar - there will be four connected)

    2)     When a push switch is activiated, commence a sequence of turning each output on for 3 seconds then off before moving on to the next output for three seconds untill each output has been sequentually activated for three seconds then stop.

     

    I can control the outputs from the emulator and in code from the command line, but am struggling with the above sequence.

     

    As I'm a complete programming noob, I could do with seeing some examples of code - I'm quick to learn, and can adapt stuff, but I'm really struggling with putting this sequence together for the PiFace Digital board.

     

    Any ideas? Help very much appreciated.

     

    Thanks!

    Colin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hiteccol80
    hiteccol80 over 6 years ago in reply to e14 Contributor

    Hi I read your question with great interest as I want to do something very similar with the same set up as you have.  Could you let me have your script please.

     

    My requirement is as follows but I am sure I could use your script.

     

    Help!

     

    I'm a complete noob at Python, although do have a background in computer hardware and electronics.

     

    I have a Pi B+ and a PiFace Digital 2 - all working fine and I can control each of the outputs from the emulator and the command line in code using one of the examples provided etc.

     

    I want to create a programe that does the following:

     

    1)     Wait for an input on one of the inputs (a push switch or similar - there will be four connected)

    2)     When a push switch is activiated, commence a sequence of turning each output on for 3 seconds then off before moving on to the next output for three seconds untill each output has been sequentually activated for three seconds then stop.

     

    I can control the outputs from the emulator and in code from the command line, but am struggling with the above sequence.

     

    As I'm a complete programming noob, I could do with seeing some examples of code - I'm quick to learn, and can adapt stuff, but I'm really struggling with putting this sequence together for the PiFace Digital board.

     

    Any ideas? Help very much appreciated.

     

    Thanks!

    Colin.