Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum have you debugged a Pico2 RISC program with a PICOPROBE / DEBUGPROBE?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 699 subscribers
  • Views 4402 views
  • Users 0 members are here
  • pico2
  • pico
  • pico 2
  • pico_eurocard
  • pico-eurocard
Related

have you debugged a Pico2 RISC program with a PICOPROBE / DEBUGPROBE?

Jan Cumps
Jan Cumps over 1 year ago

Have you been able to debug a C Pico2 RISC project with a PicoProbe / DebugProbe?

edit: solution:  RE: have you debugged a Pico2 RISC program with a PICOPROBE / DEBUGPROBE? 

I use VSCode and the Raspberry Pico Extension - all up to date as of today - to create a Pico2 project.
If that project is using Pico2 ARM cores, the debugger manages to program the RP2350 and debug it.
If I switch that project to RISC (or create a fresh Pico2 RISC project), the build succeeds, but debugging doesn't.

image

Error:

[2025-06-19T22:57:07.909Z] SERVER CONSOLE DEBUG: onBackendConnect: gdb-server session connected. You can switch to "DEBUG CONSOLE" to see GDB interactions.
"C:\\Users\\jancu/.pico-sdk/openocd/0.12.0+dev/openocd.exe" -c "gdb_port 50000" -c "tcl_port 50001" -c "telnet_port 50002" -s "C:\\Users\\jancu/.pico-sdk/openocd/0.12.0+dev/scripts" -f "c:/Users/jancu/.vscode/extensions/marus25.cortex-debug-1.12.1/support/openocd-helpers.tcl" -f interface/cmsis-dap.cfg -f target/rp2350-riscv.cfg -c "adapter speed 5000"
Open On-Chip Debugger 0.12.0+dev-g75bc439-dirty (2024-08-08-15:04)
Licensed under GNU GPL v2
For bug reports, read
openocd.org/.../bugs.html
CDLiveWatchSetup
Info : Hardware thread awareness created
Info : Hardware thread awareness created
adapter speed: 5000 kHz
Info : Listening on port 50001 for tcl connections
Info : Listening on port 50002 for telnet connections
Info : Using CMSIS-DAPv2 interface with VID:PID=0x2e8a:0x000c, serial=4150323038323713
Info : CMSIS-DAP: SWD supported
Info : CMSIS-DAP: Atomic commands supported
Info : CMSIS-DAP: Test domain timer supported
Info : CMSIS-DAP: FW Version = 2.0.0
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 0 SWDIO/TMS = 0 TDI = 0 TDO = 0 nTRST = 0 nRESET = 0
Info : CMSIS-DAP: Interface ready
Info : clock speed 5000 kHz
Info : SWD DPIDR 0x4c013477
Info : [rp2350.dap.core0] datacount=1 progbufsize=2
Info : [rp2350.dap.core0] unavailable.
Error: [rp2350.dap.core0] Examination failed
Warn : target rp2350.dap.core0 examination failed
Info : [rp2350.dap.core1] datacount=1 progbufsize=2
Info : [rp2350.dap.core1] unavailable.
Error: [rp2350.dap.core1] Examination failed
Warn : target rp2350.dap.core1 examination failed
Info : starting gdb server for rp2350.dap.core0 on 50000
Info : Listening on port 50000 for gdb connections
Info : accepting 'gdb' connection on tcp/50000
Error: Target not examined yet
Error executing event gdb-attach on target rp2350.dap.core0:

Error: Target not examined yet
Error: Function FUNC_FLASH_EXIT_XIP not found in RP2xxx ROM.
Error: auto_probe failed
Error: Connect failed. Consider setting up a gdb-attach event for the target to prepare target for GDB connect, or use 'gdb_memory_map disable'.
Error: attempted 'gdb' connection rejected
[2025-06-19T22:57:10.180Z] SERVER CONSOLE DEBUG: onBackendConnect: gdb-server session closed
GDB server session ended. This terminal will be reused, waiting for next session to start...

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    0 Jan Cumps over 1 year ago

    repeatable solution to get a new RP2350 debug-able in riscv mode:

    1 time:

    • build a program
    • start pico2 up in BOOTSEL mode (push bootsel and connect to computer with USB)
    • from project folder, execute (I use VSCode PowerShell terminal): picotool reboot -c riscv -u
    • drop the riscv uf2 firmware on the disc (only needed 1 time)
    • disconnect

    from then on:

    • connect a debugger, and now you can flash and debug with the default Pico Debug (Cortex-Debug) profile.
    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 1 year ago

    repeatable solution to get a new RP2350 debug-able in riscv mode:

    1 time:

    • build a program
    • start pico2 up in BOOTSEL mode (push bootsel and connect to computer with USB)
    • from project folder, execute (I use VSCode PowerShell terminal): picotool reboot -c riscv -u
    • drop the riscv uf2 firmware on the disc (only needed 1 time)
    • disconnect

    from then on:

    • connect a debugger, and now you can flash and debug with the default Pico Debug (Cortex-Debug) profile.
    • Cancel
    • Vote Up +5 Vote Down