Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 5 randomly reboots when powering an SSD over USB
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • +1 person also asked this people also asked this
  • Replies 17 replies
  • Answers 1 answer
  • Subscribers 701 subscribers
  • Views 922 views
  • Users 0 members are here
  • Locale or Language
Related

Raspberry Pi 5 randomly reboots when powering an SSD over USB

italo_ragazzo
italo_ragazzo 1 month ago

I’m using a Raspberry Pi 5 with an NVMe SSD connected through a USB 3 enclosure. The Pi works normally when the SSD is disconnected, but occasionally reboots when the SSD is under sustained read/write load.I purchased this one in Italy, so it might function differently.

The power supply is rated at 27W, and the issue seems more likely to happen when the CPU is also under load. Has anyone seen this with the Raspberry Pi 5, and would using a higher-rated USB-C supply or a powered USB hub be the recommended solution?

Thank you

best,
Salvatore B.
florist Italy
LTC

  • Sign in to reply
  • Cancel
Parents
  • veluv01
    0 veluv01 1 month ago

    I'm using the M.2 HAT+ to access the NVMe SSD (uses around 5W on R/W, running SLM's) , it works without any problem. If the power supply you're using doesn't have the 5V 5A profile, it's also a cause of the issue you're facing.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • cstanton
    0 cstanton 1 month ago in reply to veluv01
    veluv01 said:
    If the power supply you're using doesn't have the 5V 5A profile,

    Yes, thank you. This's the particular USB-PD profile that the Pi 5 is fussy about.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J 1 month ago in reply to cstanton

    I have the official PI5 supply.  Not at home for a few days so out of interest, is that good enough?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton 1 month ago in reply to Andrew J

    The official Pi 5 supply is exactly the correct one to use with the required USB-PD profile. It should be enough.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J 1 month ago in reply to cstanton

    Thanks.  Must be some other incompatibility then; I just couldn’t get to the bottom of it and because I was using it for HA, which I got thoroughly #}%&£@ off with, I gave up on it.  At least until I find another project suitable for the PI.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton 1 month ago in reply to Andrew J

    The problem might be with the enclosure, sometimes they do not expect higher power pull which has changed depending on what PCIe standard they expect/support.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chekov
    0 chekov 1 month ago in reply to cstanton

    Not sure if this will help get to the root of this particular problem, but they do discuss some methods to measure power consumption here:

    forums.raspberrypi.com/viewtopic.php

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • veluv01
    +1 veluv01 1 month ago in reply to cstanton

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Andrew J
    0 Andrew J 1 month ago in reply to veluv01

    When I get home I’ll dig it out.  I formatted it with HAOS but presumably the underlying config is common.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur 1 month ago in reply to cstanton

    I'm not that confident in all PI5 supplies being the same. The 5A sucker is much larger and weightier than the typical Pi power supply. I have a variety of PS kicking around and the size I noticed.

    I'm not saying you are wrong but PS for Pi's has always been contentious issue for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Andrew J
    0 Andrew J 1 month ago in reply to colporteur

    I've just checked what I have.  The case is an Argon One V3 m.2 https://argon40.com/en-gb/products/argon-one-v3-m-2-nvme-case.  The power supply is an official PI supply, P1224, rated 5.1V 5.0A (the 27W version.)  The power supply connects directly into the case through a USB C port.  I see there is a higher powered supply, 45W, but that is profiled at 9V 5A and offers the same 5.1V 5A profile so I can't see it making any difference.  I don't know that power is a problem in any case!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Andrew J
    0 Andrew J 1 month ago in reply to colporteur

    I've just checked what I have.  The case is an Argon One V3 m.2 https://argon40.com/en-gb/products/argon-one-v3-m-2-nvme-case.  The power supply is an official PI supply, P1224, rated 5.1V 5.0A (the 27W version.)  The power supply connects directly into the case through a USB C port.  I see there is a higher powered supply, 45W, but that is profiled at 9V 5A and offers the same 5.1V 5A profile so I can't see it making any difference.  I don't know that power is a problem in any case!