Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Putty shows error :connection refused but pinging is okay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 711 subscribers
  • Views 7724 views
  • Users 0 members are here
  • raspberry_pi
Related

Putty shows error :connection refused but pinging is okay

e14 Contributor
e14 Contributor over 10 years ago

Hey guys

 

I'm using windows 7 and im getting error from putty even after successfull pinging of pie

I also disabled the firewall but same error is displaying

I installed kikat on pie and also verify by using HDMI monitor but now i want to connect it to my pc using ssh connection

  • Sign in to reply
  • Cancel
Parents
  • rew
    rew over 10 years ago

    "connection refused" means that the pi is up and running but there is nobody waiting at the designated port (number 22 in this case).

     

    This would happen for example if the sshd program is not running. Try typing "sudo apt-get install ssh" on the pi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to rew

    Seems like a silly question to ask, so, since I am feeling a bit silly... Did you go into configurations and turn on the SSH component on the Pi?  It is located under the advanced features.  I like to use sudo raspi-config a little better than the GUI because I am really old, and like to feel the command line when I am working on computers.

     

    Jack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 10 years ago in reply to jack.chaney56

    I think the problem is he is running Android Kit Kat on his pi, as he semi stated in the OP. The normal debian/raspbian instructions are not going to work. A couple of people have given him direction in that aspect. I have no experience running android on the Pi, so I can't really help.

     

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mconners
    mconners over 10 years ago in reply to jack.chaney56

    I think the problem is he is running Android Kit Kat on his pi, as he semi stated in the OP. The normal debian/raspbian instructions are not going to work. A couple of people have given him direction in that aspect. I have no experience running android on the Pi, so I can't really help.

     

     

    Mike