Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Putty shows error :connection refused but pinging is okay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 711 subscribers
  • Views 7735 views
  • Users 0 members are here
  • raspberry_pi
Related

Putty shows error :connection refused but pinging is okay

e14 Contributor
e14 Contributor over 10 years ago

Hey guys

 

I'm using windows 7 and im getting error from putty even after successfull pinging of pie

I also disabled the firewall but same error is displaying

I installed kikat on pie and also verify by using HDMI monitor but now i want to connect it to my pc using ssh connection

  • Sign in to reply
  • Cancel
  • rew
    rew over 10 years ago

    "connection refused" means that the pi is up and running but there is nobody waiting at the designated port (number 22 in this case).

     

    This would happen for example if the sshd program is not running. Try typing "sudo apt-get install ssh" on the pi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago

    You need root aces on kitkat for How To Install SSH Server As Root On Android 4.4 KitKat | Megaleecher.Net

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to clem57

    On 11NOV15, I installed Putty on a Win10-PC. It was gotten at: bit.ly/win32putty. Worked good for me. Have a Rooted-B&N-Nook-HD+ that is running CM11 (Kit-Kat), have NOT tried Putty on this unit (Tablet).

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to uscdadnyc

    I forgot to mention that: A  RaspPi 1 B was the object-client of the Putty-client s/w on my Win10 PC. This RaspPi 1B was/is running "2015-02-18-wheezy-minibian" as the O/S.

    USCDADNYC  (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rew

    Hey roger 

    can u plz tell how can i write that code"sudo apt -get install ssh"

    coz im using window 7

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to rew

    I'm tottaly confused that how can i enable the ssh connection on pie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to rew

    Seems like a silly question to ask, so, since I am feeling a bit silly... Did you go into configurations and turn on the SSH component on the Pi?  It is located under the advanced features.  I like to use sudo raspi-config a little better than the GUI because I am really old, and like to feel the command line when I am working on computers.

     

    Jack.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to uscdadnyc

    Not a problem, Pi B1 or B+ work the same. Just run sudo raspi-config and select advanced features and SSH to activate SSH login.  You can also turn on the serial interface to make it completely operational from PuTTY.

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 10 years ago in reply to jack.chaney56

    I think the problem is he is running Android Kit Kat on his pi, as he semi stated in the OP. The normal debian/raspbian instructions are not going to work. A couple of people have given him direction in that aspect. I have no experience running android on the Pi, so I can't really help.

     

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Exactly Michael and as i told you guys im running the android os on pie so these rasbian commands are not going to work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>