Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Putty shows error :connection refused but pinging is okay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 711 subscribers
  • Views 7756 views
  • Users 0 members are here
  • raspberry_pi
Related

Putty shows error :connection refused but pinging is okay

e14 Contributor
e14 Contributor over 10 years ago

Hey guys

 

I'm using windows 7 and im getting error from putty even after successfull pinging of pie

I also disabled the firewall but same error is displaying

I installed kikat on pie and also verify by using HDMI monitor but now i want to connect it to my pc using ssh connection

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Exactly Michael and as i told you guys im running the android os on pie so these rasbian commands are not going to work

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to e14 Contributor

    Since Android is just a disguised form of Linux, you might try checking out http://www.linuxfromscratch.org and go to the beyond section for an instruction on installing SSH.

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to jack.chaney56

    This is a Teachable Moment:

    RS wrote>>...I'm using windows 7 and im getting error from putty even after successfull pinging of pie...

    -----

    then describes further his situation.

    ______

    then RS writes>>...I installed kikat on pie and also verify by using HDMI monitor but now i want to connect it to my pc using ssh connection

    USCDADNYC reply>> Ambiguous when taken in context w/ the first two sentences. Was the installation of KitKat an attempt to Troubleshoot the Problem? OR was it (in this case), an explanation of Initial H/W, S/W Set-up?. I'll say it again, Context is Everything.

    Perhaps it should have been worded "...I [had] installed Kitkat [initially] on pie...."?

    AAR this begs the following Q: why Android on RaspPi? There is more support for Raspbian/Minibian.

    And to JC: And Linux originated(?) from Unix (an AT&T product- my old old employer-many years ago)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to uscdadnyc

    Hey Edward can u plzz help  me to solve my problem rather than focussing on my context

     

    thanks  Jack for ur help  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to uscdadnyc

    Been off the grid for a few days... Now that I am back I can respond a bit to what has been said.  uscdadnyc has to follow his history, to see that UNIX was an AT&T product with extreme cost unless specifically for education, mostly because the US federal government had a tight grip preventing an OS (not viewed as part of communications) from being marketed.  While at university, Linus became enamored with UNIX and decided to develop a multi-threading kernel with the same features found in UNIX (everything is a file, and all IO is either serial or block) calling it Linux, and aims it to support GNU tools.  Lots of people liked it and helped out with making it successful.  Fast forward a bit, and UNIX gets sold to XENIX, XENIX sues Linux over infringement and looses (mostly because they stole stuff too). Sun rises and sets image.

     

    I know about all this stuff because I lived through most of it.  My dad worked at "The Labs" in the '60s, After we moved back to Michigan, dad drove Scott McNealy to Scout meetings. My brother and I were in band with him and Barry (his brother).  I was on the project where the issues with XENIX might have started (lawyers were trying to make a bad case for more money).

     

    Android is a Linux extension (because UNIX wasn't available). rockko  Android on RasPi is a good example of why RasPi was created in the first place, to provide a great platform for experimentation.

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to jack.chaney56

    To JC: Woulda Coulda Shoulda. Nice to go down Memory Lane singing Bruce Springsteen's "Glory Days". I was at AT&T b/f Divestiture (1984?). It was a different world w/ the then Technical/Legal/Regulation Environment. Back then I was an Engineer/IT person. Now I am a (US) Patent Atty, who can look retrospectively at Decisions w/ a knowledge of Legal/Business factors that I did not know then. Woulda Coulda Shoulda. BTW didn't Novell(sp?) also own Unix at one time?

    AAR back to to situation at Hand. I ask AGAIN why Android on the RaspPi H/W Platform? Why re-invent the Wheel? If Raspbian is sufficient?

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to uscdadnyc

    Sometimes, it is necessary for people to learn from their own mistakes. Kind of the "can lead a horse to water" situation.  I agree completely, about why reinvent the wheel here, and Raspbian would get to the solution quicker.  But then, why replace relays with digital switches.  Occasionally, a different answer provides a better solution, it can also cause a spectacular failure, but we never know unless someone is willing to take the chance.

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to uscdadnyc

    Sometimes, it is necessary for people to learn from their own mistakes. Kind of the "can lead a horse to water" situation.  I agree completely, about why reinvent the wheel here, and Raspbian would get to the solution quicker.  But then, why replace relays with digital switches.  Occasionally, a different answer provides a better solution, it can also cause a spectacular failure, but we never know unless someone is willing to take the chance.

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • uscdadnyc
    uscdadnyc over 10 years ago in reply to jack.chaney56

    It is about ROI (Return On Investment), the original Poster has a different view of ROI as opposed to our view(s) of ROI . Raspbian vs. Android, on RaspPi. Blast from the Past: AT&T was in a Regulatory/Anti-Trust Environment, that possibly hindered original Unix Language development/distribution. Present-Day WRT Essential Patents (for inter-operative-ability) it is now FRAND (Fair Reasonable, And Non-Discriminatory) licensing of these SEP's

    (Standard Essential Patents). Different Time. Different Place. Different Environment.

    But Again I ask? Why Android on RaspPi H/W Platform?

    USCDADNYC (NY NY USA)