Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum LCD
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 708 subscribers
  • Views 5298 views
  • Users 0 members are here
  • raspberry_pi
Related

LCD

Workshopshed
Workshopshed over 9 years ago

I got myself a 7inch LCD cheap on Ebay thinking that it had a HDMI connector on it but it actually only has a ribbon connector which is described as a "LCD Interface 24-bit parallel".

 

7" Capacitive Touch 800*480 TFT TTL LCD Screen Display Module For HDMI | eBay

 

LCD Interface Definition

 

PIN NO. SYMBOL DESCRIPTION Type FUNCTION

 

1 VLED- Backlight negative input Backlight negative, connects to GND or PWM control

2 VLED+ Backlight Positive input Backlight Positive, 5V typical

3 GND Ground input Ground

4 VCC Power supply input Power supply, 3.3V

5 R0 Data lines input Red layer data lines

6 R1

7 R2

8 R3

9 R4

10 R5

11 R6

 

I was wondering if there was some kind of module I could get that would convert the HDMI signal back to the LCD signal. Any suggestions what to search for?

image

  • Sign in to reply
  • Cancel
Parents
  • the-dubster
    the-dubster over 9 years ago

    If it does turn out to be LVDS . . .

     

     

     

                   Righto, here is an eBay.co.uk link to a board (and screen - which I know you don't need).

     

                   Included in the listing is a bunch of compatible displays and - more helpfully maybe - they offer a match-up service to your screen.

     

                   Could be a starting point.

     

                   HDMI VGA DVI 50PIN TTL LVDS Controller Board+8inch LCD Display for Raspberry PI | eBay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to the-dubster

    I did some counting and the cable has definately got 50 pins. Its too fine pitched but also too wide to fit into the DPI connector.

    The connector that goes from the LCD to the board is labelled as 7dd1+1 fpc and the front of the board LCD070. The resolution is 800 * 480 (Pixel).

     

    The possible candidate driver I found was this one which uses a VS-TY2662-V1 chip described as coping with 7 to 10 inch boards

     

    New SainSmart 10.1 Inch TFT LCD Monitor Driver Board HDMI VGA for Raspberry Pi | eBay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • the-dubster
    the-dubster over 9 years ago in reply to Workshopshed

    Spotted that one (and others) too with my eBay wanderings, < £15 GBP isn't bad either.

     

     

    And the board has some startling similarities to my link . . . .

     

     

    Also, by the time it arrives we'll have all forgotten about this conversation too!! imageimageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to the-dubster

    If all these comment(ers) are using this situation as a Teachable-Moment, then go right ahead. BUT if the object is to get a working 7" touchscreen for a RaspPi 3 B, then I would CUT my losses ($16.12 pounds = $15.42 USD). Get the Official RaspPi 7" Touch Screen (`$70.00 USD). I read the specs at that URL for the eBay entry for this $16.12 pounds, and it seems incomplete at Best. My knowledge dates back to my 73' BSEE (Syracuse Univ. NY USA), so maybe I am not up to speed. It maybe worth your trouble, It won't be worth my time and money. It is up to you. Like people say: "You can pay me Now or you can Pay me Later".

    USCDADNYC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • the-dubster
    the-dubster over 9 years ago in reply to uscdadnyc

    I have an old HP laptop screen and will be doing the same, if I can get it up and running for under £17 then I will.

     

    I sure as heck can't afford to splash out £65 GBP for the smaller official screen, of a far lower resolution than the FREE item I have - (15.4-inch wide-screen display; 1,280x800).

     

    I don't like the word 'can't' - it needs changing to 'haven't figured out how to yet'!

     

    (except for striking a match on jelly - you really can't strike a match on jelly)!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to uscdadnyc

    Hi Edward, yes cutting my losses was definitely an option. I've seen Makibes 7in screens with a proper HDMI connector for around £40 and that definitely seems a better option that buying separate boards that might not work together. Key lesson learnt is to re-read those EBay listing as you might not be getting what you thought.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to Workshopshed

    Here is what I did. Combined RaspPi 3 B, Smartpi Touch Case and the official 7" touch screen in one package w/ Options. image

    Option One: Attached a Bitscope onto the Lego Nobs that are on the SmartPi Touch Case:

    image

    Option Two: You will need a "Dremel Tool" to cut the Plastic Backside of the SmartPi Case to EXPOSE the HDMI Connector

    image

    ALL Parts (when in the U.S.A.) are available thru either/or MCM Electronics or element14.

    To complete the above Picture, you will need a "Dremel" Tool to cutaway at the Plastic. AND buy a "TOP"

    Right-Angle HDMI Adapter.

    image

    Works Great. Now if only my RaspPi Zero would work.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • uscdadnyc
    uscdadnyc over 9 years ago in reply to Workshopshed

    Here is what I did. Combined RaspPi 3 B, Smartpi Touch Case and the official 7" touch screen in one package w/ Options. image

    Option One: Attached a Bitscope onto the Lego Nobs that are on the SmartPi Touch Case:

    image

    Option Two: You will need a "Dremel Tool" to cut the Plastic Backside of the SmartPi Case to EXPOSE the HDMI Connector

    image

    ALL Parts (when in the U.S.A.) are available thru either/or MCM Electronics or element14.

    To complete the above Picture, you will need a "Dremel" Tool to cutaway at the Plastic. AND buy a "TOP"

    Right-Angle HDMI Adapter.

    image

    Works Great. Now if only my RaspPi Zero would work.

    USCDADNYC (NY NY USA)