Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 705 subscribers
  • Views 894 views
  • Users 0 members are here
  • raspberry_pi
Related

Pi Code

samirjisan
samirjisan over 9 years ago

I want to run DC motors with raspberry pi 3 using relay can any one please give me the code ?

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    The code looks like it is for a full H bridge driver, not a couple of relays. The code is using 4 outputs in total and you only have two connected in your diagram

     

    Also in the diagram it looks like you have pin 8 connected to ground of the relay board. It should be pin6, 9 or 14.

    Image result for pi pinout

    Lastly it looks like you're powering the relay board from the 5V of the PI (Pin 2). Is this just for the opto isolators or is it powering the relays as well, if so this may be too much noise / load for the PI. I can't see what is behind the wires to be sure.

     

    The basic code methodology looks correct as a basis to work from, but you need to change the various functions (Forward, Back, Left, Right, Pivot etc) to drive the relays instead of the H Bridge seems it is coded for

    If you can show how your wiring the motor to the relays, we can help you move forward.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    The code looks like it is for a full H bridge driver, not a couple of relays. The code is using 4 outputs in total and you only have two connected in your diagram

     

    Also in the diagram it looks like you have pin 8 connected to ground of the relay board. It should be pin6, 9 or 14.

    Image result for pi pinout

    Lastly it looks like you're powering the relay board from the 5V of the PI (Pin 2). Is this just for the opto isolators or is it powering the relays as well, if so this may be too much noise / load for the PI. I can't see what is behind the wires to be sure.

     

    The basic code methodology looks correct as a basis to work from, but you need to change the various functions (Forward, Back, Left, Right, Pivot etc) to drive the relays instead of the H Bridge seems it is coded for

    If you can show how your wiring the motor to the relays, we can help you move forward.