Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 705 subscribers
  • Views 893 views
  • Users 0 members are here
  • raspberry_pi
Related

Pi Code

samirjisan
samirjisan over 9 years ago

I want to run DC motors with raspberry pi 3 using relay can any one please give me the code ?

  • Sign in to reply
  • Cancel
  • ajens23
    ajens23 over 9 years ago

    Hi Samir,

     

    Do you want us to cook and eat your breakfast for you too?

     

    You can get better responses by offering more information and perhaps doing a quick Google search before posting.

     

    At a minimum you will need to amplify the 3.3V GPIO pin to whatever your relay requires a 2n2222 transistor or equivalent should do the trick

    but you may need an external power supply.

     

    How big of a motor, what voltage? Current draw?

    What language are you programming in?

    What PI do you have?

    How much electronics knowledge do you have?

    What is your ultimate goal.....?

    Have you tried any of the PI tutorial sites?

    https://www.engadget.com/2012/09/04/raspberry-pi-getting-started-guide-how-to/

     

    https://business.tutsplus.com/tutorials/controlling-dc-motors-using-python-with-a-raspberry-pi--cms-20051

     

    The people on here want to help, but the same old low content questions get old fast.

     

    Al

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • samirjisan
    samirjisan over 9 years ago in reply to ajens23

    imageimage

     

     

     

    I use 12V power source for relay and this is not the connection. I want to know is the code is correct?  The code I use given bellow.

     

     

     

    import RPi.GPIO as gpio

    import time

    import sys

    import Tkinter as tk

     

    def init():

        gpio.setmode(gpio.BOARD)

        gpio.setup(7, gpio.OUT)

        gpio.setup(11, gpio.OUT)

        gpio.setup(13, gpio.OUT)

        gpio.setup(15, gpio.OUT)

     

    def forward(tf):

        gpio.output(7, gpio.HIGH)

        gpio.output(11, gpio.LOW)

        gpio.output(13, gpio.HIGH)

        gpio.output(15, gpio.LOW)

        time.sleep(tf)

        gpio.cleanup()

     

    def reverse(tf):

        gpio.output(7, gpio.LOW)

        gpio.output(11, gpio.HIGH)

        gpio.output(13, gpio.LOW)

        gpio.output(15, gpio.HIGH)

        time.sleep(tf)

        gpio.cleanup()

     

    def turn_left(tf):

        gpio.setup(7, True)

        gpio.setup(11, True)

        gpio.setup(13, True)

        gpio.setup(15, False)

        time.sleep(tf)

        gpio.cleanup()

     

    def turn_right(tf):

        gpio.setup(7, False)

        gpio.setup(11, True)

        gpio.setup(13, False)

        gpio.setup(15, False)

        time.sleep(tf)

        gpio.cleanup()

     

    def pivot_left(tf):

        gpio.setup(7, True)

        gpio.setup(11, False)

        gpio.setup(13, True)

        gpio.setup(15, False)

        time.sleep(tf)

        gpio.cleanup()

     

    def pivot_right(tf):

        gpio.setup(7, False)

        gpio.setup(11, True)

        gpio.setup(13, False)

        gpio.setup(15, True)

        time.sleep(tf)

        gpio.cleanup()

     

    def key_input(event):

        init()

        print 'key:', event.char

        key_press = event.char

        sleep_time = 0.001

     

        if key_press.lower() =='w':

            forward(sleep_time)

        elif key_press.lower() =='s':

            reverse(sleep_time)

        elif key_press.lower() =='a':

            turn_left(sleep_time)

        elif key_press.lower() =='d':

            turn_right(sleep_time)

        elif key_press.lower() =='q':

            pivot_left(sleep_time)

        elif key_press.lower() =='e':

            pivot_right(sleep_time)

        else :

            print "try again "

     

     

    command = tk.Tk()

    command.bind('<KeyPress>', key_input)

    command.mainloop()

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ajens23
    ajens23 over 9 years ago in reply to samirjisan

    Hi Samir,

     

    That is a much better post, thank you.

     

    Sorry I don't code for the PI myself, but it looks wonky (anyone else?)

    Why are forward and reverse coded differently than  the turns and pivots?

     

    Are you using 2 motors or 4?

    Are those solid state relays or mechanical?

    Why does it look like your are running the GPIO pins as if you had direct motor hookup; when you are using a relay board?

     

     

    So you have control of IO pins, and your relay has a power amplifier already.

    What are you using as a power supply for the motor? Those window motors tend to draw a lot of amps. I have a slightly larger one that will pull up to 20 amps locked rotor.

    If you are going to drive 4 of them you will need a pretty stout power supply. 

     

    Take a moment and walk me through your code and what you are expecting it to do.

     

    Thanks,

     

    Al

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago

    The code looks like it is for a full H bridge driver, not a couple of relays. The code is using 4 outputs in total and you only have two connected in your diagram

     

    Also in the diagram it looks like you have pin 8 connected to ground of the relay board. It should be pin6, 9 or 14.

    Image result for pi pinout

    Lastly it looks like you're powering the relay board from the 5V of the PI (Pin 2). Is this just for the opto isolators or is it powering the relays as well, if so this may be too much noise / load for the PI. I can't see what is behind the wires to be sure.

     

    The basic code methodology looks correct as a basis to work from, but you need to change the various functions (Forward, Back, Left, Right, Pivot etc) to drive the relays instead of the H Bridge seems it is coded for

    If you can show how your wiring the motor to the relays, we can help you move forward.