Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi killer? ASUS - 90MB0QY1-M0EAY0
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 711 subscribers
  • Views 5362 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry pi killer? ASUS - 90MB0QY1-M0EAY0

coops375
coops375 over 9 years ago

ASUS  90MB0QY1-M0EAY0  Tinker Board

 

image

 

image source: Asus Tinker Board is designed to trump the Raspberry Pi 3 - Gadgets - News - HEXUS.net

  • Sign in to reply
  • Cancel
Parents
  • bwelsby
    bwelsby over 9 years ago

    I have had the Tinker Board for two days now but no sign of the OS for it yet, not impressed and starting to loose interest.

    Has the hardware been released too soon?

     

    A rather expensive brick image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 9 years ago in reply to bwelsby

    Kodi 14.2 Linux Ported to Rockchip RK3288 with VPU Hardware Decoding

     

    something to play with in the meantime?

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 9 years ago in reply to mconners

    Now bwelsby has something to do for the next 2 days.

     

    Mike

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 9 years ago in reply to mconners

    mconners 2 days and more THANK YOU!!! I had tried searching Asus but didn't find anything and  CPC were supposed to be sending me the link when it became available.

    Just running the debian distro...  it's fast image

     

    Thanks again,

    Brian

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 9 years ago in reply to bwelsby

    Good to hear bwelsby Look forward to your review.

     

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 9 years ago in reply to mconners

    BTW, I googled for Rockchip RK3288 Linux Distro to find all the stuff I found.

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 9 years ago in reply to bwelsby

    Just running the debian distro... it's fast

     

    It must have been fast to setup as well, that didn't take you long.

     

    Mike

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 9 years ago in reply to mconners

    Michael Conners wrote:

     

    Just running the debian distro... it's fast

     

    It must have been fast to setup as well, that didn't take you long.

     

    Mike

    Fast D/L  on Virginmedia Broadband image

    Quick to write on a 16G Sandisk Ultra uSD  using USB3.0 adapter. (2.1Gbyte image)

    Plugged in powered up and around 18 seconds to full boot into gui.

     

    Brian

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 9 years ago in reply to bwelsby

    Nice!!!

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mconners
    mconners over 9 years ago in reply to bwelsby

    did you pull down any of the API docs they had for the GPIO, looks like they had both C and Python?

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 9 years ago in reply to mconners

    I did yes but not had time to digest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to mconners

    The (C) GPIO looks like very crude hack from Pi based stuff.

     

    Have you found any I2C examples/library yet ?

     

    I need to test something with I2C and I thought this might be  a good way to kill multiple birds with one Rock !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 9 years ago in reply to mconners

    The (C) GPIO looks like very crude hack from Pi based stuff.

     

    Have you found any I2C examples/library yet ?

     

    I need to test something with I2C and I thought this might be  a good way to kill multiple birds with one Rock !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rew
    rew over 9 years ago in reply to michaelkellett

    For I2C, I expect that there is a kernel driver, and that you can use the standard I2C tools like i2cdetect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to rew

    Thanks Roger, I've never used any of these tiny Linux thingies so I'm not sure where to look for stuff.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to michaelkellett

    Hi Michael,

    The problem is, most documentation/tutorials online are often written just for one SBC, e.g. Raspberry Pi or BBB, and do not mention that its likely the code will work on all platforms. It is particularly

    irritating when APIs even have the word 'pi' in the function names, when in reality they may work on other platforms too. Maybe it is information hiding, or maybe the developers of the documentation/tutorials didn't know.

    Anyway, for I2C, the easiest way is to check in the /dev folder, if there is an entry called i2c-1 or i2c-2 or something. If so, then one of these will provide driver based access to the I2C pins on the connector, and the

    access should work in any language with any library provided it uses the driver (which isn't often mentioned anywhere in the documentation but could be visible in the source code).

    I don't know which language you wished to use, but (for example) for C programming the access is via the 'ioctl' function. Just to make it slightly higher-level (but still fairly low-level) I wrote some wrapper functions to

    have an easier-to-understand API for I2C. It is available here, in the files i2cfunc.h and i2cfunc.c :

    https://github.com/shabaz123/lcd3

    (to see how it is used, the file lcd3-test.c could be examined). In short, to use I2C with this wrapper library, these are some of the functions that are available:

    i2c_open

    i2c_write

    i2c_read

    i2c_close

    (the full list and short documentation is in the i2cfunc.h file, it is mostly self-explanatory to be honest).

    It doesn't handle everything but handles things like the repeated start which some online tutorials etc miss.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to shabaz

    Thanks for the info - I've just ordered a board but it'll be a while until I can play with it.

     

    I'm keen on the 1GB  Ethernet done properly on this board so I have some hope of it being useful.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 9 years ago in reply to rew

    Roger Wolff wrote:

     

    For I2C, I expect that there is a kernel driver, and that you can use the standard I2C tools like i2cdetect.

    Yep the i2c is all working as far as I can tell.  I tried the RPi camera (latest version) and got that working.

    I also tried the RPi Touchscreen display but that isn't working ... yet to  determine why but it does show up on the i2c bus.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 9 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    Thanks for the info - I've just ordered a board but it'll be a while until I can play with it.

     

    I'm keen on the 1GB Ethernet done properly on this board so I have some hope of it being useful.

     

    MK

    The big points for me are the 1G Ethernet, 2G memory and the ability to add a decent WiFi antenna. I am not too bothered about the 4k video at the moment.

     

    Brian