Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Your Breakdown of Raspberry Pi Customization
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 68 replies
  • Subscribers 720 subscribers
  • Views 8167 views
  • Users 0 members are here
  • customized pi
  • customized_pi
  • customization_service
  • customization
  • customisation
  • customization service
  • raspberry pi
  • raspberry-pi
  • raspberrypi
  • customised pi
  • customisation service
Related

Your Breakdown of Raspberry Pi Customization

spannerspencer
spannerspencer over 10 years ago

You might have just seen the official joint announcement from the Raspberry Pi Foundation and element14 regarding an exclusive new customization service for the Raspberry Pi, and we'd love to hear your thoughts on the subject.

 

Bulk Customization Services

The facts are these:

 

You can now open a dialogue with element14 about creating a Raspberry Pi that's tailored to specific needs, on orders of 3,000 units or more. You can reconfigure the board, add new functionality, add or remove features, change the memory configuration; pretty much anything besides tinkering with the GPU and related software. A full breakdown of the service can be found here: Raspberry Pi Customization Service

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cooking Up a Custom Raspberry Pi

Clearly this is aimed squarely at OEM manufacturers, suppliers and bigger companies due to the minimum order quantity, but such places are still populated by engineers and makers who'd be the ones that determine just what a customized Raspberry Pi would require for specific needs.image

 

So we thought it'd be valuable to get the element14 community's opinion on this new service.

 

Will companies find a lot of use for it, and what might they need a custom Pi for?

 

Which kinds of customization are likely to be the most popular? Expansion of the device, or minimization?

 

Give us your predictions on the future of element14's Raspberry Pi Customization Service below, and who knows how it might evolve.

  • Sign in to reply
  • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to rew

    Woldff, I agree with you that probably they won't change the base PCB motherboard. First of all because it is too risky.

     

    Instead, also adding components is not more difficult than remove. As a matter of fact I think they pose limits that we don't now yet, that dives the opportunity to have 3000+ devices for example including a LCD, with a different connector, with a specific board presoldered on it and so on.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to balearicdynamics

    Enrico Miglino wrote:

     

    Woldff, I agree with you that probably they won't change the base PCB motherboard. First of all because it is too risky.

    There are two statements in the linked discussion that make me think otherwise:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    I'd like to see a ram socket like a laptop uses DDR3

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • poordom
    poordom over 10 years ago in reply to e14 Contributor

    Enrico,


    I love the items you consider for customisation, simply because the items mentioned could be used as part of a Home Automation customisation.


    I would add to your list a built on Z-Wave communication module.


    Dom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi !

     

    Did you ever think about building such the inexpensive , very small computer  ( carefully sealed ) for marine purpose ?

    Price of the product is here a real factor. Laptops consume a lot f power and are not lasting enough to withstand harsh sea environment conditions.

    Friend of mine killed 5 laptops during one and half year sailing trip.

    Greetings

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 10 years ago

    Sounds like an opportunity for hardware device makers to embed RPi into more products.

     

    I agree with much of the conversation above, that it ultimately all depends on pricing.

     

    Can you give us an idea of pricing?

     

    Take Frederick's idea as an example, as that seems representative of a very reasonable request a company might make:

    Frederick Vandenbosch wrote:

     

    A customisation I'd like to see is a low(er) profile RPi2:

    • 2x 1 USB port iso 2x 2ports
    • GPIO pins at 90° angle
    • no ethernet port

    (In short, a Raspberry Pi 2 Model A ...)

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rdibened
    rdibened over 10 years ago

    My biggest problem with my Raspberry Pi's are as follows.  I have two model "B" and one Pi-2.  As I run a junk call blocker, a OpenVPN server, Motion Detection surveillance software, and a Weather Station on my Pi's.  They are on 24/7 causing corruption of the SD cards after several months.  I plan to use a laptop drive connected via USB though a powered hub to run the second partition that holds the linux system.  This is a relatively simple hack and would add about 60ma of power consumption.  I would love to see either an add on or an re-designed Pi with a build in "Low" power hard drive or a long lasting SSD.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • pixster
    pixster over 10 years ago

    WHERE IS USB 3.0?    Change the controller chip so this will be possible.

    I'm going to keep bitching about this until this happens!! image

     

    I have ALL USB 3.0 device, and their dogging along since you wont incorporate this change!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to gadget.iom

    Not so sure, Paul image

     

    They speak of Re-configure, that means leave untouched (or may mean so) and incorporating that means add parts over the PCB as well as change the PCB. But maybe they accept also PCB modifications ... It's only specualtion image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to balearicdynamics

    The video of the press conference seemed fairly clear: They will redesign the board as needed to add whatever functionality the customer desires. That's why its a minimum of 3000 units.

     

    I expect that there will be some fairly radical re-designs but the chances are that we will never see them as they will be propriety designs, kept exclusively for that customer.

     

    @ Ted Mieske: That's not on the cards, all redesigns will feature the existing range of Pi SOCs.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>