Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Phone Call On PC
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 705 subscribers
  • Views 624 views
  • Users 0 members are here
  • raspberry_pi
Related

Phone Call On PC

nicolaoscon96
nicolaoscon96 over 9 years ago

Hello Again,

 

As I mention in other posts I am working on  a home automation project and I want to make it like a personal assistance as JARVIS is in IronMan Movies.All the coding and circuit boards are mostly design by me except the Raspberry Pi and The arduino image. So as the title say i want to write a code for my PC software (i wrote mostly of the main software in Visual Basic 2010) that it will be able to receive incoming calls and also the caller ID.Is there any way to achieve that? I searched the internet but i can't find any similar and if this is possible am i going to need to install on my pc a 56k dial up modem?

 

Any ideas are welcome

Thanks a lot nicolaoscon96

  • Sign in to reply
  • Cancel
Parents
  • geralds
    geralds over 9 years ago

    Hi,

     

    As explained by others, this is an old technique.
    We have used a long-range modem with 2.4kbd.
    The call ID must be enabled by the service provider, then the ID can also be received.
    The transmitter, the remote system, has inserted the ID in the software and sends it together with the status protocol.
    The receiver, the stationary system, now identifies with the ID, which transmitter transmits its states.
    This data is then evaluated in the software of the plant.

    Today, the Internet is normally used with the WAN-LAN interface; Gateway, or Router.
    With the analog modem the data with this protocol are used.
    The hardware of the local system can also have a LAN modem connection.
    Then you have to connect the modem to a virtual LAN-COM port.
    This virtual COM port can be easily set up in the operating system.

     


    image
    All necessary programs for the connection are available in the operating system and the application of the local system accesses these interfaces.

    With your Visual Studio you can write your own application software.

     

    Best Regards,

    Gerald

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 9 years ago

    Hi,

     

    As explained by others, this is an old technique.
    We have used a long-range modem with 2.4kbd.
    The call ID must be enabled by the service provider, then the ID can also be received.
    The transmitter, the remote system, has inserted the ID in the software and sends it together with the status protocol.
    The receiver, the stationary system, now identifies with the ID, which transmitter transmits its states.
    This data is then evaluated in the software of the plant.

    Today, the Internet is normally used with the WAN-LAN interface; Gateway, or Router.
    With the analog modem the data with this protocol are used.
    The hardware of the local system can also have a LAN modem connection.
    Then you have to connect the modem to a virtual LAN-COM port.
    This virtual COM port can be easily set up in the operating system.

     


    image
    All necessary programs for the connection are available in the operating system and the application of the local system accesses these interfaces.

    With your Visual Studio you can write your own application software.

     

    Best Regards,

    Gerald