Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Case/Material to Protect Raspberry Pi 3b and Zero in hostile environment
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 708 subscribers
  • Views 3348 views
  • Users 0 members are here
  • raspberry_pi
  • raspberry pi
Related

Case/Material to Protect Raspberry Pi 3b and Zero in hostile environment

skeevestevens
skeevestevens over 8 years ago

Hi all,

 

I'm working on a project at the moment where the Raspberry Pi 3b and Zero (both in the same box doing different functions) are in a hostile environment.

 

The best example would be... imagine it was attached to a small shipping container where it is constantly picked up by a forklift, put down violently, dropped, banged into, etc.

 

There are a lot of variables, but the only one I am worried about at the moment is the Pi's themselves in the box that will be attached.

 

What is the best way to mount them, or material to surround them with that would best protect them from being destroyed quickly?

 

Thanks for the help guys.

 

...Skeeve

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB over 8 years ago

    Hi Skeeve.

     

    Make sure that all of your components are securely fastened.

    If there is any flexibility at all, you will get things breaking off due to the moment of inertial. Even small things.

    If you can, seal everything in a podding compound.

    Try wrapping the case with gel to get as much shock absorption as you can.

    If any part of the insides can move, they will probably break off after repeated drops.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 8 years ago in reply to DAB

    If there is any flexibility at all, you will get things breaking off due to the moment of inertial. Even small things.

    If you have a rigid box and drop it from 10cm, and the floor does not give in so that the box stops inside a stopping distance of about 0.1mm, then the G-force experienced by the box (and everything rigidly attached) is going to be 1000G's. Having say 1cm of "cushion" is going to reduce the G-loads enormously.

     

    So for stuff that is shipped and might be dropped once, they use Styrofoam. It crushes and absorbs energy when under a high load. For stuff like "hard disks" inside a "ruggedized" enclosure, you see rubber used as a cushioning material.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rew
    rew over 8 years ago in reply to DAB

    If there is any flexibility at all, you will get things breaking off due to the moment of inertial. Even small things.

    If you have a rigid box and drop it from 10cm, and the floor does not give in so that the box stops inside a stopping distance of about 0.1mm, then the G-force experienced by the box (and everything rigidly attached) is going to be 1000G's. Having say 1cm of "cushion" is going to reduce the G-loads enormously.

     

    So for stuff that is shipped and might be dropped once, they use Styrofoam. It crushes and absorbs energy when under a high load. For stuff like "hard disks" inside a "ruggedized" enclosure, you see rubber used as a cushioning material.