Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Case/Material to Protect Raspberry Pi 3b and Zero in hostile environment
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 708 subscribers
  • Views 3329 views
  • Users 0 members are here
  • raspberry_pi
  • raspberry pi
Related

Case/Material to Protect Raspberry Pi 3b and Zero in hostile environment

skeevestevens
skeevestevens over 8 years ago

Hi all,

 

I'm working on a project at the moment where the Raspberry Pi 3b and Zero (both in the same box doing different functions) are in a hostile environment.

 

The best example would be... imagine it was attached to a small shipping container where it is constantly picked up by a forklift, put down violently, dropped, banged into, etc.

 

There are a lot of variables, but the only one I am worried about at the moment is the Pi's themselves in the box that will be attached.

 

What is the best way to mount them, or material to surround them with that would best protect them from being destroyed quickly?

 

Thanks for the help guys.

 

...Skeeve

  • Sign in to reply
  • Cancel
  • DAB
    DAB over 8 years ago in reply to skeevestevens

    The more cushioning you can put around the boards the better.

     

    I agree with the others about very ridged mounting.  Keep all components firmly attached with hard points.

    Adding gel or padding helps to dissipate energy and keep the components from flexing or moving too much.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • skeevestevens
    skeevestevens over 8 years ago in reply to DAB

    I'm confused.

     

    Rigid mounting + cushioning seems the opposite of each other.

     

    I wasn't planning on having the unit just floating and bouncing around.

     

    I was thinking more along the lines of suspension.

     

    I have a space of 30mm to work within... and can compress top and bottom.

    I also need to make sure it doesn't overheat... so I was thinking Gel

    either side - the kind you might have in an arm/wrist rest.

     

    ...Skeeve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago

    Ben Heck did an episode on a data logger to investigate baggage handling:

    Episode 232: Ben Heck’s Luggage Detective Episode

    A test using something like this may give you some real world data to understand what you re up against.

     

    I've seen a number of delicate electronic items shipped in a 'trampoline sandwich'. Basically the equipment sits trapped between two sheets of rubbery plastic type material which is then supported in a cardboard frame inside the box (and then in some cases the box is an inner box suspended inside an outer box by foam cushioning).

     

    This is perhaps similar to the techniques used in audio where a microphone is suspended in a shock mount using a bungee cord arrangement to provide mechanical noise isolation.

    https://upload.wikimedia.org/wikipedia/commons/b/b8/AKG_Perception_120_USB_condenser_microphone_with_SH_100_shock_mount.…

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
<