Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Case/Material to Protect Raspberry Pi 3b and Zero in hostile environment
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 708 subscribers
  • Views 3328 views
  • Users 0 members are here
  • raspberry_pi
  • raspberry pi
Related

Case/Material to Protect Raspberry Pi 3b and Zero in hostile environment

skeevestevens
skeevestevens over 8 years ago

Hi all,

 

I'm working on a project at the moment where the Raspberry Pi 3b and Zero (both in the same box doing different functions) are in a hostile environment.

 

The best example would be... imagine it was attached to a small shipping container where it is constantly picked up by a forklift, put down violently, dropped, banged into, etc.

 

There are a lot of variables, but the only one I am worried about at the moment is the Pi's themselves in the box that will be attached.

 

What is the best way to mount them, or material to surround them with that would best protect them from being destroyed quickly?

 

Thanks for the help guys.

 

...Skeeve

  • Sign in to reply
  • Cancel
  • genebren
    genebren over 8 years ago

    Hi Skeeve,

     

    I have not used any of these cases, but I thought that this might be of help:

    https://www.makeuseof.com/tag/5-ways-to-ruggedise-your-raspberry-pi/

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago

    Polycarbonate, cast acrylic, PETE, ABS, or similar materials are good choices for enclosures.

    With proper tools anything can be constructed from design.

    Element 14 has a large selection of enclosures and custom  services as well.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 8 years ago

    Hi Skeeve.

     

    Make sure that all of your components are securely fastened.

    If there is any flexibility at all, you will get things breaking off due to the moment of inertial. Even small things.

    If you can, seal everything in a podding compound.

    Try wrapping the case with gel to get as much shock absorption as you can.

    If any part of the insides can move, they will probably break off after repeated drops.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 8 years ago

    Strong cases made of polycarbonate, aluminum or die-cast metal are a good start, but the case also should be mounted on shock mounts or foam to minimize shock loading. And make sure all cables have adequate strain relief.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago

    Materials with UV protectant, anti-static/esd safe, and hydrophobic properties are optimal.

    Many manufactured enclosures can be found with waterproof/waterproof silicone seals that can protect your design from environmental factors such as moisture and debris. A conformal coating can provide extra protection as well. 

    Protection from EMI should also be considered.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ninjatrent
    ninjatrent over 8 years ago in reply to ninjatrent

    correction, waterproof/ weather resistant image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skeevestevens
    skeevestevens over 8 years ago in reply to DAB

    Hmm. I thought them being anchored would be worse.

     

    If they were floating on some kind of gel base, and able to move a

    little... kind of like suspension on a car... when it is tight, it is very

    rough.

     

     

     

     

    ...Skeeve

     

     

    --

     

    Skeeve Stevens - Genius As A Service

     

    Email: skeeve@niisch.com / Cell: +61(0)414 753 383

    Skype: skeeve ; Twitter: @SkeeveStevens

     

     

    "You inspire us to inspire you"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • skeevestevens
    skeevestevens over 8 years ago in reply to skeevestevens

    Sorry about the email signature... I assumed it would strip it when replying via email.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 8 years ago in reply to DAB

    If there is any flexibility at all, you will get things breaking off due to the moment of inertial. Even small things.

    If you have a rigid box and drop it from 10cm, and the floor does not give in so that the box stops inside a stopping distance of about 0.1mm, then the G-force experienced by the box (and everything rigidly attached) is going to be 1000G's. Having say 1cm of "cushion" is going to reduce the G-loads enormously.

     

    So for stuff that is shipped and might be dropped once, they use Styrofoam. It crushes and absorbs energy when under a high load. For stuff like "hard disks" inside a "ruggedized" enclosure, you see rubber used as a cushioning material.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 8 years ago

    Skeeve,

     

    For a diy approach you could shock mount the RPi3 and PiZero to a small metal plate (eg aluminium). Use 2.5mm machine screws, rubber tap washers/grommets, suitable metal washers and light duty compression springs. You'd have a mounting that had some dampening in the plane parallel to your pcb as well as perpendicular. Adjusting the nuts (suitably threadlocked) to give just the right amount of restraint.

     

    Like this:

    image

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>