Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Deep Neural Network Benchmark with Raspberry Pi 2, 3 and 3+
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 703 subscribers
  • Views 4210 views
  • Users 0 members are here
  • neural_network
  • neural network
  • raspberry pi benchmark
  • rasberry_pi_3_b_plus
  • opencv
  • raspberry_pi
  • caffe
  • dnn
  • power consumption
  • benchmark
  • power efficiency
Related

Deep Neural Network Benchmark with Raspberry Pi 2, 3 and 3+

bernhardmayer
bernhardmayer over 8 years ago

With this benchmark I want to show you how the different versions of the Raspberry Pi perform with deep neural networks and how much power they consume. I am runing the network with OpenCV. The tested Raspberry Pi models are Raspberry Pi 2, Raspberry Pi 3 and Raspberry Pi 3 Model B+.

 

OpenCV installation

 

Reasonable support for neural networks in OpenCV began with version 3.3.0. Unfortunately the latest OpenCV version in the Raspbian repositories is 2.4.9.1. So you have to install it manually and compile it from the sources. You can find a good installation guide here: https://www.pyimagesearch.com/2016/04/18/install-guide-raspberry-pi-3-raspbian-jessie-opencv-3/

You can leave out the python stuff since we don't need it here. I installed the latest OpenCV version which is now 3.4.1. On my Raspberry Pi 3 Model B+ I encountered a lot of problems when I used all 4 cores for compiling. So I had to compile it using only a single core. Thus it took about 5 hours to compile.

 

Running deep neural networks

 

There exist different framworks for neural networks but most of them are supported by OpenCV. I am using the caffe framework because there already exists a nice example in the OpenCV documentation: https://docs.opencv.org/3.4.0/d5/de7/tutorial_dnn_googlenet.html

It uses the pre trainend GoogLeNet for image classification. You can find information on the network on this website: Caffe | Model Zoo   So, no training is necessary, just download the network and let it run. Furthermore training deep neural networks on the Raspberry Pi is no fun because you need way more computing power to do this in reasonable time.

 

I adjusted the example a little bit since using the same image like thousands have done before is a little bit lame. I will use images from the Raspberry Pi camera and find out what the network sees in them. This is a little bit more realistic because there are a lot of use cases for this in, for example, robotics where small computers with real time capabilities like the Raspberry Pi are needed at the edge.

 

Here is my code:

#include <iostream>
#include <string>
#include <opencv2/dnn.hpp>
#include <opencv2/core/utils/trace.hpp>
#include <opencv2/opencv.hpp>
#include <thread>


// global variables for exchange between threads
cv::VideoCapture cap;    // create camera input
cv::Mat cameraImage;  // create opencv mat for camera

void cameraThread(void)    // function for the camera thread
{
    while(1)    // loop forever
    {
        cap >> cameraImage;    // copy camera input to opencv mat
    }
}

/* Find best class for the blob (i. e. class with maximal probability) */
static void getMaxClass(const cv::Mat &probBlob, int *classId, double *classProb)
{
    cv::Mat probMat = probBlob.reshape(1, 1); //reshape the blob to 1x1000 matrix
    cv::Point classNumber;
    minMaxLoc(probMat, NULL, classProb, NULL, &classNumber);
    *classId = classNumber.x;
}
static std::vector readClassNames(const char *filename = "synset_words.txt")
{
    std::vector classNames;
    std::ifstream fp(filename);
    if (!fp.is_open())
    {
        std::cerr << "File with classes labels not found: " << filename << std::endl;
        exit(-1);
    }
    std::string name;
    while (!fp.eof())
    {
        std::getline(fp, name);
        if (name.length())
            classNames.push_back( name.substr(name.find(' ')+1) );
    }
    fp.close();
    return classNames;
}

int main( int argc, char** argv )
{
    int ende=0;
    std::thread tcam;    // create thread pointer

    std::cout << "OpenCV version : " << CV_VERSION << std::endl;    // print opencv version for debug

    std::string model = "bvlc_googlenet.caffemodel";    // define filenames for neural network
    std::string proto = "bvlc_googlenet.prototxt";

    cv::dnn::Net net = cv::dnn::readNetFromCaffe(proto, model); // open net
    
    if (net.empty())
    {
        std::cerr << "Can't load network by using the following files: " << std::endl;
        std::cerr << "proto: " << proto << std::endl;
        std::cerr << "model: " << model << std::endl;
        return -1;
    }
    
    cap.open(0);        // open camera
    if(!cap.isOpened()) 
    {
        std::cout << "no camera found!" << std::endl;
        return -1;
    }
    cap >> cameraImage;    // copy camera input to opencv mat to get data to startup
    tcam=std::thread(cameraThread);    // start extra thread to get camera input
    std::cout << "starting ..." << std::endl;

    while(ende==0)
    {
//GoogLeNet accepts only 224x224 BGR-images
        cv::Mat image;
        cameraImage.copyTo(image);    // copy camera image to have local copy for modifications
        cv::Mat inputBlob = cv::dnn::blobFromImage(image, 1.0f, cv::Size(224, 224),cv::Scalar(104, 117, 123), false);   //Convert Mat to batch of images
    
        cv::TickMeter t;
        net.setInput(inputBlob, "data"); //set the network input
        t.start();  // start timer
        cv::Mat prob=net.forward("prob");    // computer output
        t.stop();  // stop timer

        int classId;
        double classProb;
        getMaxClass(prob, &classId, &classProb);//find the best class
        std::vector classNames = readClassNames();
        std::cout << "Best class: #" << classId << " '" << classNames.at(classId) << "'" << std::endl;    // print best class
        std::cout << "Probability: " << classProb * 100 << "%" << std::endl;    // print propability
        std::ostringstream buf;
        buf << "Best class: #" << classId << " '" << classNames.at(classId) << "' - ";
        buf << "Probability: " << classProb * 100 << "%";
        cv::putText(image,buf.str(),cv::Point2f(10,20),0,0.5,cv::Scalar(255,255,255),1,1);  // print buf to image

        std::cout << "Time: " << (double)t.getTimeMilli() / t.getCounter() << " ms" << std::endl;  // print result of timer


        cv::imshow("image",image);    // show image
        char key=cv::waitKey(1);    // check if end
        if(key=='e') ende=1;
    }
    return 0;
}

 

The program uses a second thread to read the data of the camera so that there is no delay in the stream.

 

Power measurements

 

To power the Raspberry Pi I made a little PCB with a Texas Instruments TPS54335 buck regulator on it. It takes 12 V as an input and generates 5 V for the Raspberry Pi. Additionally there is a Texas Instruments INA226 power monitor on the 12 V rail to measure input voltage and current. The INA226 is also connected to the I2C bus of the Raspberry Pi. So the Raspberry Pi can read out its current power consumption (Actually there are some losses in the voltage regulator but when I use the same regulator for all tests it should be comparable)

 

Test setup

 

I did all test with the same camera and SD card. I just exchanged the Raspbery Pi. The system is running Raspbian Stretch with Destop, Version March 2018, but the boot option is set to console only. Ethernet is connected, WiFi is off. Nothing is connected to USB, no monitor attached.

The system was installed and setup on the Raspberry Pi 3 Model B+ and then the same SD-Card was transferred to the other models.

 

During all tests the camera will see the scene on the screenshot below and identify it as teddy bear.

image

 

Results

 

power in idle

Since I already had the test setup I also made some measurements in the idle mode. I was logged in via ssh and was at the bash prompt.

 

Model
Current (A)
Power (W)
Raspberry Pi 20.1281.53
Raspberry Pi 30.1471.76
Raspberry Pi 3 Model B+0.2032.43

power during calculation of neural network

 

Model
Current (A)
Power (W)
Raspberry Pi 20.2783.32
Raspberry Pi 30.4215.05
Raspberry Pi 3 Model B+0.5636.76

execution time of neural network

 

Model
time (ms)
Raspberry Pi 22635
Raspberry Pi 31804
Raspberry Pi 3 Model B+1548

energy consumption for each cycle of the neural network

Given the execution time and power consumption one can calculate how much energy each cycle of the neural network consumes.

 

Model

Energy (Ws)

Raspberry Pi 28.75
Raspberry Pi 39.11
Raspberry Pi 3 Model B+10.46

 

Conclusion

 

The new Raspberry Pi 3 Model B+ calculates the neural network nearly twice as fast as the Raspberry Pi 2. On the other hand it also needs twice as much power. When you compare Raspberry Pi 2 and 3 the newer is a lot faster and consumes more power but the energy efficiency of these two models is nearly the same. The new Raspberry Pi 3 Model B+ has a worse efficiency than its predecessors. It has to be cleared why it is so bad. Maybe it is because of the Gigabit-Ethernet-IC or the new Wifi module.

But for now I have to state: The new model B+ should only be taken if you really need the processing power und your results fast. Projects where energy efficiency is important should stick to the old Raspberry Pi 3 or even the Raspberry Pi 2.

 

Do you have any ideas or comments on my measurements?

  • Sign in to reply
  • Cancel
Parents
  • genebren
    genebren over 8 years ago

    Bernhard,

    Going fast has a price.  And in the this case it is more current.  Just a minor point, but the majority of your power is being dissipated in your regulator.  In fairness to your setup, your relative power usage is correct, but for actual power used by the Raspberry Pi, the power should be 5V*I not 12V*I (5 * 0.278 = 1.39W and not 12 * 0.278 = 3.336W, as 1.946W are be dissipated by your regulator.

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bernhardmayer
    bernhardmayer over 8 years ago in reply to genebren

    Hi Gene,

    my power regulator is a Texas Instruments TPS54335 and it is a switching regulator. The losses should somewhere between 10 and 20 %. So the correct formula should be 12V * I * 0.8.

    Bernhard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bernhardmayer
    bernhardmayer over 8 years ago in reply to genebren

    Hi Gene,

    my power regulator is a Texas Instruments TPS54335 and it is a switching regulator. The losses should somewhere between 10 and 20 %. So the correct formula should be 12V * I * 0.8.

    Bernhard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to bernhardmayer

    Bernhard,

     

    Good point.  I would guess that you might closer to correct on the total power.  If you really wanted to know that actual power consumed by the Raspberry Pi in these test (and not artifacts of the regulation), the better test might be to measure the current delivered to the Pi and not the input current to the regulator.  The Pi power would then be I x E, where E would be 5V.  Either way, the readings that you took, really do show the effect of processing load on the Pi due to the calculations being performed.

     

    Good work!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bernhardmayer
    bernhardmayer over 8 years ago in reply to genebren

    Gene,

    I have to admit measuring at the 5 V input rail would be way better.

    Unfortunately I only had the board with the voltage regulator and the measurement on the 12 V side. But I plan to make a PCB where I can connect the original Raspberry Pi power supply and measure directly on the 5 V. But again, it will take a few weeks until the new PCB is here. Then I will do the measurements again.

    Bernhard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rew
    rew over 8 years ago in reply to bernhardmayer

    Hi Bernhard,

    If you send me your address, I'll send you an easy tool to make those measurements. My domain is bitwizard.nl, the info@ email address works.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • bernhardmayer
    bernhardmayer over 8 years ago in reply to rew

    Hi Roger, the email is on its way. Bernhard