Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Desktop install gives me this message
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 706 subscribers
  • Views 2227 views
  • Users 0 members are here
  • raspberry_pi_space
  • pi desktop install error
Related

Pi Desktop install gives me this message

massimj
massimj over 8 years ago

I am trying to get my Pi Desktop to work. I did the removal of the old desktop, bu then when I went ot run the install for the new desktop, while in the directory with the file in question, I get this:

 

(Reading database ... 137322 files and directories currently installed.)

Preparing to unpack pidesktop-base-1.1.0.deb ...

Unpacking pidesktop-base (1.0.0) over (1.0.0) ...

Setting up pidesktop-base (1.0.0) ...

Failed to enable unit: File embest-shutdown.service: No such file or directory

Failed to enable unit: File embest.service: No such file or directory

 

Can someone shed any light on why I get this erro ,when the instruction mentions no problem?  The removal went ok, but the install fails.

 

The command is :  pi@raspberrypi:~/Downloads $ sudo dpkg -i pidesktop-base-1.1.0.deb

 

Thanks for any help with this error, and getting my pi desktop to work.

  • Sign in to reply
  • Cancel
Parents
  • rweatonnz
    rweatonnz over 8 years ago

    I had the same errors.  It turned out to be caused by following the written instructions that came with the pi-desktop and downloading and installing pydesktop.deb.  When that did not work research brought me to this website which said to download and install the newer version with sudo dpkg -i pidesktop-base-1.1.0.deb.  This yielded the same error that you are getting. Once I did a sudo dpkg -r pidesktop-base and a sudo dpkg -r pidesktop-base-1.1.0 and then did another install with sudo dpkg -i pidesktop-base-1.1.0.deb it all installed OK.

    I am not that experienced with all this.   I was trying to set up a Pi-Desktop with a 1TB KingSpec msata set to boot from the SSD.  The msata checks out fine on linux desktop but I could not get it to reliably and consistently boot.

    Search this site for hoopsurfer or go to:  https://github.com/hoopsurfer/pidesktop He has done a fork of the pidesktop package and at least for me it is working better.  Still regardless of what I did I could not get the KingSpec 1TB msata to consistently boot so I followed hoopsurfers instructions for berryboot and used a 32gB short USB flash drive to install Raspian on and formated the msata drive as an ext4 drive for additional storage.  Should note I am using a Pi3B+, have a correct official 2.5A power supply (several actually), did all the setup tricks correctly but none of those produced a consistent ability to boot directly from the msata ssd.  Working good the way I have it set up now though which will be fine for me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rweatonnz
    rweatonnz over 8 years ago

    I had the same errors.  It turned out to be caused by following the written instructions that came with the pi-desktop and downloading and installing pydesktop.deb.  When that did not work research brought me to this website which said to download and install the newer version with sudo dpkg -i pidesktop-base-1.1.0.deb.  This yielded the same error that you are getting. Once I did a sudo dpkg -r pidesktop-base and a sudo dpkg -r pidesktop-base-1.1.0 and then did another install with sudo dpkg -i pidesktop-base-1.1.0.deb it all installed OK.

    I am not that experienced with all this.   I was trying to set up a Pi-Desktop with a 1TB KingSpec msata set to boot from the SSD.  The msata checks out fine on linux desktop but I could not get it to reliably and consistently boot.

    Search this site for hoopsurfer or go to:  https://github.com/hoopsurfer/pidesktop He has done a fork of the pidesktop package and at least for me it is working better.  Still regardless of what I did I could not get the KingSpec 1TB msata to consistently boot so I followed hoopsurfers instructions for berryboot and used a 32gB short USB flash drive to install Raspian on and formated the msata drive as an ext4 drive for additional storage.  Should note I am using a Pi3B+, have a correct official 2.5A power supply (several actually), did all the setup tricks correctly but none of those produced a consistent ability to boot directly from the msata ssd.  Working good the way I have it set up now though which will be fine for me.