Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB joystick only works through unpowered hub?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 706 subscribers
  • Views 2709 views
  • Users 0 members are here
  • usb
  • retropie
Related

USB joystick only works through unpowered hub?

andywest
andywest over 8 years ago

I'm nearly finished building a handheld game system running RetroPie. However, there's one thing I can't get working.

 

I'm using a USB joystick encoder (https://www.amazon.com/Reyann-Arcade-Encoder-Joystick-Fighting/dp/B00UUROWWK/). I've hand-wired a USB cable to the test pads of a Raspberry Pi 1 Model A+ with 512MB RAM. The cable is terminated with an A-type female connector. The encoder has a hand-wired cable with an A-type male connector.

 

When the encoder is connected directly to the Pi, the power light illuminates for less than a second and then goes out. RetroPie does not detect it. However, if I plug the encoder into a USB 2 hub (https://www.adafruit.com/product/2998 ) then it works. It's important to note that I am NOT supplying external power to the hub.

 

The fact that it works with the hub suggests that it's not a problem with incorrect wiring or lack of power. Just in case, I built a separate test extender cable with the data wires swapped. As expected, it didn't work. I also tested the encoder on a Windows 10 PC (without swapping the wires) and it works fine.

 

Can anyone think of why this might be failing or know a way to fix it? Thanks!

  • Sign in to reply
  • Cancel
Parents
  • andywest
    andywest over 8 years ago

    In the end I just did the simplest thing I could think of. I stripped a 2-port USB hub down to the PCB and soldered it straight to the Pi. Works fine. I also threw a USB keyboard receiver dongle in there so I can mess around with configuration, etc. more easily. It's a tight fit, but as long as it doesn't overheat I think I'm good.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • andywest
    andywest over 8 years ago

    In the end I just did the simplest thing I could think of. I stripped a 2-port USB hub down to the PCB and soldered it straight to the Pi. Works fine. I also threw a USB keyboard receiver dongle in there so I can mess around with configuration, etc. more easily. It's a tight fit, but as long as it doesn't overheat I think I'm good.