Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 3 B+ broken, no green light
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 706 subscribers
  • Views 18644 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
  • raspberry_pi
Related

Raspberry Pi 3 B+ broken, no green light

mmetzner
mmetzner over 7 years ago

Hello Guys,

My Raspberry Pi is driving me nuts.

First I thought the fuse is broken, but I still doesn't work after leaving it off for two days. I tried several microSD cards and also 2 different power supplys, which both work with another pi.

It stopped working when I plugged in a usb drive. It just turned black and now only the red light is lighting up. there isn't any physical damage on the board. it just stopped working, what can I do?

 

Thanks for your help!

Max

  • Sign in to reply
  • Cancel
  • cstanton
    cstanton over 7 years ago

    Make sure you're using the official raspberry pi power supply unit rated at 5 volts, 2.5 amps, the Pi 3 B+ takes that bit more power, especially with USB devices attached, than older models.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • luislabmo
    luislabmo over 7 years ago

    The Red LED on the Raspberry Pi indicates Power. If it blinks a little or doesn't blink at all as soon as you connect the Pi to power:

    • You may be having power fault (may be a bad USB cable, bad adapter, an adapter not powerful enough, etc)
    • Your Pi may be fried (hopefully this is not the case)

    As indicated by cstanton is better to discard power issues by using the Official Raspberry Pi adapterOfficial Raspberry Pi adapter.

     

    Another way you may discard possible USB Power IN issues is to power the Pi directly to the GPIO pins. This method will bypass some power safety measurements so is advised only if you know what to do and you have a 5V regulated power supply that can provide enough current -at least 2.1 is advisable to play safe.

     

    More information about LED statuses on the Raspberry Pi here: https://elinux.org/R-Pi_Troubleshooting#Power_.2F_Start-up

     

    Luis

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mmetzner
    mmetzner over 7 years ago in reply to luislabmo

    Ok. The powersupply works without problems on another pi. it has 2,5 A. Another Samsung Plug doesn't work that way.

    Haven't come around to test powering it directly with the GPIO pins, but I will look into that, when I am back in the lab.

    Thank you so far!