Raspberry Pi Projects
  • Products
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Blog HAL-CAM 9001 - Building a Power over Ethernet (PoE) Supply
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 23 Sep 2016 4:58 AM Date Created
  • Views 11540 views
  • Likes 18 likes
  • Comments 23 comments
  • maxrefdes98
  • power over ethernet
  • o halcam
  • camera_v2
  • ccd
  • rpiintermediate
  • beagleboneblackindustrial
  • beaglebone_black
  • raspberry pi video camera
  • projects
  • cctv
  • raspberry_pi
  • eejournal
  • raspberry pi
  • bbb
  • poe
  • camera
  • video camera
  • maxim
  • raspberry_pi_camera
  • closed circuit television
  • raspberry_pi_projects
  • halcam
  • closed circu*
  • rpi_projects
Related
Recommended

HAL-CAM 9001 - Building a Power over Ethernet (PoE) Supply

shabaz
shabaz
23 Sep 2016

Introduction

This blog post is about powering a new security camera (HAL-CAM 9001) using network cables. These could be cables already installed in an office or home environment, saving costs, or they could be new cables installed indoors or outdoors (using weather resistant cable).

 

This sub-project is part of the HAL-CAM 9001 project but it is generic enough to suit other scenarios too. It could be used to power a Raspberry Pi remotely for other tasks. Other single board computers (SBCs) can benefit from this project too.

 

HAL-CAM 9001 doesn’t have a lot of free space inside so this project was made to be ultra-compact; 2cm high and 6x5cm footprint. This project supplies 5V at up to 2.5A.

The schematic and PCB files are attached, ready to be sent to a board manufacturer.

image

 

What is PoE?

Power over Ethernet is one of these technologies that when you use it, you find you really need it. Over the years it has saved costs, copper, and provided a reliable and safe solution to providing energy to many diverse devices over Ethernet based local area network (LAN) connections.

 

At its debut, it was said that standards-compliant PoE was effectively one of the few worldwide standards for power so one could take a device and be assured it would work anywhere in the world, in contrast with the mains supply voltages and plug shapes which vary from country to country. And it doesn’t require an electrician to install!

 

Part of the safety of PoE comes from the ability to automatically and electronically control the delivery of power. By default, the network connection has no substantial power capability enabled and is finger-safe. When the connected device requests power the far end will switch on the supply. Note: the equipment that can supply power is known as the Power Sourcing Equipment (PSE), and the device to be powered is the Powered Device (PD).

 

With the earlier standard (IEEE 802.3af) the request was as simple as having a 25k resistor across a couple of pins. If the resistor was present, then the far end would turn on the power. This solution provided about 13W of power to the PD. The later standard IEEE 802.3at nearly doubled this capability, to just over 25W of power. This later standard had a more complicated method of enabling power; the PD would provide a varying load over time in a special combination that would allow the PSE to detect that the PD was an 802.3at capable device and then supply up to one of four particular levels of power. Once this was achieved it was possible to signal information in Ethernet packets to further refine the power requirements.

 

Today Universal PoE (UPOE) has more than doubled the power capability to 60W – equivalent to an incandescent light bulb!

image

 

This project provides IEEE 802.3af and 802.3at standards based power capability. The output is at 5V, capable of up to 2.5A (i.e. up to 12.5W). This level of output is ideal for remotely powering HAL-CAM 9001, or other Raspberry Pi projects, BeagleBone Black (BBB) or other single board computers (SBCs).

image

 

Note that the powered device doesn’t actually need to have an Ethernet connection at all. It is possible to use PoE to charge your mobile phone.

image

 

How do I get PoE?

Assuming standards-based PoE is required then the best way is to pick up a switch with 802.3af or 802.3at capability. In the UK for consumer use the 802.3af compliant 8-port TP-LINK TL-SG1008P costs about £50 from Amazon and provides 4 devices with up to 13W of power each, simultaneously (I have not tried this switch so it isn’t a recommendation, just a pointer to what is out there).

 

There are also so-called ‘PoE Injector’ adapters, also misleadingly called 2-port PoE switches sometimes. These are not great because often they are not IEEE 802.3af or 802.3at compliant and may supply power all the time; they are therefore not very green because their power cannot be shut down electronically. A true standards compliant PoE capable switch is the far better choice and doesn’t cost much as mentioned earlier, considering it can power up to four devices.

 

At the device end, it needs to support the same standard. If the device doesn’t support PoE then an off-the-shelf external PoE adapter can be used; it is standards compliant and taps off the supply to be used to power the device.

 

Building It

image

The schematic is shown below; it is really simple because most of the functionality is contained in Maxim’s MAXREFDES98MAXREFDES98 board which contains a DC-DC converter and the circuitry to handle the standards negotiation. The rest of the board mainly consists of the Ethernet transformers and connectors. Note that it would be wise to add some suppression circuitry as detailed in the original HAL-CAM blog page; I forgot to add it to this revision 1 PCB but the same method (TVS diodes) can be used as in the original blog post. At some stage I will update this blog post with revision 2 files which will correct this omission.

image

 

To construct this project, solder up the smallest parts first (the resistors and capacitors), ending with the largest parts. The fuse is optionally available in a socket which will fit the board but I chose to save some cost and directly solder the fuse.

 

Network cables are available in short lengths but I wanted an extremely short length (a few cm) for fitting inside HAL-CAM 9001 so I used an RJ45 tool to do that. The back of the PCB has a reference indicating which color wire goes where.

image

 

Testing It

There is not much chance of error during assembly since there are so few parts in this project (the part values are in the schematic but a list of components will be published in the next few days). I connected this project via the longest length of network cable that I had (5m long) to a switch, enabled PoE on it (some switches require configuration for this) and then used a multimeter to confirm 5V was present on the output supply connector. The on-board LED was lit too, confirming that the board was receiving power. The multimeter confirmed the correct output so I proceeded to plug it into the Pi and verified that the Ethernet link came up and I had network connectivity. I can now issue a shutdown command to the Pi remotely using SSH, and then configure the switch to disable power. Whenever I want to turn the Pi on, I can configure the switch to turn on the PoE capability.

 

There are additional tests that should be done (such as confirm the voltage output under changing loads, verify the ‘eye diagram’ for the signals over the network cable, check for RF interference and checking throughput to see if there are any packet errors occurring). These will be done later at some stage; for now the board is functioning well enough to continue HAL-CAM 9001 development.

 

Summary

PoE is easy to use and it can be useful to be able to retro-fit non-PoE devices with the capability. The Maxim module makes this really easy. The PCB files are attached ready to send to a manufacturer. Note that the PCB also has some additional “features” (see photo below) which can be hack-sawed off and put aside for now (they are for unrelated mini-projects which will be documented at some later stage; feel free to guess what they are! It is not too difficult).

image

 

See also:

 

HAL-CAM 9001 – Building a New Security Camera

Attachments:
poe-export-1.zip
  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 9 years ago +4
    Nice project. It should help with that heat problem nicely ....
  • clem57
    clem57 over 9 years ago +4
    shabaz up until now, I looked at POE as redundant. But now you gave me convincing arguments to re examine. Thanks for the research. Clem
  • jw0752
    jw0752 over 9 years ago +3
    Hi Shabaz, Thanks for posting this interesting and useful build. I will be following your future refinements. John
  • clem57
    clem57 over 9 years ago

    shabaz up until now, I looked at POE as redundant. But now you gave me convincing arguments to re examine. Thanks for the research.

    Clem

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago

    Nice project.

    It should help with that heat problem nicely ....

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shaz730
    shaz730 over 9 years ago

    Cool stuff!! Now I want to build one!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to michaelkellett

    Hi Michael,

     

    Thanks for the info! I'd looked at a TP-link one but someone had written they'd needed the injector so I'd written it off as non-standards compliant, but the one you've found does state 802.3af on that Amazon page so it should work, good price too.

    The TP-link one I'd looked at was this one, where their documentation states 802.3 but that's misleading since that's just the physical layer: https://cpc.farnell.com/tp-link/tl-poe200/adapter-kit-power-over-ethernet/dp/CS26386?krypto=neomHOrzOAdoCrXNlnHVDqkhTlLS…

     

    I'd also taken apart an 'Infomart' one to research it, but it was quite a bulky design, probably an isolated supply, but had a large heat sink and the insides were too large for the application.

    PES4012GPC0 INFOMART IT SOLUTIONS, MODULE, POE, SPLITTER, 12V | Farnell element14

     

    That Farnell module looks good! It looks perfect. I will swap out to that one in the revision 2 PCB. I'd like to make a few more of these PoE boards, but the Maxim one makes it very expensive.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to shabaz

    Hello Shabaz,

     

    Thanks for the blog.

     

    That's a very steep price for the POE module, found  this one on the web (for a tenner):

     

     

    TP-LINK TL-POE10R PoE Splitter

     

    In the past I've used Silvertel modules -  I think there were about £7 each , buying 25 at  a time.

     

    Cheapest I could find on Farnell was 1902521 at about £11 - might be pin compatible with the Maxim one but I haven't checked.

     

    I've been disappointed that POE enabled switches are still a bit pricey. We wired our house with CAT6 cable recently and I thought about having  a POE switch until I saw how much extra it would cost.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>