Raspberry Pi Projects
  • Products & Partners
  • Raspberry Pi
  • Raspberry Pi Projects
  • More
  • Cancel
Raspberry Pi Projects
Documents Building a Low Power Compact LCD Display
  • Blog
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi Projects to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 22 Apr 2016 4:41 PM Date Created
  • Last Updated Last Updated: 10 May 2021 6:52 PM
  • Views 15228 views
  • Likes 20 likes
  • Comments 55 comments
Related
Recommended

Building a Low Power Compact LCD Display

(Note: For a follow-up project which uses a larger screen, click here:Building a 3.5 Digit Low Power LCD Module  )

image

Introduction

Sometimes a really simple, low power display is needed. A lot of information can be shown on even a 7-segment display!

 

This LCD board project could be useful for such purposes. The three 7-segment digits (and two decimal places total, between the digits) can show percentages, hexadecimal values, voltages and current readings. Plenty of characters can be represented too.

 

Up to four of these displays can be connected to a single I2C bus so (for example) a power supply project could use one display for voltage and another for current, for two channels. To save costs for smaller projects a single display could be used to show more than one item of information using  a button press or periodic cycling of data on the display.

image

 

The reflective LCD that is used has no backlight but has very good contrast and in tests had excellent visibility even in dim light. The power consumption is extremely low and this makes it ideal for portable projects which might need to run for years on batteries without charging. The entire bill-of-materials is less than £5GBP (or lower if multiple displays are purchased).

The schematic and plot (gerber) files and source code is attached to this post. I had 20 PCBs made for less than the cost of a pizza.

image

As a quick test I tried it using a Raspberry Pi just counting up from 0.0 to 99.9. With very little effort it would be possible to use it to display Pi stats – for example temperature, or the IP address (one byte at a time) upon start-up. It is easy to get any script to write to the display from the command line.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Features Summary

  • 3.3V or 5V capable
  • Ultra-low current consumption (24uA at 3.3V)
  • Extremely compact; 32x21mm
  • Just a 4 wire connection; I2C Interface, 0V and VDD (3.3V or 5V)
  • Individually addressable segments for alphanumeric and other symbol use
  • Quick to assemble; less than a dozen parts
  • Low cost; about £5GBP in quantities of 1

 

Parts List

RefCodeMnfr Part #DescriptionQtyGBP Each
LCD118389301838930LCD-S301C31TRLCD-S301C31TRLCD 3-digit11.85
U124004602400460PCF85176TLCD Driver11.18
C317591221759122MC0603B104K500CT100N 0603 x7r10.01
R1, R320733492073349MCMR06X1002FTLMCMR06X1002FTL10K Res 060320.01
R2, R4, R5D.N.F.00.00
R6, R793319729331972MC0063W060352K7MC0063W060352K72.7k Res 060320.01
J1159341515934152211S-06G2211S-06GSIL header 6-way10.26
Optional177848177848D01-99012 01PCB pin sockets 12-way21.18
Optional229985622998560552-2-15-01-21-27-10-00552-2-15-01-21-27-10-0PCB pin sockets (alternative)240.07

 

Additional components for 5V operation

RefCodeMnfr Part #DescriptionQtyGBP Each
U223143722314372TPS70925DBVTTPS70925DBVTLDO 2.5V Voltage Regulator10.82
C119073431907343C1608X7R1C105K080AC1u 0603 X7R10.04
C217355421735542GRM21BR71E225KA73LGRM21BR71E225KA73L2.2u 0805 X7R10.24

 

How it Works

There are different types of LCDs, but in general they require an alternating current (AC) signal to turn on segments. Some use a square wave, others require multiple voltage levels in order to achieve high segment density with low pin count through multiplexing.

The particular LCD chosen requires a square wave, and has the benefit of providing high contrast digits. Reflective displays offer high contrast but have the disadvantage that they are opaque from the underside and cannot be lit from behind so require either ambient light to be visible or a side light.

 

Some microcontrollers feature LCD driving capability but there is a classic integrated circuit from NXP that is useful to offload the task from microcontrollers and allow the use of an I2C bus for interfacing. That IC is the PCF8576 which has been around for more than two decades. NXP have a more recent IC called PCF85176 (it appears to be backwards-compatible) and that is the one used for this project because it has very low power consumption requirements and a higher speed I2C bus capability than its predecessor.

Nothing else is needed apart from a few resistors and capacitors.

 

The LCD needs a few volts peak voltage in order to function. For 5V operation a linear regulator provides the lower voltage to run the LCD.

 

Building It

image

Order the boards from a PCB firm (the files are attached to this post). Once the PCBs arrive, the first step is to solder the PCF85176 chip. It is quite small (0.5mm spaced pins) but hand-soldering is still possible. A hot plate and solder paste would be another option. I just used a normal soldering iron (2mm tip) and no-clean flux (cleaned up afterwards) and thin solder.

 

The hardest part is perfect alignment. The way I do it is to tape the IC onto the PCB first. Then, inspect the pins using a magnifying lens. If it looks incorrect, peel the tape from one end but keep the IC attached to the tape. Move the tape and re-stick it onto the PCB. It becomes quite easy to align the IC and secure it in this manner, just moving the tape from one side at a time.

 

Next, apply a small amount of no-clean flux and start soldering. Any bridges will fall away if you re-heat with the iron, but if the bridge is persistent then use de-soldering braid. The soldering iron needs a bit of solder applied to the tip in order to get the solder-wicking effect when using the braid.

 

Optionally use pin sockets (or SIL sockets) so that the LCD does not need to be soldered. It is highly recommended that sockets are used to protect the LCD and also because it would be difficult to unsolder the LCD if there was a problem with the PCF85176 that needed examining.

After all the parts have been soldered clean the board using an IPA solution and then examine each pin on the PCF85176 under a lens (push each pin gently with the side of a scalpel blade) to verify all is well.

image

 

If the display only needs to operate from 3.3V then you don’t need to solder the linear regulator IC and its associated capacitors. If multiple displays on the same I2C bus are needed then the addresses are programmed using two 10k resistors that can be soldered in different positions (see the source code for a table which indicates this).

image

 

The attached files are slightly improved to the boards that I used, in that there is a white space for labelling them if multiple displays are needed for a single project.

 

After checks for any short circuits, the LCD can now be connected up to the Pi.

image

 

Software

As a quick test some C code was written for the ‘Pi. It was tested using a Pi 2 but should work on others, there is nothing special to the code.

To enable I2C on the ‘Pi, add the following line to /boot/config.txt (you need to be root user to do this):

dtparam i2c_arm=on

 

Reboot the Pi and then type (as root user):

modprobe i2c_dev

 

To make it persistent across reboots you can add the following (as root user) to the /etc/modules file:

i2c-dev

 

Grab the code from github. To compile the code type the following:

gcc -c i2cfunc.c -o i2cfunc.o
ar rcs libi2cfunc.a i2cfunc.o
gcc lcd3-test.c -L. -li2cfunc -o lcd3-test

 

To run it, type:

./lcd-test

 

Currently the code can display decimal points, digits 0-9 and space.

To use it, call the print_line() function. Here are some examples:

print_line(" 0.0");
print_line("1.23");
print_line("   "); // clear the screen

 

image

 

The I2C interface is a standard, and it would be very easy to port the code across to any microcontroller/Arduino/etc.

 

Summary

NXP’s I2C LCD chip continues to be useful after two decades. The cost, size and low power consumption are attractive for some use-cases. Although this project uses surface mount components they are cheap enough that it could be a useful board to practice with. The very low power consumption means that a couple of AA batteries should last for five years or more with the display always on.

 

image

 

Advanced Use: Extending the Character Set

Many characters are possible with 7-segment displays.

image

Three bytes represent which segments are to be activated. Refer to the diagram to see the bit mappings.

image

 

To extend the character set to display hyphens or alphabet characters, the following array needs to be extended:

 

const char bit_table[]=
{
  0x38, 0x00, 0x86,    0x00, 0xbe, 0x00,    0x86, 0x00, 0x38,    /* 0 */
  0x08, 0x00, 0x02,    0x00, 0x0a, 0x00,    0x02, 0x00, 0x08,    /* 1 */
  0x30, 0x00, 0x46,    0x00, 0x76, 0x00,    0x46, 0x00, 0x30,    /* 2 */
  0x18, 0x00, 0x46,    0x00, 0x5e, 0x00,    0x46, 0x00, 0x18,    /* 3 */
  0x08, 0x00, 0xc2,    0x00, 0xca, 0x00,    0xc2, 0x00, 0x08,    /* 4 */
  0x18, 0x00, 0xc4,    0x00, 0xdc, 0x00,    0xc4, 0x00, 0x18,    /* 5 */
  0x38, 0x00, 0xc4,    0x00, 0xfc, 0x00,    0xc4, 0x00, 0x38,    /* 6 */
  0x08, 0x00, 0x06,    0x00, 0x0e, 0x00,    0x06, 0x00, 0x08,    /* 7 */
  0x38, 0x00, 0xc6,    0x00, 0xfe, 0x00,    0xc6, 0x00, 0x38,    /* 8 */
  0x18, 0x00, 0xc6,    0x00, 0xde, 0x00,    0xc6, 0x00, 0x18     /* 9 */
};

 

The first group of three bytes indicates the segments that need to be turned on for the digit in the leftmost position, the second group of three refer to the center digit and the last three refer to the rightmost digit. If ASCII sequence is not followed then modify the char_prog function accordingly.

 

To enable the extra characters, the print_line function case statement checks can be extended.

Attachments:
export-lcd3.zip
export-lcd3-rev2.zip
export-lcd3-rev2-with-board-outline.zip
  • low_power
  • eagle
  • eagle-cad
  • lcd
  • rpiintermediate
  • lcd display
  • eagle_cad
  • raspberry_pi
  • display
  • nxp
  • raspberry_pi_projects
  • feature_tutorial
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 9 years ago in reply to shabaz +5
    Works fully now I'll create a follow up blog with the ported code.... edit: done - Building a Low Power Compact LCD Display - Port to Hercules Safety Microcontroller
  • DAB
    DAB over 10 years ago +4
    Great post Shabaz. You provide good information on how to use different LCD screens and interface them to a MCU. DAB
  • Jan Cumps
    Jan Cumps over 9 years ago +4
    I'm going to play along. I'll first try to talk to it with a Bus Pirate v4. Then as a low power reception indicator for a Sub-1GHz range test...
  • colporteur
    colporteur 1 month ago

    Professionally done, as always. I like the soup-to-nuts details. Make me feel I could build it myself. Except for the SMT work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Mahipal1985
    Mahipal1985 1 month ago in reply to shabaz

    Thank you 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz 1 month ago in reply to Mahipal1985

    Hi, I totally understand why the schematic isn't helpful; the website went through changes a few years ago, and the high-res images were lost. This was a major loss to thousands of old articles on this site sadly.

    I've dug around, and managed to get a better image from a KiCad import, click to enlarge and then you should be able to save the enlarged image, in high quality. I cannot update the original article for some reason.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Mahipal1985
    Mahipal1985 1 month ago in reply to shabaz

    Hi Shabaz,

    I came across your “Building a Low Power Compact LCD Display” project on the element14 community and found it very interesting, especially the use of the PCF85176T with a reflective LCD and the extremely low power consumption.

    I am currently working on a low-power CO monitor project and I am looking to use a similar reflective LCD solution with the PCF85176T.

    I noticed that you have provided the schematic, Gerber files and source code for your original project. I have been studying the schematic and PCB design, but I would really appreciate some help understanding the design in more detail.

    If possible, could you please share the original schematic/source design file (for example, the Eagle schematic/project file), or guide me on how I can obtain/open the original schematic? It would be extremely helpful for me to understand the LCD pin mapping, PCF85176T connections, VLCD circuit and address configuration correctly.

    I would also be very grateful for any advice you can give regarding adapting this design for my CO monitor project.

    Thank you very much for sharing such a useful low-power LCD design with the community.

    Best regards,
    Mahipal

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    Just made it work on the EasyL1105 board:  Low Power Compact LCD example for the EasyL1105 MSPM0 board 

    image

    This is a real time capture with 400kHz i2c clock, counting from 0 to 999, with a little pause between each count, and a larger pause at 101 for dramatic effect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shrutip
    shrutip over 6 years ago

    Hi,

    I am trying to use PCF85176H for my 7 segment LCD (2 Rows, 4 Digits each). Need to use 1:3 multiplexing mode of operation  Can anyone please guide to generate lookup table?  I am using the same library and able to turn ON display but with existing lookup table it displays incorrect values as expected....

     

    Below is Pin interface & Circuit:

    image

     

     

    image

     

    Thanks & Regards....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to colporteur

    The display I'm showing in the animation is approx 3 * 3 cm. A 1*1 cm viewport would give 40*40 pixels

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to colporteur

    Hi Sean,

     

    Depending on how experimental you want to go, an electronic zoetrope-type thing could be possible. I'm picturing something with lots of transparencies, like the circular ViewMaster things.. and rotating that with a stepper motor, with everything embedded in a model wall, or behind, and just a square visible with a frame around it. Sync'd with a white backlight, it should look like a flickering color TV maybe. But it could be a lot of effort : (

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 7 years ago in reply to Jan Cumps

    An idea I would suggest myself except for the modeling community expectation of realism.

     

    I created an arc welder that flashed on and off. Not good enough they said. In the end, light from four colours of LEDs flashing randomly, with random on and off duration, passed through a piece of fibre strand to hand of the miniature character, made muster.

     

    I saw the post on small displays and like a dog seeing a squirrel, I yanked on the leach to go have a look to see if there was a match.

     

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to colporteur

    Maybe you could simulate colour television by using a monochrome display and replacing the backlight with an rgb led?

    Cunning modulation and mixing of the 3 colours of the led may give the impression of colour tv ...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>