Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Assembled Gertboard for Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 17 Jan 2013 5:05 PM Date Created
  • Last Updated Last Updated: 10 May 2021 8:50 PM
  • Views 15984 views
  • Likes 2 likes
  • Comments 43 comments
Related
Recommended

Assembled Gertboard for Raspberry Pi

Assembled Gertboard forrpilogo_gertboard.gif
Buy NowBuy NowFeaturesUser ManualSoftwareApplicationsOther Raspberry Pi Accessories
gertboard_lg_Jan17.gif


Overview


Gertboard is the ideal add-on for Raspberry Pi. Designed by Gert van Loo, it is a flexible experimenter board that plugs directly into your Raspberry Pi, and out into the physical world, allowing you to detect and respond to external physical events. Detect and output analogue voltages. Drive powerful motors. Detect switch presses. Illuminate LEDs and drive relays. Jumper cables allow you to hook up different parts of the circuit in many different ways, allowing total flexibility. All controlled by your own Raspberry Pi.


Features:


  • Plugs directly onto Raspberry Pi GPIO socket
  • Motor controller, capable controlling a motor bi-directionally, delivering 18V and 2A maximum
  • Dual-channel D-to-A converter, 8-bit
  • Dual-channel  A-to-D converter, 10-bit
  • Onboard Atmel ATmega328ATmega328 MCU for running off-board programmes which are written, compiled and uploaded to Gertboard from Raspberry Pi
  • 6 x open collector outputs
  • 12 x LED indicators
  • 3 x momentary push switches
  • 10 x strap cables included
  • 18 x jumpers included
  • Software and manuals available to operate and learn how to use Gertboard

 


 

Back to top


Key Applications


  • Experimentation
  • Home burglar alarm
  • Motor control
  • Sensor detection and control
  • Educational applications

Back to top

  • raspberry
  • pi
  • raspberry_pi
  • for
  • assembled
  • gertboard
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • derickam
    derickam over 12 years ago in reply to derickam

    I figured it out using this resource:

     

    https://projects.drogon.net/raspberry-pi/gertboard-and-wiringpi/

     

    Had to add jumpers to the buffer chips (B1,B2,B3...etc) OUT.

    LEDS are now behaving normally. Just like a Cylon or Nightrider. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alanwood
    alanwood over 12 years ago in reply to derickam

    Hi,

     

    Have you checked that jumper J7 is in place to power the Gertboard? Also it's worth confirming that your power supply to the RPi is beefy enough.

     

    All the best.

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derickam
    derickam over 12 years ago

    Received the board and it is plugged in proper, both plug rows seated and the board oreinted as per the manual.

    Have my jumper wires (GB to B) in place and double checked.

    Unzipped and compiled Gertboard test software.(jan 2013 ver)

    When I run the leds test program all the leds blink instead of in sequence like I have seen on various youtube videos.

    Am I missing something? Jumper wire or jumper plug?

     

    Runninng RPi ver7 with raspian and the new gertboard with the surface mount LEDS.

     

    I am going to keep digging for an answer but...

     

    Any ideas would be much appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • captainofspray
    captainofspray over 13 years ago

    The Gertboard will plug directly onto the Pi's GPIO pins, so you don't actually need a cable. If you want a cable, the last comment on this page tells you where to get it  http://www.element14.com/community/docs/DOC-51726/l/assembled-gertboard-for-raspberry-pi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Is it coming with the ribbon (26 wire cable) to connect it to the pi or I have to buy the cable separately?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to e14 Contributor

    Mine was a 168 Is suppose they didnt need any more.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hello again.  I just recently received a gertboard  and was able to install the arduino IDE, but I cannot read the chip number on the Atmega so don't know if it's a 168 or 328, so how do I set up the IDE? Thanks in advance fo the help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alanwood
    alanwood over 13 years ago in reply to e14 Contributor

    Hi, The coocox software is only Windows compatible but you don't need it to experiment with the Gertboard. The supplied software is for programming ARM Cortex M micrcontrollers - neither the Gertboard nor the Raspberry Pi use this type of processor. If you go to http://coocox.org you will find a couple of boards that can use these tools. I suspect the disk was included with the Gertboard to encourage designers to try these boards as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • derekk19
    derekk19 over 13 years ago in reply to captainofspray

    As commented further on, if the gertboard is touching your ethernet plug it's mounted the wrong way round. When properly mounted one of the plastic legs on the gertboard will probably need to be removed - it will be sitting on top of the audio connector. I think this would be true, but in fact I've made up my own ribbon cable.

     

    I got a header from Element 14 (part is TE CONNECTIVITY / AMP - 2-111446-0 - HEADER, IDC, NO LATCH, 26WAY) costs about $5, which connects to the Gertboar. Also a female header (E14 part TE CONNECTIVITY / AMP SOCKET, NOVOLATCH, 26WAY, but I already had one, from a local electronics store). This connects to the pi. Plus a scrap of ribbon cable - I bought 1 metre from Element 14 (about 8 bucks). If you make your own cable (which is dead easy) be sure that you get the connectors the right way round. There are small arrows on the headers and you should align these with the coloured strip on the ribbon cable. Also arrange the the ribbon cable comes out the right side of the female connector so it comes out of your pi case rather than goes back over the pi (if that makes sense).

     

    Now my pi is in its case and my Gertboard elsewhere in my desk. And I didn't have to unsolder any headers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to zed_thirteen

    I think that cases can be quite awkward for those who are going to use external Hardware boards regardless to if it's physically connected to the 'Pi or via a cable as that cable  generally is required to be so short that the cables are stiff and awkward

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>