Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Assembled Gertboard for Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 17 Jan 2013 5:05 PM Date Created
  • Last Updated Last Updated: 10 May 2021 8:50 PM
  • Views 15985 views
  • Likes 2 likes
  • Comments 43 comments
Related
Recommended

Assembled Gertboard for Raspberry Pi

Assembled Gertboard forrpilogo_gertboard.gif
Buy NowBuy NowFeaturesUser ManualSoftwareApplicationsOther Raspberry Pi Accessories
gertboard_lg_Jan17.gif


Overview


Gertboard is the ideal add-on for Raspberry Pi. Designed by Gert van Loo, it is a flexible experimenter board that plugs directly into your Raspberry Pi, and out into the physical world, allowing you to detect and respond to external physical events. Detect and output analogue voltages. Drive powerful motors. Detect switch presses. Illuminate LEDs and drive relays. Jumper cables allow you to hook up different parts of the circuit in many different ways, allowing total flexibility. All controlled by your own Raspberry Pi.


Features:


  • Plugs directly onto Raspberry Pi GPIO socket
  • Motor controller, capable controlling a motor bi-directionally, delivering 18V and 2A maximum
  • Dual-channel D-to-A converter, 8-bit
  • Dual-channel  A-to-D converter, 10-bit
  • Onboard Atmel ATmega328ATmega328 MCU for running off-board programmes which are written, compiled and uploaded to Gertboard from Raspberry Pi
  • 6 x open collector outputs
  • 12 x LED indicators
  • 3 x momentary push switches
  • 10 x strap cables included
  • 18 x jumpers included
  • Software and manuals available to operate and learn how to use Gertboard

 


 

Back to top


Key Applications


  • Experimentation
  • Home burglar alarm
  • Motor control
  • Sensor detection and control
  • Educational applications

Back to top

  • raspberry
  • pi
  • raspberry_pi
  • for
  • assembled
  • gertboard
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • captainofspray
    captainofspray over 13 years ago in reply to e14 Contributor

    1. Change directory to wherever you installed the programs

    2. Start the command name with ./ (dot-slash) - this means to look for the program in the current directory

       sudo ./buttons

         [the sudo is necessary because the GPIO access is root only]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Am a bit confused. I have downloaded the main software and extracted it. Having set up 'buttons' to run as a test, I can't get the programme to start from Terminal. I give up, how do I start the 'buttons' programme?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    I am trying to get my head around the gertboard, and I have a question, in the manual, figure 9 input and output jumpers.

    Where on the Schematic is B1 through B4 input and output jumpers show?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • epmueller
    epmueller over 13 years ago

    David... true.  I faced mine toward the center of the board not the edge.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zed_thirteen
    zed_thirteen over 13 years ago in reply to epmueller

    Edward, if you put a right angle connector on the underside of the board the two rows of pins will be reversed - at least I think they will.

     

    When plugged into an IDC cable header pins 1 to 13 will connect to 14 to 26 and pins 14 to 26 will connect to 1 to 13.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • zed_thirteen
    zed_thirteen over 13 years ago in reply to zed_thirteen

    I got around my connector problem by buying a "Raspberry Pi Stacking Header - 2x13 Extra Tall" from http://www.hobbytronics.co.uk/raspberry-pi/rpi-stackable_header-long.

     

    I had to de-solder the header from the underside of the Gertboard and replace it with this. The Gerboard can now either be plugged in to the top of the Pi or can be connected using a ribbon cable.

     

    I did try to de-solder the whole 26 way connector from the Gertboard but it wouldn't budge.

    I had to use a hacksaw to saw through the original header at about 2mm away from the board (on the joint between the two plastic types) and then de-solder each pin individually. Be warned, there is considerable risk with this so do this at your own risk.

     

    Anyway, some photos here:

    http://s1195.beta.photobucket.com/user/zed_thirteen/library/Raspberry%20Pi%20Stuff

     

    Hope it helps someone else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    I have an issue that I am looking for help with.  I received a Gert Board and working with the demo software and everything was working great until I tried the Motor demo.  I connected a 10v 2 amp power supply across the Power contacts, checked for correct connection. Connected a servo motor to MotA and MotB.  Tried running the motor directly, the motor actually draws about 1.8 amps @ 10 v.

    I ran the Motor demo, as soon as I pressed return, the PI went dead.  The pwr led is lit but the PI shows no activity, I can not reboot, the unit is completely unresponsive, even when the GertBoard is detached.  The 2 amp fuse did not blow.

    One of the reasons I wanted the Gertboard was not only the variety of IO but protecting the PI unit. 

    Has anybody seen similar problems?  Can not explain any problems on my set up, but having the motor controller capable of killing the processor is a problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • captainofspray
    captainofspray over 13 years ago

    Thanks, Stuart. I did realise sometime later after I had made the comment.

     

    Apologies to everybody I convinced to get a ribbon cable - it's not necessary.

     

    However, is it really so blindingly obvious? A simple diagram, either in the box, or in Gert's User Manual would have helped me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to captainofspray

    Tim, if your Gertboard is touching your Ethernet socket, it pluged in the wrong way round.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • joeman
    joeman over 13 years ago in reply to e14 Contributor

    Hey Borchaman:

     

    Post a question in our "Feedback and Support" page, someone can probably help you out thereimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>