Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents PiFace Home Timeswitch - turning a light on and off
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: PEarle
  • Date Created: 23 May 2013 8:29 PM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:29 AM
  • Views 5395 views
  • Likes 1 like
  • Comments 46 comments
Related
Recommended

PiFace Home Timeswitch - turning a light on and off

** Update**

 

I've now implemented this using an Energie Pi Controlled mains Socket - see my blog at Home Automation using ENERGENIE - ENER002-2PI

 

For details on the Energie socket see ENER002-2PI - ENERGENIE - RF CONTROLLED MAINS SOCKETS, FOR | CPC


 

 

One of the things I wanted to do with my Pi from the outset was to be able to use it as a timer, to turn a light on and off at night when I was out, as a simple form of home security. Being something of a newbie when it comes to electronics, my biggest problem was how to wire it up to be able to turn the power on and off.

 

The Pi relays are rated at a maximum of 20v and 5amps - therefore I cannot connect the Pi directly to the 'mains powered' light !!!

 

What I am planning on doing is investigating using a to a commercial relay which can cope with the current. When I've done that I shall update this blog again with details of the how the Pi can safely control a mains powered device.

 

However, the rest of the blog is still valid as it explains how the relay on the PiFace is operated and will be used for the Timer application, when completed.

 

I've written a java program to control the light switching on and off which does the following;

 

  • Calculate a random wait time between two values that I have supplied (2 and 20 minutes at the moment)
  • Wait for that period of time to elapse
  • At the end of the wait time, toggle the relay - switch it on if it was already off, and vice-versa.
  • repeat the above ad infinitum

 

The result is that the light will keep turning on and off in a random pattern making it look as if someone is using the room even when I'm not there !

 

 

Java Code

I've already written a document about using Java on the Pi - see http://www.element14.com/community/docs/DOC-54112/l/java-on-the-raspberry-pi. The code that I used for this project is attached to this document (e.g. timeswitch.zip)

 

 

Running Automatically

My intention is really to have this as a 'black box' function so that the TimeSwitch application will run as soon as the Pi is switched on. This is accomplished quite easily - all I need to do is write a script to run the java application, and then add it to the initialisation script.

 

The script to run the java application is as follows ;

cd /opt/pi4j/examples
java -classpath .:classes:/opt/pi4j/lib/'*' com.phe.datetime.TimeSwitch

To run at start up I have edited  /tec/rc.local and added the following line

 

/opt/pi4j/examples/timeswitch.sh > /opt/pi4j/examples/timeswitch.log

 

This will execute the java app at start up and also pipe any log messages to timeswitch.log.

Attachments:
timeswitch.zip
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to Problemchild +2
    Maybe a DANGER rating from Bunny minion through to Skeleton minion
  • mcb1
    mcb1 over 12 years ago in reply to michaelkellett +1
    If you look at the RCSwitch there is a RPi solution. Frederick also used these to interface as an I2C device. http://www.element14.com/community/community/design-challenges/forget-me-not/blog/2014/08/11…
  • mcb1
    mcb1 over 12 years ago in reply to eatojg +1
    This adds a piece for the RPI and while it suits the UK, there are many others using a similar 433 or 315 MHz RF control. The code in the Watts Clever have a 24 bit data stream, but in reality it only…
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to mcb1

    Done

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to Robert Peter Oakes

    Just delete the numbers.

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to rew

    Rodger

    Very interesting ... thanks

    NZ and Australia both use 120 deg and you're right about the power capability.

     

    Most houses here are 60A/phase but are usually single phase at 230v.

    Neutral and earth are the same potential (they derive the neutral from the earth at the transformer)

     

    cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to rew

    Not my image , I borrowed it and without looking close enough (I saw what I was looking for, not what was correct) but now you mention it, yes I totally agree, when I get home I will create an image of my own and replace this one

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 12 years ago in reply to mcb1

    Yes, the USA has 180 degree out-of-phase system (and 2 phases), while europe has a 120 degreen phase shift and three phases. I don't know what the rest of the world does.

     

    If your wires can carry say 10A, at 200V(*), you can can carry 2kW using two wires. Upgrade to four wires and you can transport 4kW, right? Well, for USA and their system that's true. But with the 120 degree phase shift, you can transport 6kW with those same 4 wires!

     

    That's the advantage of the three-phase system.

     

     

    (*) I'm using nice round numbers, to ease manual calculations. No relationship with actual real-world voltages or currents implied.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to rew

    There seems to be lots of "incorrect" images out there.

     

    Its also interesting that it shows the phases as 180 degrees apart.

    Here our phases are 120 deg (meaning all three equal 360).

     

    Obviously the load in the neutral (which is often a screen around the phase cores) should be zero, but at worst only carries the current of one phase.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 12 years ago in reply to Robert Peter Oakes

    Peter, it would be best not to post such WRONG images. When the voltage is "120V AC" the RMS value of the sine wave is 120V. That means that the top of the sine wave is at around 170V. Pictures like yours perpetuate the falsehood that the peaks are at the rated voltage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to mcb1

    yup, there is a wiring technique where if you need 2 * 110V but at full current and uses one twin socket. The ones  here can be split by removing a jumper and then you connect one phase to the lower and one to the upper giving 110V on each but there actually separate phases centered around neutral

    imageimage

    on some socket types you can split the bridge between the upper and lower socket

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to Problemchild

    As I said up further I couldn't report it as it was generated by a staff member.

    Trying to implement something similar is probably going to run into the same problems.

     

    Besides we all know that the 'ignorant' don't read the warnings ...image

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to eatojg

    Yes that was what we were asking the original poster (and he was a staff member).

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>