Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Introducing the Raspberry Pi Zero
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 23 Nov 2015 7:28 PM Date Created
  • Last Updated Last Updated: 1 Mar 2016 5:24 PM
  • Views 21059 views
  • Likes 20 likes
  • Comments 91 comments
Related
Recommended

Introducing the Raspberry Pi Zero

Raspberry Pi Zero

This ultra-small and ultra-slim Raspberry Pi board is the smallest form factor Raspberry Pi on the market today at only 65mm long by 30mm wide and 5mm deep. The board supports mini connectors to save on space, and the 40pin GPIO is unpopulated providing the flexibility to use only the connections your solution requires.image

 

Features

  • Broadcom BCM2835 ARMv6  system-on-a-chip, running at up to 1GHz
  • 512MB on-board RAM
  • Unpopulated 40pin GPIO for added flexibility
  • MicroSD port for OS and storage
  • Micro USB power input
  • 1x Micro USB Data port and Mini HDMI Port

(comes with Micro USB ‘On the Go’ adapter and Mini HDMI to HDMI adapter)

 

Buy Now

Raspberry Pi Zero  SOLD OUT
Raspberry Pi Zero & NOOBS MicroSD Card SOLD OUT
Raspberry Pi Zero BoardRaspberry Pi Zero Board
Mini-HDMI to HDMI AdapterMini-HDMI to HDMI Adapter
Micro USB "On the Go" to USB AdapterMicro USB "On the Go" to USB Adapter
8GB MicroSD Card Pre-Loaded with NOOBS
MicroSD to SD Card Adapter

 

Raspberry Pi Zero on element14

Want to learn more about the Pi Zero and what it can do? Check out our exclusive coverage right here at element14.

image

Overview of the Raspberry Pi Zero

Get all the facts about the smallest, slimmest Raspberry Pi in one page. Everything you need to know about the Zero.

image

Five Things You Need to Know About the Raspberry Pi Zero

You're bound to have a bunch of burning questions about the Zero, so we've answered the most common ones right here.

image

Raspberry Pi Zero Comparison Chart

Curious about how the Raspberry Pi Zero stands up alongside the rest of the fruitful family of single board computers? Here's a comparison chart.

image

Raspberry Pi Zero Retro Gaming System

Our first ultra-slim Pi project inside a big, fat, retro TV. We turn the Raspberry Pi Zero into a retro gaming hero -- and so can you by following our build along project.

  • raspberry pi zero
  • raspberry_pi
  • raspberry pi
  • pi_zero
  • raspberrypi
  • pi zero
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • fvan
    fvan over 10 years ago in reply to spannerspencer +8
    Sure thing:
  • Workshopshed
    Workshopshed over 10 years ago in reply to Workshopshed +7
    Some enhancements, note that the dimensions still need checking
  • fvan
    fvan over 10 years ago +7
    Made my own little mod While piggy-back wifi is nice, piggy-back USB hub is even better: The Pi is powered by the USB hub, and up to 4 dongles can be connected. Using low profile dongles keeps everything…
  • cstanton
    cstanton over 10 years ago in reply to hareeshgs

    You can connect to WiFi using an SPI WiFi adapter. It doesn't have to be USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hareeshgs
    hareeshgs over 10 years ago in reply to Problemchild

    Yes, exactly, the ambient we are having in Kerala (India) is 26 to 35 degrees.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to hareeshgs

    It would be interesting to know what kind of ambient temperature you have Hareesh?

    Over here it wouldn't be much more than 20C most of the time, to stand up to constant use in a hot country you may need that extra cooling especially in an enclosure

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to johnbeetem

    True I think the Ground plane probably did more than the connectors though from both the heat and generally calming things down electrically point of view.

     

    That Ethernet chip is rather flaky anyway

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 10 years ago in reply to Workshopshed

    It's a contentious and debate-able issue.

    Personally I think they get toasty, especially when enclosed. A heatsink isn't going to harm it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hareeshgs
    hareeshgs over 10 years ago in reply to rew

    I don't know, USB devices that drain more current will work directly eg., external HDD. Only option to connect to network is the USB port via WIFI dongle. We may have to use externally powered USB hubs for additional devices (as see on the making the smart TV ad).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to Problemchild

    John Alexander wrote:

     

    Do you think that the connectors offered any effective cooling John. The hottest thing on the board when I did the thermal imaging was the NIC/HUB chip which is now of course missing.

    I would say yes.  The original RasPi Model B 1.0 PC board had a design error that caused the LAN chip to overhead on many boards.  They fixed this on the 2.0 PCB and also added a lot of ground plane vias under the LAN chip to conduct heat to the ground plane.  This in turn conducts to the connector shells which then act as heat sinks.  Conduction cooling can be very useful for surface-mount devices.  Large connectors help, particularly if they can conduct to a metal case.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hareeshgs
    hareeshgs over 10 years ago in reply to johnbeetem

    For my B, I was using heat sinks+ cooling fan when using as an OSMC media centre.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hareeshgs
    hareeshgs over 10 years ago in reply to Workshopshed

    Dear Andy, Thanks for the pictures.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rew
    rew over 10 years ago in reply to johnbeetem

    If anything the "ethernetchip"  only ADDS to raspberry pi heating problems: It consumes around half the power budget of the whole 'pi.

     

    So... with a current specified at 160mA, the power that the module can draw is limited to 5V*160mA = 800mW. For a big chip like the BCM2835, 800mW will dissipate without heat sink without any trouble. (and that's assuming that ALL power will dissipate in the BCM2835 and RAM chip, which is probably close but not quite).

     

    P.S. Got an email 5 minutes ago: "shipped".... From UK will take a day or two to NL.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>