Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents Raspberry Pi 3 Model B Technical Specifications
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 22 Feb 2016 8:38 PM Date Created
  • Last Updated Last Updated: 10 May 2021 7:23 PM
  • Views 41478 views
  • Likes 15 likes
  • Comments 65 comments
Related
Recommended

Raspberry Pi 3 Model B Technical Specifications

imageNEW! Raspberry Pi 3 Model B
Comparison ChartFrequently Asked QuestionsUnboxing Video
40 Pin OutPi3 Video Arcade Project

 

         

image                                                                     
image
   

NEW! Raspberry Pi 3 Model B

   

Buy NowBuy NowBuy NowBuy Now

   

Learn More image

   

 

   

Key Improvements from Pi 2 Model B to Pi 3 Model B:

image Next Generation QUAD Core Broadcom BCM2837 64bit processor

image Processor speed has increased from 900MHz on Pi 2 to 1.2Ghz

image BCM43438 WiFi on board

image Bluetooth Low Energy (BLE) on board

image Upgraded switched power source up to 2.5 Amps (can now power even more powerful devices over USB ports)

 

Other Technical Specification:

image 40pin extended GPIO

image 4 x USB 2 ports

image 4 pole Stereo output and Composite video port

image Full size HDMI output

image CSI camera port for connecting the Raspberry Pi cameraRaspberry Pi camera

image DSI display port for connecting the Raspberry Pi touch screen displayRaspberry Pi touch screen display

image Micro SD port for loading your operating system and storing data

image Upgraded switched Micro USB power source (now supports up to 2.5 Amps)

image The same form factor as the Pi 2 Model BPi 2 Model B, - the only difference is the location of the onboard LEDs

  • tech specs
  • pi3
  • raspberry_pi_space
  • raspberry pi 3
  • technical specifications
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • spannerspencer
    spannerspencer over 10 years ago in reply to madshenriksen +3
    There's dedicated hardware for lots of things, but I'd certainly be interested in seeing if the Pi3 can be put to this kind of purpose -- my NAS is getting kind of old, and uses a lot more juice than a…
  • madshenriksen
    madshenriksen over 10 years ago in reply to spannerspencer +3
    Exactly Spanner Spencer. The Raspberry approach was chosen because it could fill my need at a very low cost, and with low power (I haven't look at the power consumption of other NAS hardware). I haven…
  • Problemchild
    Problemchild over 10 years ago in reply to cstanton +3
    Yes Chris. to be honest the software RAID under Linux has surpassed the speed of the HW implementations for years at least under x86 ... Obviously the ability to off load that function to some H/W is good…
  • clem57
    clem57 over 9 years ago in reply to alfredd

    Here is one source of cards and why they work/do not work: RPi SD cards - eLinux.org . Note this may be oldish

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wneo
    wneo over 9 years ago in reply to alfredd

    According to the datasheet for the Broadcom BCM2835 available here,

    The External Mass Media Controller (EMMC) is an embedded MultiMediaTm and SDTm card interface provided by ArasanTm. It is compliant to the following standards:

    • SDTm Host Controller Standard Specification Version 3.0 Draft 1.0

    • SDIOTm card specification version 3.0

    • SDTm Memory Card Specification Draft version 3.0

    • SDTm Memory Card Security Specification version 1.01

    • MMCTm Specification version 3.31,4.2 and 4.4

    As per this, Host Controller Standard Specification Version 3.0 Draft 1.0 implies UHS-I bus interface. So, you should be looking for a card that is microSDHC1 I (<32 GB) or microSDXC2 I (>32 GB) when it comes to capacity and Speed Class 10 (C10) or UHS Speed Class I (U1) when it comes to speed.

     

    1Secure Digital High Capacity
    2Secure Digital eXtended Capacity

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • alfredd
    alfredd over 9 years ago

    Hi,

    I got my Pi recently. I wanted to get a high speed MicroSD card for my Pi but I am unable to get any details on what Read and Write speeds are supported by the Pi 3 Model B.

    If anyone here has any idea, could you please let me know.

     

    Thanks.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to aonbreakin

    http://www.switchdoc.com/2014/08/ibeacon-raspberry-pi-scanner-python/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aonbreakin
    aonbreakin over 9 years ago

    Is it suitable for scan iBeacon by Bluetooth on board?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to edsoprano

    edsoprano does this help RASPBERRYPI3-MODB-1GB. - RASPBERRY-PI - Raspberry Pi 3 Modelo B | Newark element14 México

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • edsoprano
    edsoprano over 9 years ago

    hi, what is price in mexican pesos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    For a discussion of heat and the Raspberry Pi 3, see Raspberry Pi Operating Temperature Comparison (A+, B+, Zero, Pi 2, Pi 3)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Please see question below.  I was actually trying to find the operating temperature range as well.  For an "industrial" grade product, one would think the documentation would be up to professional standards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jimjulian
    jimjulian over 10 years ago

    Hello,

     

       What's the temperature operating range?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>