Raspberry Pi
  • Products
  • More
Raspberry Pi
Documents Raspberry Pi 2 Model B 1GB Technical Specifications
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 23 Jan 2015 4:01 PM Date Created
  • Last Updated Last Updated: 10 May 2021 7:09 PM
  • Views 32988 views
  • Likes 6 likes
  • Comments 62 comments
Related
Recommended

Raspberry Pi 2 Model B 1GB Technical Specifications

image

image

The Raspberry Pi 2 Model B 1GB
6X Faster

Learn More

 

Buy NowBuy Now

 

Benefits  image
Technical Specifications  image
Features  image

Benefits:

Get personal with your Pi. Welcome to the Raspberry Piimage 2, the single board computer that thinks it’s a home PC.

Enhanced Quad Core Processor and 1GB RAM now provides you with the opportunity to:

  • Build your own workstation – create and manage your documents and spreadsheets with ease using LibreOfficeimage
  • Faster and more enjoyable gaming – experience less lag and more seamless gaming in all your favourites. Can’t wait to demolish buildings in Minecraftimage, trigger your TNT now and be amazed by the results!
  • No more buffer face – boots up Raspbian in less than half the time as the Model B+
  • More power for your favourite projects – create Space Progammes, Time Lapse Videos, GPS tracking, HD audio and lots more with a full ecosystem of supporting accessories.
  • All your previous Raspberry Pi projects are 100% backward compatible with the new Raspberry Pi 2 Model B 1GB

Technical Specifications:

  • Broadcom BCM2837 Arm7 Quad Core Processor powered Single Board Computer running at 900MHz
  • 1GB RAM
  • 40pin extended GPIO
  • 4 x USB 2 ports
  • 4 pole Stereo output and Composite video port
  • Full size HDMI
  • CSI camera port for connecting the Raspberry Pi camera
  • DSI display port for connecting the Raspberry Pi touch screen display
  • Micro SD port for loading your operating system and storing data
  • Micro USB power source

Raspberry Pi 2 Model B Features:

  • Broadcom BCM2837Arm7 Quad Core Processor powered Single Board Computer running at 900MHz
  • 1GB RAM so you can now run bigger and more powerful applications
  • Identical board layout and footprint as the Model B+, so all cases and 3rd party add-on boards designed for the Model B+ will be fully compatible.
  • Fully HAT compatible
  • 40pin extended GPIO to enhance your “real world” projects. GPIO is 100% compatible with the Model B+ and A+ boards. First 26 pins are identical to the Model A and Model B boards to provide full backward compatibility across all boards.
  • Connect a Raspberry Pi camera and touch screen display (each sold separately)
  • Stream and watch Hi-definition video output at 1080P
  • Micro SD slot for storing information and loading your operating systems.
  • Advanced power management:
  • You can now provide up to 1.2 AMP to the USB port – enabling you to connect more power hungry USB devices directly to the Raspberry PI. (This feature requires a 2Amp micro USB Power Supply)
  • 10/100 Ethernet Port to quickly connect the Raspberry Pi to the Internet
  • Combined 4-pole jack for connecting your stereo audio out and composite video out
  • raspberry
  • broadcom bcm2837
  • the
  • pi
  • 2
  • new
  • b
  • raspberry_pi_space
  • technical
  • 1gb
  • model
  • specifications
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • alnico
    alnico over 10 years ago in reply to Former Member +1
    I moved over 1000 miles from it, unfortunately. Fortunately, I have a buddy that is close and can buy and ship to me cheaper than the element 14 'personal' partner does.
  • shabaz
    shabaz over 10 years ago in reply to Former Member +1
    No full schematic is publicly available (it is not open source). But yes, you can directly connect 5V DC to the 40-way connector if you wish to.
Parents
  • Former Member
    Former Member over 10 years ago

    I am interested in obtaining a low-power pc for use in managing a small IoT installation at unattended remote locations and have seen references to a number of ready made systems comprising a RPi as a base-station/internet access, and low-power (1 to 2 mA) Arduino nodes.    I am seeking detailed info on how to run a RPi in unattended, using a minimum power configuration, especially as mains power may not be available 24/7.    I see both the PR and specification on your site state the RPi 2 B has 'Advanced Power Management'.  Can you send me a links to info/articles on this feature ?    Having googled around for info on RPi power consumption I have seen various 3rd party articles, from which I gather under standard conditions the A+ takes a bit less power then the Pi 2 (http://raspi.tv/2015/raspberry-pi2-power-and-performance-measurement).  However, I would guess a base-station IoT monitoring task requires little compute power (was thinking for simple single-node locations, a single Arduino system sufficient to both collect & store data, and allow an internet connection to access it) and wanted to know more how 'Advanced Power Management' can help that, and if it was possible to easily disable 3 cores to save the 150mA estimated in above link ?    (If I can get a RP 2 to run on power closer to the A+, obviously I would prefer the RP 2 on account of its greater capability for other uses)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Former Member
    Former Member over 10 years ago

    I am interested in obtaining a low-power pc for use in managing a small IoT installation at unattended remote locations and have seen references to a number of ready made systems comprising a RPi as a base-station/internet access, and low-power (1 to 2 mA) Arduino nodes.    I am seeking detailed info on how to run a RPi in unattended, using a minimum power configuration, especially as mains power may not be available 24/7.    I see both the PR and specification on your site state the RPi 2 B has 'Advanced Power Management'.  Can you send me a links to info/articles on this feature ?    Having googled around for info on RPi power consumption I have seen various 3rd party articles, from which I gather under standard conditions the A+ takes a bit less power then the Pi 2 (http://raspi.tv/2015/raspberry-pi2-power-and-performance-measurement).  However, I would guess a base-station IoT monitoring task requires little compute power (was thinking for simple single-node locations, a single Arduino system sufficient to both collect & store data, and allow an internet connection to access it) and wanted to know more how 'Advanced Power Management' can help that, and if it was possible to easily disable 3 cores to save the 150mA estimated in above link ?    (If I can get a RP 2 to run on power closer to the A+, obviously I would prefer the RP 2 on account of its greater capability for other uses)