Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi Pico
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 13 Jan 2021 5:44 PM Date Created
  • Last Updated Last Updated: 27 Jan 2021 3:48 PM
  • Views 21103 views
  • Likes 20 likes
  • Comments 128 comments
Related
Recommended

Raspberry Pi Pico

image

Raspberry Pi Pico

 

Buy NowBuy Now
Buy Now from CPCBuy Now from CPC

 

We are very excited to introduce the all new Raspberry Pi Pico, a tiny, $4, MicroPython and C/C++ board with custom RP2040 silicon.

This is the first product from the Raspberry Pi Foundation built with their in house designed RP2040.

At $4 and available individually or even available on reels, this Raspberry Pi is the next step in home and industrial products.

Looking at the edge of the PCB you can see the Raspberry Pi Pico has been designed to be used with header pins or soldered directly onto your products PCB.

James Adams, Chief Operating Officer, Raspberry Pi Trading, said:

“This is the start of an exciting new era for Raspberry Pi. With Raspberry Pi Pico, and RP2040, we have been able to draw on insights drawn from a decade of using other vendors’ microcontrollers, and to create an innovative silicon platform for our customers. People have used Raspberry Pi to create a broader spread of projects and products than we could have imagined a decade ago; we’re sure the same will be true of Raspberry Pi Pico.”

image

Raspberry Pi Pico Specifications:

  • GPIO and Debug Pins
  • RP2040 Microcontroller
  • Two cores clocked at 133MHz
  • 256KB RAM
  • 2MB of On-board Flash Memory
  • Micro-USB B Port for Power, Data and Reprogramming of the Flash memory.

 

Raspberry Pi Pico Peripherals:

  • I2C x4
  • SPI x2
  • PWM x2
  • UART x2
  • Timer
  • RTC
  • ADC & TS

 

Raspberry Pi Pico Dimensions:

21mm (W) x 51.3mm (L) x 3.9mm (H)

 

Raspberry Pi Pico GPIO Pinout

image

 


The 40 pin 21x51 'DIP' style 1mm thick PCB with 0.1" through-hole pins also with edge castellations

  • Exposes 26 multi-function 3.3V General Purpose I/O (GPIO)
  • 23 GPIO are digital-only and 3 are ADC capable
  • Can be surface mounted as a module
  • 3-pin ARM Serial Wire Debug (SWD) port


First Product built on Raspberry Pi designed Silicon - Meet the RP2040

Raspberry Pi Pico is built around the brand-new Raspberry Pi RP2040 microcontroller, delivering a flexible, highly affordable development platform that can also be directly deployed into end products, reducing time-to-market. RP2040 offers high performance for integer workloads, a large on-chip memory, and a wide range of I/O options, making it a flexible solution for a wide range of microcontroller applications.
Professional design engineers who are already comfortable working with Raspberry Pi will easily adopt the Raspberry Pi Pico and appreciate its ease of use and affordability.

image

RP2040 Microcontroller.
RP2040 is a low-cost, high-performance microcontroller device with flexible digital interfaces. Key features:


• Dual Cortex M0+ processors, up to 133 MHz

• 264 kB of embedded SRAM in 6 banks

• 30 multifunction GPIO

• 6 dedicated IO for SPI Flash (supporting XIP)

• Dedicated hardware for commonly used peripherals

• Programmable IO for extended peripheral support

• 4 channel ADC with internal temperature sensor, 0.5 MSa/s, 12 bit conversion

• USB 1.1 Host/Device




Developer tools
Simple drag and drop programming via micro-USB. 3-pin Serial Wire Debug (SWD) for interactive debugging. Comprehensive C SDK, mature MicroPython port, and extensive examples and documentation.

image

Power
On-board power supply to generate 3.3V for RP2040 and external circuitry. Wide input voltage range, from 1.8V to 5.5V, giving designers the flexibility to select their preferred power source.


Raspberry Pi Pico Size and Layout:




image

  • raspberry pico
  • gpio
  • raspberry pi pico
  • farnell
  • pico
  • gpio pinout
  • new raspbery pi
  • dimensions
  • pi_pico
  • raspberry_pi
  • raspberry_pi_pico
  • raspberry pi
  • raspberrypi
  • rp2040
  • raspberry pi pico gpio
  • rpi
  • technical specification
  • specification
  • pinout
  • pi pico gpio
  • pi pico
  • cpc
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 5 years ago +12
    Certainly an interesting device, and I'm sure it will become very popular. I must say that personally I'm not a fan of MicroPython - or any interpreted embedded languages. I feel that the real strength…
  • Workshopshed
    Workshopshed over 5 years ago +11
    Looks to be a powerful little board in a nice form factor. I love the fact it has sensible mounting holes even if that does make the silkscreen for those pins a little hard to read. I'd be interested to…
  • Fred27
    Fred27 over 5 years ago +10
    It looks like other companies (the usual suspects) are making boards based on the RP2040 too. https://www.cnx-software.com/2021/01/21/third-party-raspberry-pi-rp2040-boards-from-arduino-adafruit-sparkfun…
  • robogary
    robogary over 5 years ago

    ROFL - I bit, looks cool. Who can beat it at $4 ?

    Click BUY NOW, cost $7.99 ...none available 

    Always a bridesmaid, never a bride :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago in reply to cstanton

    There is a wide range of experiences - as usual it depends on how well the corporate interests align with each other. I've had manufacturers where I couldn't get the time of day, but I've also had manufactures that fly a team of engineers in to discuss how they can modify their chip to make it suit our application better.

    It shouldn't be a surprise that chip manufacturers are careful with their IP. A lot of money gets spent reverse engineering chip designs, so there is a big motive to shortcut that process by using industrial espionage and consequently a big motive to prevent it.

    In this case the Raspberry Pi folks chose companies that were unlikely to try and clone the chip, and they only gave them a few weeks of advance notice of information that was going to be released publicly anyway, so they could afford to take the risk of reduced IP protection processes.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 5 years ago in reply to cstanton

    cstanton  wrote:

     

    >It sounded like exaggeration though

     

    It really isn't. 7 years ago I experienced similar, and it's obviously burned other people as well...

     

    I've been there. Some big companies act like they are doing YOU a favour, and make you jump through all the hoops they come up with. That can add up to significant costs for smaller companies.

     

    Also, "Signing an NDA" is never that easy - lawyer costs can add up quickly, and often even if you do get your lawyers pointing out dangerous things, the big companies won't budge: "that's our NDA, take it or leave it".

     

    I think the point was that dealing with some large companies can get very cumbersome, time consuming and expensive.

     

    Maybe that part was directed towards a specific company they had just dealt with, along with some strong hinting meant specifically for them.

     

    Best,

    -Nico

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 5 years ago in reply to jomoenginer

    It's been the VideoCore mainly, for a long time developers have had to work with the 'binary blob' for the GPU component.

     

    Raspberry Pi Trading have done considerable efforts with people to work on having open source OpenGL and OpenCL support for the VideoCore rather than resorting to the blob, though I believe Broadcom still have some lockdown limits on it.

     

    It's definitely not through lack of trying and I'd say Raspberry Pi have done great work to handle the limitations they've had with the platform in this regard and continue to work towards their goals, especially as an education platform which is their main aim.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 5 years ago in reply to BigG

    BigG  wrote:

     

    Mind you, RPI's approach has also drawn criticism from many open source hardware developers for showing favouritism.

    Perhaps this is due to traditionally the RPI's are not actually Open Source unlike something like a Beaglebone. They keep their chip design as propriety and do not let folks have access to it. I would image NDAs are involved if they did allow access to the secret sauce.

     

    Although fun to do so, bashing the "terrible chip giants" in a public video might not be the most productive means of getting things done with them.  In the end, it really is for a $4 dev board. I could be wrong though.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 5 years ago in reply to michaelkellett

    Yep, this tends to happen when young companies are still growing and thriving. Mind you they did hit on the two key elements that are important to any development led business... namely will this cost me time and money. When organisations add in layers or departments that have separate budgets, these management layers tend to focus on justifying their worth by keeping busy (i.e. lots of meetings to discuss things). However, there is a sting in the tail. Young companies tend to forget the other important criteria, which has serious teeth but is seldom drawn, namely risk or a costly failure.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 5 years ago in reply to shabaz

    It did seem a bit childish - Adafruit can do their bit and it's useful, but they aren't going to be building many state of the art wafer fabs. I'm quite impressed by just how many new chips and how much support the big companies like ST, Analog, TI etc manage to pump out.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to cstanton

    Are we talking about the same segment in the video?

     

    To summarise, it amounts to Adafruit feeling they have too many zoom calls with marketing, and an insistence that they spend a week in-person which must be an exaggeration, because how would it scale if each semiconductor manufacturer spent a week with each potential customer?

     

    EDIT: Also they talk about NDAs. Pretty sure it doesn't take five zoom calls to exchange their pre-prepared NDAs. I've seen a 'battle of the forms' where both sides want the other side to use their NDA, but this isn't unusual, and very quick for Adafruit to get their lawyers to review, if they are so agile.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 5 years ago in reply to shabaz

    >It sounded like exaggeration though

     

    It really isn't. 7 years ago I experienced similar, and it's obviously burned other people as well, and that experience has stayed with them and likely isn't giving the companies another opportunity/chance.

     

    It's mainly very different now, partly because it's been forced to be (thankfully). That's all I'm going to say.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 5 years ago in reply to jomoenginer

    I agree there were some great comments. I think they were really taking pot shots at their national champions, who have not really had a need to evolve their business models. In my opinion, the company who is doing things differently, when it comes to launching new products is Nordic Semiconductor. Another one, although I do not know much about them, so I could be wrong, is CEVA. Both appear to work off some sort of licensing model.

     

    Mind you, RPI's approach has also drawn criticism from many open source hardware developers for showing favouritism.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>