Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi Pico
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 13 Jan 2021 5:44 PM Date Created
  • Last Updated Last Updated: 27 Jan 2021 3:48 PM
  • Views 21101 views
  • Likes 20 likes
  • Comments 128 comments
Related
Recommended

Raspberry Pi Pico

image

Raspberry Pi Pico

 

Buy NowBuy Now
Buy Now from CPCBuy Now from CPC

 

We are very excited to introduce the all new Raspberry Pi Pico, a tiny, $4, MicroPython and C/C++ board with custom RP2040 silicon.

This is the first product from the Raspberry Pi Foundation built with their in house designed RP2040.

At $4 and available individually or even available on reels, this Raspberry Pi is the next step in home and industrial products.

Looking at the edge of the PCB you can see the Raspberry Pi Pico has been designed to be used with header pins or soldered directly onto your products PCB.

James Adams, Chief Operating Officer, Raspberry Pi Trading, said:

“This is the start of an exciting new era for Raspberry Pi. With Raspberry Pi Pico, and RP2040, we have been able to draw on insights drawn from a decade of using other vendors’ microcontrollers, and to create an innovative silicon platform for our customers. People have used Raspberry Pi to create a broader spread of projects and products than we could have imagined a decade ago; we’re sure the same will be true of Raspberry Pi Pico.”

image

Raspberry Pi Pico Specifications:

  • GPIO and Debug Pins
  • RP2040 Microcontroller
  • Two cores clocked at 133MHz
  • 256KB RAM
  • 2MB of On-board Flash Memory
  • Micro-USB B Port for Power, Data and Reprogramming of the Flash memory.

 

Raspberry Pi Pico Peripherals:

  • I2C x4
  • SPI x2
  • PWM x2
  • UART x2
  • Timer
  • RTC
  • ADC & TS

 

Raspberry Pi Pico Dimensions:

21mm (W) x 51.3mm (L) x 3.9mm (H)

 

Raspberry Pi Pico GPIO Pinout

image

 


The 40 pin 21x51 'DIP' style 1mm thick PCB with 0.1" through-hole pins also with edge castellations

  • Exposes 26 multi-function 3.3V General Purpose I/O (GPIO)
  • 23 GPIO are digital-only and 3 are ADC capable
  • Can be surface mounted as a module
  • 3-pin ARM Serial Wire Debug (SWD) port


First Product built on Raspberry Pi designed Silicon - Meet the RP2040

Raspberry Pi Pico is built around the brand-new Raspberry Pi RP2040 microcontroller, delivering a flexible, highly affordable development platform that can also be directly deployed into end products, reducing time-to-market. RP2040 offers high performance for integer workloads, a large on-chip memory, and a wide range of I/O options, making it a flexible solution for a wide range of microcontroller applications.
Professional design engineers who are already comfortable working with Raspberry Pi will easily adopt the Raspberry Pi Pico and appreciate its ease of use and affordability.

image

RP2040 Microcontroller.
RP2040 is a low-cost, high-performance microcontroller device with flexible digital interfaces. Key features:


• Dual Cortex M0+ processors, up to 133 MHz

• 264 kB of embedded SRAM in 6 banks

• 30 multifunction GPIO

• 6 dedicated IO for SPI Flash (supporting XIP)

• Dedicated hardware for commonly used peripherals

• Programmable IO for extended peripheral support

• 4 channel ADC with internal temperature sensor, 0.5 MSa/s, 12 bit conversion

• USB 1.1 Host/Device




Developer tools
Simple drag and drop programming via micro-USB. 3-pin Serial Wire Debug (SWD) for interactive debugging. Comprehensive C SDK, mature MicroPython port, and extensive examples and documentation.

image

Power
On-board power supply to generate 3.3V for RP2040 and external circuitry. Wide input voltage range, from 1.8V to 5.5V, giving designers the flexibility to select their preferred power source.


Raspberry Pi Pico Size and Layout:




image

  • raspberry pico
  • gpio
  • raspberry pi pico
  • farnell
  • pico
  • gpio pinout
  • new raspbery pi
  • dimensions
  • pi_pico
  • raspberry_pi
  • raspberry_pi_pico
  • raspberry pi
  • raspberrypi
  • rp2040
  • raspberry pi pico gpio
  • rpi
  • technical specification
  • specification
  • pinout
  • pi pico gpio
  • pi pico
  • cpc
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 5 years ago +12
    Certainly an interesting device, and I'm sure it will become very popular. I must say that personally I'm not a fan of MicroPython - or any interpreted embedded languages. I feel that the real strength…
  • Workshopshed
    Workshopshed over 5 years ago +11
    Looks to be a powerful little board in a nice form factor. I love the fact it has sensible mounting holes even if that does make the silkscreen for those pins a little hard to read. I'd be interested to…
  • Fred27
    Fred27 over 5 years ago +10
    It looks like other companies (the usual suspects) are making boards based on the RP2040 too. https://www.cnx-software.com/2021/01/21/third-party-raspberry-pi-rp2040-boards-from-arduino-adafruit-sparkfun…
  • sokol07
    sokol07 over 5 years ago

    I know they are available elsewhere but I wanted to spend money from Project14 getting a bunch of them... Maybe not 25 but a few. image

    And there is some kind of a problem with Pico on Polish Farnell - the search bar can't find it, it can't be found by number, when I got to the product site from this article it was first unavailable, than available in future, after delivery, than unavailable again and now there is only information that there is no price or availability information.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 5 years ago

    If you are in the US and near a Micro Center that has the Pico in stock, you can grab it for just $2.00,

    https://www.microcenter.com/product/632771/raspberry-pi-pico

     

    I think I am ready that correct.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kk99
    kk99 over 5 years ago in reply to sokol07

    It is available in botland.pl image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sokol07
    sokol07 over 5 years ago

    Aaaaand it's still unavailable in Polish Farnell store... image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bernhardmayer
    bernhardmayer over 5 years ago

    I think this is a very interesting board.

    Just want to add a link to my project: PicoMKRAdapter - connect Arduino MKR Shields to Raspberry Pi Pico to use Arduino MKR Shields with the Pico.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 5 years ago in reply to jomoenginer

    Hi jomoenginer was your last reply meant for neerajrd82 , rather than me? image

     

    As you show, the build process does indeed produce a range of file formats, including .hex!

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 5 years ago in reply to neilk

    Is there something you are seeing that I am not?

     

    From the build I have run, not only is a .uf2 file create, but a .hex, bin, dis, and .elf files are created. This is noted in Chapter 7 of the Getting Started guide.

    Note regarding the UF2  (USB  Flashing  Format) :

    UF2 (USB Flashing Format) is a file format, developed by Microsoft, that is used for flashing the RP2040 board overUSB. More details can be found on the

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neerajrd82
    neerajrd82 over 5 years ago

    Everything i have read about this board in documentation is good enough. But only thing which can trouble us during the course of development is in near future is the absence of support of *.hex or *.bin file. Raspberry Pi Pico board designers should work out this issue immediately.    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 5 years ago in reply to robogary

    The listings are... being updated, they'll settle once stock's sorted out. Or should be image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • BigG
    BigG over 5 years ago in reply to cstanton

    Another interesting insight is that the companies Raspberry PI brought in early were both product designers as well as being product resellers. In other words, this would be similar to what AVNET achieved, working with Microsoft to develop and resell the Azure Sphere products.... although I suspect there were a lot more meetings involved (and probably NDA's signed too).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>