Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116448 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • kcollins@us.ibm.com
    kcollins@us.ibm.com over 9 years ago

    I get errors after I run "sudo apt-get install matchbox-keyboard"... There are multiple error messages after the message Get:3 http://mirrordirector.raspian.org/raspian/ jessie/main.... it says E: Failed to fetch http://mirrordirector.raspian.rog/raspian/pool/main/libf/libfakekey/libafakey0_0.1-8.1_armhf.deb Size mismatch I ran sudo apt-get update, and I ran sudo apt-get upgrade, then I ran sudo apt-get install matchbox-keyboard, but I still get the same error. Any ideas what I should do to get the on screen keyboard to work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Macmuchmore
    Macmuchmore over 9 years ago

    I just got the Raspberry Pi 7" Touchscreen Display (using it with a Raspberry Pi 3 and the latest Raspbian Jessie) and on the box it says the screen resolution is 800x480. In the System tab of the Raspberry Pi Configuration, it lists the resolution at 720x480.

     

    1) Why is it not going to 800x480 automatically?

    2) If I attempt to change the resolution in the System tab, in the dropdown it does not list the 800x480 resolution.

    3) Can I actually get the Pi to display 800x480, or is 720x480 it? If I can, how do I change the output to 800x480?

    4) if the screen is only 720x480, why does the box say 800x480?

     

    Thanks,

    Macmuchmore

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wd0ug
    wd0ug over 9 years ago in reply to wd0ug

    After some searching, I found the answer that works so I'll post it here for others with the same problem.  It's not my solution, it is attributed to a user named 'Rasadmin' so thanks.  This disables the screen timeout on the 7" display:

    Step 1: sudo nano /etc/lightdm/lightdm.conf

    In that file look for [SeatDefaults]

    Step 2: Insert this line:

    xserver-command=X -s 0 dpms

    Now save the file and re-boot.  The display stays lit all the time.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • iron.invin
    iron.invin over 9 years ago

    I bought one of these screens some years ago, and it came with a v1.0 controller board that didn't support brightness settings.

    Can I ask if this comes with the v1.1 board now?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wd0ug
    wd0ug over 9 years ago in reply to fvan

    Thanks, but that does not work.  Any other things to try?  I'm running the current version of NOOBS that came with the Raspberry Pi 3. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 9 years ago in reply to wd0ug

    A quick Google search returns the following procedure: Disable screensaver and screen blanking Raspberry Pi - ETCwiki  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wd0ug
    wd0ug over 9 years ago

    I wrote a clock program to display time and weather.  When I let it run, the 7" display turns off after a few minutes.  How can I force the display to stay on all the time?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • njmoz
    njmoz over 9 years ago in reply to fvan

    Hi

     

    Jessie

     

    Internet now stable and on

    Ive done an update and upgrade then re installed matchbox keyboard ... all

    this time without error messages  Ive even rerun matchbox keyboard and it

    indicates I have latest version

     

    I have powered down and back up again but it not in the accessory directory

    like before , did a seach (matchbox) in root and it not there

     

     

     

    Kind Regards

     

     

     

    Neil Jackson (Mba)

    +44 (0)20 3239 9074

    +27 (0) 71 5090 107

    Skype njchongoene

    neil@uk-esc.com

    www.uk-esc.com

     

     

    We Develop Your Business & Your Future

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 9 years ago in reply to njmoz

    Yes, but which distribution/version? Raspbian Wheezy, Raspbian Jessie, Ubuntu MATE, ... etc ?

     

    I would suggest you download the latest Raspbian Jessie and try again: https://www.raspberrypi.org/downloads/raspbian/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • njmoz
    njmoz over 9 years ago in reply to fvan

    Linux .. Phython 3 IDLE

     

    Im running it again I think its the internet failing over , it now stuck at

    unpacking raspberrypi-kernel been there 30 min

     

    Kind Regards

     

     

     

    Neil Jackson (Mba)

    +44 (0)20 3239 9074

    +27 (0) 71 5090 107

    Skype njchongoene

    neil@uk-esc.com

    www.uk-esc.com

     

     

    We Develop Your Business & Your Future

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>