Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116460 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • e14 Contributor
    e14 Contributor over 10 years ago

    I'm having problems with the keyboard that is recommended to install .

    once I open my desktop icons disappear.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spydergto
    spydergto over 10 years ago

    I want to replace item number 4 the stand off 's with a shorter based one i am looking to "squish" as much as possible everything and i will eventually desolder a pi 3 board for the smallest possible fit however i need to know what the screw size on these is that goes into the metal holder of the screen and i see that its pi sized 3 # screw threw the pi into the stand off ? where might i get a kit ? i bought a 2 and 3 mm small stand off kit on ebay for other projects but need i suppose 3 mm screw into the stand off with 3.5 mm into the board and short stand off ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wreeve
    wreeve over 10 years ago

    The touchscreen display seems to work okay except with one application that does not use the touchscreen functions.

     

    In this case, the display does not properly center (runs off the right side of the screen) and some text is oversized. I spent several hours trying different settings in config.txt and could move it slightly by adjusting overscan (both enabled and disabled) and also by setting hdmi_cvt to 800 x 480 with 60 Hz rate. I also tried several different hdmi_mode settings. However, the display never gets centered. Also, screenshots (using scrot or screenshot) are worse yet (they do not shift at all with different settings).

     

    I have a Tontec 7" LCD with 1024 x 600 resolution and it works fine. All I had to do was setup hdmi_cvt and it worked without any other adjustment.

     

    Has anyone else encountered a problem like this with the touchscreen display or have a suggested solution?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • chronos70
    chronos70 over 10 years ago

    Anyone know what the operating temperature range is for the display? I'm planning a device that will have to withstand the summer in Florida. That means sitting in direct sunlight. Will the extreme heat warp or damage anything?

     

    TIA

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Yes it does have its own power. Normally this will not be a problem. But I have had times where I had to unplug the screen power. But after that the screen will not come back. You have to reboot the PI to get the screen back.

    Is there no way to bring the screen back without a reboot?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    Do you have the screen power off Pi? I would separate the power for the 7 inch screen.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi all. The screen works very well. I have 2 issues that I hope somebody can help with.

     

    1) If the screen power goes off I can not get the screen back. I have to reboot the PI to get the screen to work again.

    2) When using VNC to remote control the desktop. The screen will not turn off (screen saver). I have to touch the screen after disconnecting from the PI for it to switch off.

     

    I hope somebody can give me some help to fix these 2 problems.

     

    Regards.

     

    Jaco.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 10 years ago in reply to shabaz

    I confirm the orientation can be changed in software. Not ideal as shabaz mentioned due to the viewing angles, but certainly not bad or unworkable either! I never even noticed there was an issue, to be honest.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    Hi Jay,

     

    I'n sure the touchscreen orientation can be changed in software, I've just never tried it.

    If you're happy with the reduced view angle then

    according to this link Official 7" Raspberry Pi Touch Screen FAQ - Announcements - Pimoroni Buccaneers

    they state that the orientation of the display and the touchscreen can be rotated.

    <snippet>:

    To do this, open /boot/config.txt in your favourite editor and add the line:

     

    lcd_rotate=2

    This will rotate both the LCD and the touch coordinates back to the right rotation for our display stand.

    Don't use the documented display_rotate, it performs a performance expensive rotation of the screen and does not rotate the touch input.

     

    Personally I'd rotate the entire unit and enclosure if possible, but I understand that may not be feasible if you've bought some enclosure with integrated camera.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    This is a real crummy way to send out a product for the public !

     

    The enclosure is arranged incorrectly, or the screen is arranged incorrectly, and either issue has no minor fix that will get the unit back to function without requiring additional parts/expense, or looking bad.

     

    This is not good, the unit cannot be flipped upside down, as the integrated camera mount will be on the bottom and will not be able to mount it.

    Alternatively, the screen cannot simply be turned upside down to get the orange cable around, because the Pi will then lose it's enclosure opening for the USB/Network/Power.

     

    Maybe I could leave the Pi unmounted and flip that back around so the ports will gain access through the enclosure , but then the display and camera ribbons will be out of orientation, looks like that would require a longer display ribbon for more money and delays.

     

    So the plastic enclosure is the part that was incorrectly arranged. Has this been updated?

    Now I'll have to go back to the retailer and open every box of enclosures, looking for the correct orientation. so I won't have to totally hack up this enclosure to simply get it to be functional.

    It's going to be sad if the whole batch at the store is the wrong orientation.

     

    To accommodate the faulty enclosure, rotation of the touchscreen by 180degrees would solve touchscreen/control issue, and then simply deal with the potential view angle situation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>