Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116461 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    Jay Johnson wrote:

     

    The display comes in 180degree rotated, but I was able to get that fixed...

     

    But the touchscreen control needs to be rotated 180degrees.

     

     

    Hi Jay,

     

    If your display is oriented with the orange flex connection at the top, then it is the wrong way around (viewing angles are impacted).

    The optimal orientation is with the orange flex connection at the bottom (try it, you'll notice a large visual difference).

    With the correct orientation, you do not need to rotate in software.

    There are some enclosures that incorrectly have the flex connection at the top, this is because the raspberry pi foundation originally messed up with their messaging.

    You can still probably fix that, by just turning everything up side down (and fashion your own modifications to the enclosure as needed).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to smudger

    Well I found Virtual Keyboard for the Raspberry Pi which explains how to setup your own menu. I really do not know why it does not show up?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    The display comes in 180degree rotated, but I was able to get that fixed...

     

    But the touchscreen control needs to be rotated 180degrees.

     

    I see the link to rotate 90 degrees, but it's done with an XY swap. That will not be correct to rotate 180degrees with.

     

    ? Anyone have a link to tutorial on rotating the touchscreen controls 180degrees(and not the xy swap)?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • smudger
    smudger over 10 years ago in reply to smudger

    But then again ... after updating the f/w and executing apt-get update/upgrade again in case and rebooting Menu -> Accessories still doesn't have a Keyboard entry.

     

    Back to square one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • smudger
    smudger over 10 years ago in reply to smudger

    Ah OK. Found it. I'd forgotten about the firmware upgrade process as I haven't used that for over a year. Use it or lose it!

     

    Thanks Clem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • smudger
    smudger over 10 years ago in reply to clem57

    Please explain. Your comment is rather useless as it stands.

     

    Software is as updated as possible and hardware is latest. So what needs upgrade?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to smudger

    rpi-upgrade is needed!smudger

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • smudger
    smudger over 10 years ago

    OK Touchscreen working fine.

     

    Executed apt-get update & apt-get upgrade, installed package for matchbox-keyboard, rebooted.

     

    Menu -> Accessories doesn't have an entry for Keyboard!

     

    However I can run /usr/bin/matchbox-keyboard and the virtual keyboard appears.

     

    Running 2016-05-17-raspbian-jessie.img on Raspberry Pi 3 model B

     

    Has the Menu item been re-sited, if so where? I can't find it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi,

     

    I'm using the 7" touchscreen display in an Python-Programm mainly based on the pygame Python modules.

    For the user-interface I use image-rectangles and the function ... if Button.collidepoint(mousex, mousey)): ...

    When starting the program from the desktop or from the Python developmentsystem everything works perfect.

     

    The program (torsionsensor.py) is thought to run per autostart when the system is booted. That is realized

    with this lines at the end of the /etc/rc.local:

    ...

    sudo python /home/pi/python-programs/torsionsensor.py &

    exit 0

     

    The program starts running at the end of the boot-process as it should do. But now the touch-position seems

    to be severely out of calibration. The mouse cursor is positioned at the upper left corner of the display at

    the beginning. When touching the screen somewhere and moving the finger on the screen the mouse-cursor will

    follow this contact in that same almost constant distance (x- and y- axis).

     

    I then added the line:

    pygame.mouse.set_pos([WINDOWHALFWIDTH,WINDOWHALFHEIGHT])   ## [400,240]

    to the begin of the program which forces the mouse-cursor to the center of the display at the beginning.

    Then the cursor will jump to the finger-position when touching the screen and will follow this position -

    but not perfectly correct. The cursor moves further than the finger, so it reachses the screens edges

    (left, right, top, bottom) earlyer.

    This can be managed by applying a scaling factor and repositioning the cursor from within the program.

    Unfortunately there ist still a problem that the program will abort when the cursor reaches the left edge

    of the screen or sometimes randomly.

    Overscan is disabled in the raspi-config.

     

    For me it seems to be some mismath in the comunication of the tough-cursor of the display and the

    mouse-cursor of the raspbian - system.

     

    Do you have some idea how I can avoid all this re-positioning and rescaling - stuff and get a correct

    positioning of the mouse-cursor?

     

    Thank you for any hint or help!

     

    Jürgen M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    Nope, Yup and correct.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>