Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116537 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Hello Alex and everybody,

    I cant be called an expert, and I have assembled my new RPi touch display "botom up" to allow the cables (Power, hdmi...) to be on the top, so I had to rotate the display together with the touch screen feature of course !

    I found this post searching for an How to ...

    Inspired by your above indications (September 11), I have used : "display_rotate=2" in /boot/config.txt to make display rotate 180°. So far so good !

    I still had to rotate the touch screen part. And then a simple derivation of the changes indicated in the /usr/share/X11/xorg.conf.d/10-evdev.conf file failed.

    I could manage to find a way by adding this section:

    Section "InputClass"

            Identifier "RPi Touch"

            MatchDevicePath "/dev/input/event*"

            Option "InvertX" "1"

            Option "InvertY" "1"

            Driver "evdev"

    EndSection

    I used : MatchDevicePath "/dev/input/event*", instead of MatchDevicePath "/dev/input/event0" by analogy with the other sections of the file ;

    I added the line Driver "evdev"  for the same reasons.

    I am no sure of which of both changes solved the case (I'd bet on the ''driver' line), but it worked finally !

    Thank you Alex for these indications which inspired me !  image

     

    Edit : Oh no ! this also rotated the touch pad of my Rii keyboard !  i think i will go back to start (assembly of the display)...

    Edit 2 : Got confirmation that the wrong orientation upside down was a bug, returning sreen to seller, who will ship another one, hopefully not  bugged !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Thanks David, excellent!

     

    -Pete.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    The instructions given on this page are INCOMPLETE (as at 12/Jan/2016).  In Step 7 it shows the GND (black) and +5V (red) jumper cables connecting between the Raspberry Pi and the display adapter board.  However it does not show the other two jumper cables.  These two more jumper cables are not just spare - they ARE REQUIRED.  The SCL and SDA signals must also be connected between the two boards.  THEN the display should work.  This additional information I found at Raspberry Pi 7" touch screen assembly guide – The Pi Hut

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    How to adjust this displayer brightness?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    The kit includes four jumper wires, but the instructions only detail use of two. What are the other two wires for?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jack.chaney56
    jack.chaney56 over 10 years ago in reply to e14 Contributor

    The obvious answer could sound like blaspheme... "Get rid of Microsoft".  There I said it, now I have to watch for the black helicopters.

     

    Have a nice time,

    Jack

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    I just received a version V1.1 of this display and it doesn't work with Windows 10 IOT. When connecting and "old" V1.0 version, windows shows up on the display but with the new version Windows only shows via HDMI.

     

    When using Raspbian everything works fine on my 7"display so it's not a connection issue.

     

    Any ideas?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago

    Best open new question under raspberry PI Paul Regan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Setting up a new Raspberry Pi 7" Touchscreen Display.

     

    Downloaded updates and applied upgrades.

     

    The text screen display is clear and rock solid, but when I type startx and go to GUI the screen only partially loads. The menu bar across the top is missing, and the top border of the screen flashes back-and-forth. The only thing showing on the screen is the waste basket.

     

    I'm guessing it's a display configuration issue, but I'm not sure what specifically it is. And I'm not sure why running updates and upgrades didn't reset those settings so the display runs properly.

     

    Any ideas? Thanks!

     

    PSR

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Alex,

     

    Hello.  Did you ever manage to get touch to work?  I am seeing issues w/ JDK/JRE 8 and JavaFX too.  I am getting the following error at the Netbeans console: 

         "SEVERE: 601 udevInput.c:1596 lens_input_pointerEvents_handleSync: malformed multi touch event - ignoring".

     

    I did find the following post, which I believe leads to a hack solution, but it does lead to some clues about what is wrong.  I need a better solution if I have to reboot when removing USB devices: 

         Solved: eGalax Touch Screen issues with JavaFX (on Raspberry Pi) | JavaFX Delight 

     

    -Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>