Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116538 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    Were the white plastic parts of the connectors that interface to the flat flex raised, cable inserted and then pushed back down?

    I can't see that you've done anything wrong to be honest. You may need to return it from where it was purchased, but may be worth waiting a day or two in case

    anyone else on the forum has suggestions. There is a guide to the configuration details here just in case you can spot any deviation between that and what you encountered when

    setting up the display: Essential Raspberry Pi Peripherals #2 (annex 2): 7" LCD touch screen display installation notes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to shabaz

    image

    Here's my setup. You can see the jumper cables from one and six to the bottom and the ribbon cables. I double checked my cables on the adapter board and they are all perfect. When it's powered, I place my power cord into the adapter, and it powers the Pi (I know because the lights on the Pi turns on)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    Can you take photograph(s) of your setup, showing in detail how you have connected the boards together and any cables? An overall photo and then detail near the connections.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to shabaz

    The current is 2.5A. The red light on the Pi turns on, and so does the green. When I connect it with HDMI, it works flawlessly. There are no other symptoms. My Pi works great, but its just the screen and the adapter board. And finally, yes there were no errors and yes the orientation is correct. I think that this may be an issue with the screen itself. Is there any way to fix it? I dont want to spend 60 pounds on a new screen.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    The voltage may be 5V, but current is shown in amps (or milliamps). It may say 1A for example or 2000mA as another example. Also you need to be precise. 'It doesn't work' is insufficient information. Are indicators lighting up to show network activity for example, or does the RPI not boot at all? Do you still observe output via HDMI? Any other symptoms? Dimmer power LED?  By 'No and Yes'  do you mean 'No there were no errors' and 'yes the orientation is correct'?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to shabaz

    No and yes. The max current is 5V. However, I am using a US-UK adapter. Would that change something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to e14 Contributor

    I know you say you've tried everything in dozens of videos, but with no additional information I think the following needs confirming:

     

    Were there any errors generated during the update/upgrade part of the instructions?

    Is the flat flex connector oriented in the same way as the photos?

    What is the max current that your power supply supports?

    Could you try a smartphone power supply, in case the one you're using cannot supply enough current?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hey all,

     

    I recently bought a Raspberry Pi 2 with this screen. I followed dozens of videos and websites, and it still doesn't work (I did everything they said- the ribbon cable on the back and front of the adapter board, screw it down, and connect the Pi to it with a DSI cable and 2 wires. Plug in the adapter to a socket and somehow it should work. For me, however, it does not.) I have an SD card with the newest version of Raspbian installed. I have made my Pi work on my TV through an HDMI cable, so I can enter commands if needed.

     

    Please help! :(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • xamabc
    xamabc over 10 years ago

    good morning

    I am a novice in reference to raspberry pi. I recently acquired a Raspberry Pi 2 model B. I also bought a 7-inch screen (touch screen). So far no problem. I followed all the tutorial but can not get the touch of the screen work. I have image but does not work the touch panel. Any suggestions?

     

    Buenos dias

    Soy un novato en referencia a raspberry pi. Hace poco he adquirido una Raspberry Pi 2 modelo B y la pantalla de 7 pulgadas (pantalla tactil). Hasta aqui ningun problema. He seguido todo el tutorial pero no consigo que funcione la parte tactil de la pantalla. Tengo imagen pero no funciona el panel tactil. Alguna sujerencia?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    I have the display working ok but I cannot get the keyboard (on the screen) to show.

    sudo apt-get install matchbox-keyboard installs ok and I run update and upgrade but the keyboard is not showing in Accessories.

    Do I need to run some configuration or initialization?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>