Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116547 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hello Enrico,

    I'm sorry, but after a last disassembly followed by reassembly helped my daughter who lent me the eyes to the connections, the screen remains black desperately. Rest there a hope?

    Thierry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Hello Thierry,

     

    I am sorry that you loose so much time but IMO it is the only way to be 100% sure. If the stuff again does not work I suggest at this point that you ask for a replacement. I think that some of your previous posts and comments in this discussion may give a clear explanation of the issue to the technical support.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hello Enrico,

    To answer your last point tonight I disconnect the set and I redo the operations one by one by taking the time to check the accuracy of my editing.

    Thierry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Hello Thierry,

     

    well at least we are speaking of the system in the same condition and this works here. So, please check the following things (I know that it is boring but it is nice to recheck again). The two power cables from the display board to the Raspberry PI are connected correctly? (black and red cables). I suppose yes, check that you have plugged them in the right way (Vcc and GND).

     

    The second thing to check is the flat cable. Pay attention to the image in the tutorial on top of this page, the flat cable has the connectors only on one side. And the surface of the cabe (hopefully) is blue-written on one side and white on the other. When the flat cable is connected correctly between the two boards, the blue written side should be the external one while the white side should be the internal one. Is this ok too ? If no, simply revert the direction as if you connect it wrong there is not contact at all and nothing appear.

     

    P.S. from the photos yo have published on your original post these two things seems ok, but it is just to be 100% sure.

     

    Let me know. Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hello Enrico,

    I looked at the old forum posts and more precisely the link
    Essential Peripherals Raspberry Pi # 2 (annex 2): 7 "LCD touch screen display installation notes
    I installed the 2015-05-05 Rasbian Wheezy and I did after installing an update as specified in your link. I rebooted my Raspberry after unplugging the HDMI terminal, ascended the white tablecloth and plugged my power 5V 2A, and the screen remains black.

    Thierry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Hello Thierry,

     

    please take a look to the past posts in this discussion, I have already shared the solution to your issues. If you can't find them let me know and I will repost them.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    That's eight days I received my screen 7 "Touchscreen, I checked the connection of tables, the 5V supply. My Raspberry Pi Model B 2 rotates with Openplotter (Debian Wheezy OpenCPN +) and as I branch out my TV I have a resolution of 1824x984, automatic display setting I can not change. Finally I also did a system update (sudo apt-get upgrade && sudo apt-get update). I do not know what to do to run my 7 "screen.
    Can you help me
    Thank you

     

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to morrellm

    Hi Mike,

     

    In the post I wrote a full enclosure to solve a couple of potential issues when using the display as-is, but it's a personal initative. In the post mentioned above, the images shows the prototype while here you can find the finished one : https://drobott.com/item/129/Raspberry-PI-7andquot-Touch-Screen-Display-Custom-Frame

    Here instead I have published the assembly guide instructable: Raspberry PI Touch Screen Frame and Case Assembly Guide

     

    Cheers. Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • morrellm
    morrellm over 11 years ago

    Has anyone come up with a reliable on/off switch for the touchscreen ??  Inserting the mini USB connector is getting old real quick?

     

    I also see a frame adapter and stand is out there.  Is the plan to offer a full enclosure?  Seems to be the next step.  Here a jumper from the display board to a female USB connector that can be mounted to the side of the enclosure is the way to go!

     

    Just streaming folks.!

     

    BTW, never in my life time did I ever think my Linux knowledge would be put to a "fun" use! Thanks!

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to morrellm

    Hello Mike,

     

    more than an idea image The keyboard as far as I know does not appear in the menu in no one version of the Pi but randomly it happens in the menu image

     

    So, don't worry and take a look to these tutorials I wrote about the installation and use of the LCD with the PI:

     

    Essential Raspberry Pi Peripherals #2 (annex 1): Making a custom frame for the 7" LCD touch screen display

    Essential Raspberry Pi Peripherals #2 (annex 2): 7" LCD touch screen display installation notes

    Essential Raspberry Pi Peripherals #3: The kivy framework for small display and touch screens

     

    For completeness I have put all the three tutorials but the keyboard issue workaround is explained in the second link above.

     

    Cheers. Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>