Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Documents Raspberry Pi 7” Touchscreen Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: joeman
  • Date Created: 11 Aug 2015 6:55 PM Date Created
  • Last Updated Last Updated: 16 May 2022 10:17 AM
  • Views 116556 views
  • Likes 20 likes
  • Comments 478 comments
Related
Recommended

Raspberry Pi 7” Touchscreen Display

image

Raspberry Pi 7” Touchscreen Display

Buy Here  Display Installation Guide

Install Virtual Keyboard* Other Pi Accessories  image

The 7” Touchscreen Monitor for Raspberry Pi gives users the ability to create all-in-one, integrated projects such as tablets, infotainment systems and embedded projects. The 800 x 480 display connects via an adapter board which handles power and signal conversion. Only two connections to the Pi are required; power from the Pi’s GPIO port and a ribbon cable that connects to the DSI port present on all Raspberry Pi’s.  Touchscreen drivers with support for 10-finger touch and an on-screen keyboard will be integrated into the latest Raspbian OS for full functionality without the need for a physical keyboard or mouse.

*Note: Your NEW Rasp Pi 7.0 needs you to Add a Virtual Keyboard….

imageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Raspberry Pi Sense HAT

image

Learn More  image

Technical Specification:

image  7” Touchscreen Display

image  Screen Dimensions: 194mm x 110mm x 20mm (including standoffs)

image  Viewable screen size: 155mm x 86mm

image  Screen Resolution 800 x 480 pixels

image  10 finger capacitive touch

image  Connects to the Raspberry Pi board using a ribbon cable connected to the DSI port

image  Adapter board is used to power the display and convert the parallel signals from the display to the serial (DSI) port on the Raspberry Pi

image  Will require the latest version of Raspbian OS to operate correctly

 

Features and Benefits

image  Turn your Raspberry Pi into a touch screen tablet, infotainment system, or standalone device.

image  Truly Interactive - the latest software drivers will support a virtual ‘on screen’ keyboard, so there is no need to plug in a keyboard and mouse.

image  Make your own ‘Internet of Things’ (IoT) devices including a visual display. Simply connect your Raspberry Pi, develop a Python script to interact with the display, and you’re ready to create your own home automation devices with touch screen capability.

image  A range of educational software and programs available on the Raspberry Pi will be touch enabled, making learning and programming easier on the Raspberry Pi.

Kit Contents

image  7” Touchscreen Display

image  Adapter Board

image  DSI Ribbon cable

image  4 x stand-offs and screws (used to mount the adapter board and Raspberry Pi board to the back of the display

image  4 x jumper wires (used to connect the power from the Adapter Board and the GPIO pins on the Pi so the 2Amp power is shared across both units)

NOTE: THE RASPBERRY PI AND POWER SUPPLY ARE NOT INCLUDED IN THIS KIT AND ARE SOLD SEPARATELY.

Compatible With:

Raspberry Pi 3 Model B

Raspberry Pi 2 Model B

Raspberry Pi Model B+

Raspberry Pi Model A+

The display will technically work with the Model A and Model B boards (connecting it to the DSI port on the Pi board), however the mounting holes on the back of the display will only line up with the newer board design (A+, B+, Pi 2 and Pi 3).

 

How to Install the Matchbox-Keyboard for your Pi

image

1. Connect a physical keyboard to the Raspberry Pi (or SSH into it if that’s your thing.)

2. Connect to the internet via WiFi or Ethernet.

3. Open the terminal.

4. Type sudo apt-get install matchbox-keyboard

5. Let the program download & install (takes 30s-1min depending on your connection.)

6. Exit the terminal & reboot your Pi.

7. The keyboard can be found by clicking the Menu -> Accessories -> Keyboard.

 

Operating System Support

In order to be sure you’re running the latest version of Raspbian, connect your Raspberry Pi to the Internet and then open LX Terminal.  Type ‘sudo apt-get update’ to download the latest version of the OS.  Once that’s complete, type ‘sudo apt-get upgrade’ to apply the download to your Raspberry Pi.  That way you’ll have all of the latest drivers and software needed to support the touch screen display.

Step 1

image

Step 2

image

Step 3

image

Step 4

image

Step 5

image

Step 6

image

Step 7

image

Step 8

image

Step 9

image
  • pi_guide
  • raspberry
  • pi
  • pi_display
  • raspberry_pi
  • matchbox_keyboard
  • display
  • touchscreen
  • 7”
  • guide
  • installation
  • 7_inches
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago in reply to idometeor +3
    Jason Does Meteor wrote: As mentioned, I tried that. Actually you didn't, you stated: I have tried everything and I cannot get the display to rotate in Raspbian. I have written many X configuration files…
  • softweyr
    softweyr over 11 years ago in reply to ejohnfel +2
    Yeah, this is not a bad price for a 7" display, plus you get the touchscreen, integrated keyboard, etc. And tomorrow is my birthday!
  • bwelsby
    bwelsby over 11 years ago in reply to phantomski +2
    The reduced screen size is because Overscan settings are enabled. you can either comment out the settings in /boot/config.txt or just run raspi-config and select the advanced options then Overscan , Disable…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Bitte nicht mißverstehen.

    Siehe oben. Schritt 5 und 6 beachten.

    Die Beschriftung des Flachbandes muß nach unten (von hinten aufs Display gesehen), zeigt bei Dir nach oben.

    Ich habe mein Flachband probehalber mal montiert wie Du (beidseitig meinte an beiden Anschlüssen). Da ging bei mir auch nichts.

    Ich habe mein update/upgrade ohne Display gemacht und danach erst montiert. Funktionierte auch.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    ok probiere ich mal aus. Aber das Kabel hat nur auf einer Seite Kontankte. Das Flexkabel habe ich so rein gesteckt, dass die Pins auf der Raspberry-Seite zum inneren Seite des Raspberrys zeigen. Die andere Seite des Flexkabel ist auch blau beschichtet. Will man das Kabel wie in der Beschreibung montieren muss man es quasi einmal längs um 180° drehen und einmal quer um 180° drehen.
    Ich glaube nicht, dass das ein Unterschied macht aber ich probiere es aus. Ich hatte sogar mit einer Messspitze an beiden Boards die Durchgänge geprüft.

    Zwischenfrage, erkennt der RP das Display nur, wenn das Flexband auch richtig montiert ist, resp. muss ich jedes mal get update / get upgrade durchführen`?

    Thx

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Hi Richard, thank you.

     

    Check this: https://drobott.com/item/129/Raspberry-PI-7andquot-Touch-Screen-Display-Custom-Frame

    (10% off Element14 users discount code: W0E49MYQ) image

     

    Cheers. Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bobgerman

    http://nl.farnell.com/multicomp/cbrpp-ts-blk-wht/raspberry-pi-touchscreen-enclosure/dp/2494691?MER=en-me-sr-b-all

     

    Check this enclosure

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Mein Kabel funktioniert "beidseitig gedreht" nicht (gerade probiert). Nur in der im "Installation Guide" dargestellten Variante.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    I based what I saw on my installation, the image I have attached to the post and your photo that seems having the cable to the opposite side.

     

    enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics

    Hi. You can Mount the flex cable two ways (Text inside or Outside). You only have to watch the contacts. The opposite has no contacts and is blue painted. But I'll check on this again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to balearicdynamics

    Good on you. It looks well styled, functional and I'm sure it is designed to a good standard.

    I expect (or I hope) Pimoroni will get updated stands out to their customers at no cost (not just for good relations, but because they are leaving themselves open by supplying a not-fit-for-purpose product, because all those customers are entitled to buy elsewhere an alternate case (at any reasonable price, even if it is higher) and make Pimoroni liable for any additional cost incurred - at least in the UK, but the root lies in the fact that all this should have been ironed out in the display's field trials, rather than raspberrypi,org spotting the upside-down error after releasing the product.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to shabaz

    You saw it image Well !

     

    Me too I was speachless. I examined this stupid stand from Pimoroni. And I have one here. This is not the only problem.

     

    1. The stand is upside-down and the screen should be set for 180 deg rotation to see (excluding vampires living on the ceiling)
    2. It is exclusively on the back, so as a matter of fact if you want to use this as for a protection and fix the screen somewhere, you can't.
    3. The laser-cut parts are larger than needed (maybe wrong measure). It is only just 0.7 mm but it is sufficient to make all floating until you don't fix the "support" with the back stand that is the only stuff useful.
    4. The absence of a front frame loos design and general quality of the support.

     

    Then I decided to make a project by my own and sell it. Not only but if I can earn few $ and sell it for 20$ including the light white plastic front (that has the double action of keeping all in the right position and - IMO - giving a sort of decent aesthetic, they are also a bit expensive. It sounds me like something though just last minute to give an apparent "value added" to sell it at a real higher price (about 70 pounds including the LCD).

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to balearicdynamics

    I was looking for a guide/FAQ, and found this: http://forums.pimoroni.com/t/official-7-raspberry-pi-touch-screen-faq/959

    What was interesting, is that the display was upside down and Pimoroni created a plastic stand/enclosure, and now

    the image is flipped for better viewing angles, but the stand can't be inverted. So rather than keep the better viewing angle, the

    image needs to be flipped back again by configuration for users of the stand.

    I'm speechless now..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>